Experimenting with Sensor Fusion
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Sensor Fusion
  • More
  • Cancel
Experimenting with Sensor Fusion
Forum If you have a question about the Experimenting with Sensor Fusion competition, you can ask it here.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Sensor Fusion to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 39 subscribers
  • Views 5896 views
  • Users 0 members are here
Related

If you have a question about the Experimenting with Sensor Fusion competition, you can ask it here.

rscasny
rscasny over 4 years ago

If you have a question about the Experimenting with Sensor Fusion competition, you can ask it here.

  • Sign in to reply
  • Cancel

Top Replies

  • surbhika
    surbhika over 4 years ago in reply to scottiebabe +5
    Hi scottiebabe ,,it's actually a bit daunting at first to work around xilinx tools (they are SO MANY). You can have a look at this github repository to help you work around that: https://github.com/Xilinx…
  • javagoza
    javagoza over 4 years ago in reply to scottiebabe +3
    I would like to apply, I am still in the analysis phase of what possibilities I have to do something decent in two months. I am very scared by the instability of the element14 website on weekends when…
  • scottiebabe
    scottiebabe over 4 years ago in reply to cstanton +3
    Her last project definitely puts her in the FPGA expert class :) My instinct is that starting a Image processing project from scratch is a huge undertaking. It is just a thought.
Parents
  • javagoza
    0 javagoza over 4 years ago

    While trying out one of the examples designs that come with Vivado for the SP701 board, I ran into a licensing issue. What licenses are supplied with the kit?

    • [Common 17-69] Command failed: This design contains one or more cells for which bitstream generation is not permitted: mb_preset_i/axi_ethernet_0/inst/mac/inst/tri_mode_ethernet_mac_i/bd_b764_mac_0_core () If a new IP Core license was added, in order for the new license to be picked up, the current netlist needs to be updated by resetting and re-generating the IP output products before bitstream generation.
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 4 years ago in reply to javagoza

    It seems that there are some trial licenses and specifically there is a 120-day trial license for the AXI 1G/2.5G Ethernet Subsystem

    image

    With this design it is the only IP core that reports license problems.

    image

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • saadtiwana_int
    0 saadtiwana_int over 4 years ago in reply to javagoza

    That would make sense because the Spartan-7 does not have a hard Ethernet core (unlike Zynq series, for example), and the soft Ethernet cores are not supplied for free by Xilinx. If you're not goint to use Ethernet in your project, then it's not an issues. If you are, then the 120 days trial license could cover the project duration fine. But i DO understand the frustration with limited-time trial licenses Slight smile. Especially since the (paid) IP core licenses are too expensive for individual/hobbyist use.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • saadtiwana_int
    0 saadtiwana_int over 4 years ago in reply to javagoza

    That would make sense because the Spartan-7 does not have a hard Ethernet core (unlike Zynq series, for example), and the soft Ethernet cores are not supplied for free by Xilinx. If you're not goint to use Ethernet in your project, then it's not an issues. If you are, then the 120 days trial license could cover the project duration fine. But i DO understand the frustration with limited-time trial licenses Slight smile. Especially since the (paid) IP core licenses are too expensive for individual/hobbyist use.

    • Cancel
    • Vote Up +3 Vote Down