Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog Auto-Cutoff Circuit for Room Heaters - Blog 1
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsjawale24
  • Date Created: 18 Jan 2022 5:42 PM Date Created
  • Views 5790 views
  • Likes 8 likes
  • Comments 2 comments
  • thermal switch
  • opamp
  • kemet
  • Experimenting with Thermal Switches.
  • experimenting_with_thermal_switches
  • experimenting challenge
Related
Recommended

Auto-Cutoff Circuit for Room Heaters - Blog 1

rsjawale24
rsjawale24
18 Jan 2022
Auto-Cutoff Circuit for Room Heaters - Blog 1

                Auto-Cutoff Circuit for Room Heaters - BLOG 1            

This is the first blog in the Experimenting with Thermal Switches Challenge. In this blog, I'll introduce myself and the experiments that I wish to conduct using the thermal switches from Kemet.

I'm an electronics engineer with about eight years of experience in various domains such as analog, RF, and embedded systems. I frequently participate in Design Challenges on e14 Community. I wish that someday I'll have my electronics lab to perform advanced experiments with RF and play around with instruments to analyze various circuits.

                                     Proposed Project                                  

Room heaters are very common in Indian homes during winters. Since the winter weather is not as harsh in many states, people do not have thermostats and radiators for the entire house; instead, they use typical room heaters like the one shown in the picture.

heater

These heaters are available in various models and power. This is a very basic heater with two heating elements, each 400W. Each heating element is a coiled resistance wire directly connected to the AC supply. The alternating current heats the coil according to the equation H = I2Rt, where I is the amount of current flowing in the wire, R is the resistance of the wire, and t is the amount of time the current flows.

These heaters cause suffocation and overheating of the room as there is no temperature control mechanism. These heaters are highly inefficient. But the problem with these heaters is not only their efficiency but also their safety. It comes with a simple switch at the bottom, which cuts off the power supply to the heating elements if the heater topples.

But imagine a situation on a cold wintery night, you keep the heater on and fall asleep. There have been multiple accidents and deaths due to these heaters if someone forgot to switch it off before sleeping. Hence, I plan to design a simple temperature-control circuit for such a heater using the Kemet thermal switches provided in the experiment design kit. I plan to restrict myself to using only discrete components and not go for any complex MCU as I want to keep the cost of the circuit low such that a common person can afford the circuit and easily integrate this safety feature with the heater.

                                     Block Diagram                                     

The basic block diagram of the heater with the thermal cutoff circuit is shown below.

block diagram

The basic components for the circuit consist of the heater, a relay to control the heater using the comparator output, an opamp for comparator, and the thermal switch from the design kit.

If time permits, I'll perform more experiments with the thermal switches by using them in other projects.

I would like to thank the e14 team and Kemet for sponsoring the competition and providing the kit.

  • Sign in to reply
Parents
  • Gough Lui
    Gough Lui over 4 years ago

    A heater overheat protection sounds like a perfect application for a thermal switch.

    As the switch output is a binary switching of a contact, perhaps you could drive the relay directly through the thermal switch itself and avoid the need for an op-amp as long as the relay coil current is within the rating of the switch (0.1/0.3/0.5/0.55A depending on the model). Don't forget to have a back-EMF protection diode on the relay coils.

    It may be nice to have the circuit powered from the mains as well, for convenience.

    Another thing to think about is the safety of the circuit itself - perhaps it would be best to design it in such a way that it is "fail-safe" - i.e. the heater is turned off if the battery runs out or power is lost.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to Gough Lui

    Hi Gough!

    Thanks for the input!
    Yes, I haven't yet looked into the datasheets of the thermal switches. Just to be safe and avoid any kind of false triggering, I went with an opamp.
    But yes, since it's just a switch it has only two states (ON/OFF) so I'll see if it's possible to drive the relay directly.
    Yep, the flyback diodes are assumed to be there by default as no experienced electronics engineer will miss out on that Slight smile
    I'll look into the fail-safe aspect as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsjawale24
    rsjawale24 over 4 years ago in reply to Gough Lui

    Hi Gough!

    Thanks for the input!
    Yes, I haven't yet looked into the datasheets of the thermal switches. Just to be safe and avoid any kind of false triggering, I went with an opamp.
    But yes, since it's just a switch it has only two states (ON/OFF) so I'll see if it's possible to drive the relay directly.
    Yep, the flyback diodes are assumed to be there by default as no experienced electronics engineer will miss out on that Slight smile
    I'll look into the fail-safe aspect as well.