Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog Blog 2:- The Thermal Switches Experimenter’s Kit
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: manojroy123
  • Date Created: 18 Mar 2022 1:11 PM Date Created
  • Views 1229 views
  • Likes 6 likes
  • Comments 1 comment
  • kemet
  • experimenting with Thermal Switches
Related
Recommended

Blog 2:- The Thermal Switches Experimenter’s Kit

manojroy123
manojroy123
18 Mar 2022

The Thermal Switches Experimenter’s Kit:-

The kit consist of thermal reed switch and thermal guard switch as shown in the figure 1 bellow

 image

Figure 1

 Some question that needs to be answered

What are thermal reed switch ?

Thermal Reed Switch is a highly reliable, precise temperature-sensitive switch. Its unique proprietary design features a magnet and a temperature-sensing soft ferromagnetic substance called Thermorite®. The material’s magnetic flux density decreases as the temperature increases turning it into a paramagnetic substance at the Curie temperature.

What is  Thermorite ?

Thermorite is ferri-magnetic material that changes its magnetic property rapidly at its Curie temperature.

What is a reed switch ?

The reed switch is an electrical switch operated by an applied magnetic field. 

Working of reed switch ?

The switching mechanism is comprised of two ferromagnetic blades, separated by only a few microns. When a magnet approaches these blades, the two blades pull toward one another. Once touching, the blades close the normally open (NO) contacts, allowing electricity to flow.

image

Figure 2

Working of thermal reed switch ?

Thermal reed switch are either switch on or off depending upon the temperature and the type of thermal switch. In blog 3 you will see experiment with various thermal reed switches.

What are thermal guard switch ?

Thermal Guard (OHD) are temperature-sensing switches composed of a magnet and a temperature-sensing soft ferromagnetic substance called Thermorite. This material’s saturation magnetic flux density decreases as the temperature increases, and it turns into a paramagnetic substance at its Curie temperature

Anything more looking in the kit ?

Temperature indicating paint/paper also known as thermochromic piant/paper

  • Sign in to reply
  • DAB
    DAB over 4 years ago

    Nice kit.

    I look forward to seeing your testing.