Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Blog Experimenting with Vibration Sensors  as Predictive Maintenance Model Trainer #2
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 20 Jan 2021 7:45 AM Date Created
  • Views 3459 views
  • Likes 7 likes
  • Comments 5 comments
Related
Recommended

Experimenting with Vibration Sensors  as Predictive Maintenance Model Trainer #2

fyaocn
fyaocn
20 Jan 2021

      • Kemet Vibration Sensor Experiment for Predictive Maintenance Model Trainer
      • 1 Introduction
      • 2 Hardware and Software
      • 3 Unboxing and Preliminary Functional Test
      • 4 Senaries to be tested
      • 5 Data logging
      • 6 Data training
      • 7 Data Deploing with AI capabilities
      • 8 Summary and Conclusion
      • 9  Reference and contributions

Kemet Vibration Sensor Experiment for Predictive Maintenance Model Trainer

1 Introduction

Kemet Vibration Sensor show great promising application in Predictive Maintenance in industrials. I have planned to  show how it works.

Within 60 days I have completed steps 1 only, and step 2 and step 3 are ongoing activities without available output data to show in this blog now. I have flahed one STM32H747-Discovery Board dead after I have completed a lot of work, with 2M Flash and LCD screen fit for ToughgfxDesigner and Cube-AI. I have to shift to fast deploy Arduino 101 to meet the schedule. Here is what I have got.

Step 1,Build one portable tool for vibration tracing on car, recording the data from Kemet vibration sensor

Complete with Arduino 101.

Step 2, Build one CNN model and train with DL framework. hopefully, the model can be  convergence to one valid result.

Framework complete, but data collected is not enough for model training ,the train fail without valid model for ouput.

Step 3, Deploy the model on the Embedded platform to be used as predictive maintenance hub.

That is the part I spend most of the effort. I have try tensorflow-lite on STM32F070, STM32G431 and STM32F767-nucleo, PaddlePaddle on desktop, and DeepC in arduino,and NNoM on rtthread RTOS.

That proves not valid for most of the MCUs, Flash restriction can be top one.

While STM32L476RG-nucleo with 1M flash proves valid. But I have to change to arduino 101 for quick deploy. Deploy on MCU can be challenging, but interesting. I think I would better spend more time on one new AI Engine framework for MCU. I would share the progress in blog in this year. I am tire of so many revision-ever-changing rubishes AI engine. But SesiML may be good choice, if not as critical as I am.

 

2 Hardware and Software

  • Arduino IDE 1.8.3 latest release
  • Arduino 101
  • Not including,
  • STMCubeIDE
  • ToucchGFX Designer
  • CubeMX
  • STM32H747-DIscovery, STM32G431-Nucleo,STM32-L476-Nucleo
  • STMCube-AI

 

3 Unboxing and Preliminary Functional Test

3.1 Unboxing and wiring

Sorry for not post more picture. I start this blog on last day of submission. Deadline is good thing, or I would wander and explore more and provide no output.

image

The best choice for wiring of this sensor shall be to remove out-of-factory connector, cut the line to fit the length, weld new terminals with similar color and use heat-shrinkage sheath to seal the teminals.

Try use minimal length of wire as possible, that is always good.

 

3.2 Data logging with Arduino Serial

First, test the performance of the sensor. Arduino can provide 10-bit ADC resolution up to 1024, with 512 as still state, 29 milli-second per sample cycle. That is OK for 16kHz specification. Here is simple sketch,

unsigned long myTime;
int st=10000;
void setup() {
  Serial.begin(9600);
}
void loop() {
  Serial.print("Time: ");
  myTime = micros();
  for (int i = 0; i <= st; i++) {
    int sensorValue = analogRead(A0);    
  }
  myTime=micros()-myTime;
  Serial.println(myTime); //prints time since program started
  delay(5000);          // wait a second so as not to send massive amounts of data
}

 

Output for Serial Console, With 29us per cycle ADC.

image

Use data logger for sensor data, be remember, use println() to add "\n" at each data or these is nothing to show.

image

peak shows the tap to the platform where the sensor is placed. That is very very sensitive.

 

4 Senaries to be tested

I have try with the following test,

4.1 Comparing with gryo-sensors

This vibration sensor is responsive to Z-axis acceleration, but more sensitive, the gyro-sensor on arduino 101 is Intel-Curie embedded. Not so sensitive and slow in sample frequency. But show similar tendency, it can be cross-check each other.

4.2 Tapping

Tapping, or rough rubbing on desktop can trigger the reading.

4.3 Heart beating and breath

It can be used as fast heartbeat detection and breath detection. Just hold the sensor on palm, the heartbeat can make minor shake of hand in paces, breath can bring about larger reading from sensor.

 

4.4 Small motor vibration

For small 5V motor drives fan for CPU heat-dissipation, it can detect the On/Off state.

 

4.5 Giant motor vibration

Not tested yet.

I have access to one 1MW gas turbine roaring all day aroung, that would be amazing if sensor array can be place aroung the big machine.

4.6 Car engine to be tested

Just tested to read data with Arduinio 101 data logger. Annotation is difficult simply with arduio, one Human-Machine Interface to select the running-idle-speedup-brake, the car have be mainenance recently and runs well so Fault state data is still not available.

 

5 Data logging

5.1 Function for the Datalogging

2M On-board winbond flash shall be used as data storage, the SPI port is occupied, I could not use SD card extension shield for larger size.

The following library shall be used,

#include "CurieTimerOne.h"
#include <CurieSerialFlash.h>
#include <SPI.h>

Here is funciton selection by means of serial connection on 115200bps,

Selection: (0)-Quit; (1)-lists; (2)- EraseALL; (3)-DataFlush;(4)-BatchSampling.

Press 0 , return to hint

Press 1, list all files on flash,

Press 2, Erase all the file. The file is named as .000 .001 ......, can be write once only. Refresh data need erase all.

Press 3, Outout the data to serial console to visualization or data record. I have design one simple Python Program to receive the data from Arduino 101, the data can be saved in to SQlite3 database

Press 4, Sampling on batches.

 

5.2 Arduino serial with SD

This sketch is sore of complex, with switch-case selection to define the state of Manipulation, Can not explain further, but the full code tells everything.

/* Kemet Vibration Sensor Data Logger                              
 *  For Experiment for Sensors
 *  Date Jan. 2021 by fyaocn
 *  Based on Paul Stoffregen's SerialFlash library @ https://github.com/PaulStoffregen/SerialFlash
*/


#include "CurieTimerOne.h"
#include <CurieSerialFlash.h>
#include <SPI.h>


#define FSIZE 2048  // One Block of 4k of 0~4095 due to SRAM limitation.
#define FAULTCOUNT  10
#define SAMPLECYCLE 32    //// Batch Cycle  for Kemet Vibration Sensors
const int oneSecInUsec = 1000000;   // A second in mirco second unit.
#define SAMPLERATE  1000  // Sample Rate for Kemet Vibration Sensors
int time=oneSecInUsec /SAMPLERATE;    


bool BOOL_CHIPFULL= 1;
bool BOOL_SAMPLING= 0;
int selectionByte; // 0 For Quit.
//unsigned char bps_count=10;
//unsigned char id[5];


char afilename[12] = {'S','e','n','s','o','r','D','T','.','0','0','0'};
char contents[FSIZE];
int  idxcontents;
char filename[15]; // Format 8:3:1
unsigned long filesize;


SerialFlashFile file;
int analogPin = 0;


//Blink if fault
void error(void){
  unsigned char i;
  //Serial.println("Something Wrong with error code::0x");
  for (i=0; i<FAULTCOUNT; i++) {
    digitalWrite(LED_BUILTIN,HIGH);
    delay(500);
    digitalWrite(LED_BUILTIN,LOW);
    delay(500);    
  }
}


void listfile(void){
     Serial.println("Files on the windbond Chip");
     SerialFlash.opendir();
   while (1){
    //char filename[13]; 
     if (SerialFlash.readdir(filename, sizeof(filename), filesize)) {
      Serial.print("  ");
      Serial.print(filename);
      Serial.print("  ");
      Serial.print(filesize);
      Serial.print(" bytes");
      Serial.println();
    }
    else   {
      Serial.println(" End of lists.");
      break;
    }
  }
}
    
void readfile(){
  int j;
  int dtoutput;
     Serial.println("Read File and Data Flushing.");
     SerialFlash.opendir();
   while (1){
     if (SerialFlash.readdir(filename, sizeof(filename), filesize)) {
      delay(1000);
      file = SerialFlash.open(filename);
            //Serial.println( String(filename)+"+"+String( file.size() ) );
      if (file) {
        Serial.println( String(filename)+"+"+String( file.size() ) );
        file.read(contents,file.size() );
        for (j=0; j<FSIZE ; j=j+4){
          //Serial.print(contents[j]); Serial.print(contents[j+1]);Serial.print(contents[j+2]);Serial.println(contents[j+3]);
          dtoutput=(contents[j]-48)*1000+(contents[j+1]-48)*100+(contents[j+2]-48)*10+(contents[j+3]-48);
          Serial.println(dtoutput);
  
        }
        //file.erase();
        //Serial.println("End of Dumping This File.");
      }
      else {
        Serial.println(" File Open Error.");
        error();
        break;
      }
    }
    else   {
      Serial.println(" End of Data Flushing..");
      break;
    }
  }
}


void writefile(char *wtfilename){
    //SerialFlash.readID(id);unsigned long size = SerialFlash.capacity(id);
    if (!SerialFlash.exists(wtfilename)) {
      //Serial.println("Creating file " + String(rtfilename));
      SerialFlash.create(wtfilename, FSIZE);
    }
    //contents[0]='K';
    file = SerialFlash.open(wtfilename);
    file.write(contents, strlen(contents) + 1);
    //Serial.println("String \"" + String(contents) + "\" written to file " + String(wtfilename));
}


void timedVibSensorIsr()   // callback function when interrupt is asserted
{
  int sensor = analogRead(analogPin);
  if (idxcontents<FSIZE){      
        contents[idxcontents+3]=48+sensor%10;
        contents[idxcontents+2]=48+sensor/10%10;
        contents[idxcontents+1]=48+sensor/100%10;
        contents[idxcontents] =48+sensor/1000%10;
  idxcontents=idxcontents+4;
  }
  //toggle = !toggle;  // use NOT operator to invert toggle value
}


void vibdata_sampling(void){
  unsigned char k;
  idxcontents=0;  //Serial.println("Sampling Start..."); 
  delay(1000);  // 10 seconds of delay, regularly 'interrupted' by the timer interrupt  
  for (k=0; k< SAMPLECYCLE; k++) {
      CurieTimerOne.start(time, &timedVibSensorIsr);  
      while (1) {
        delay(1);
        if (CurieTimerOne.readTickCount()>=FSIZE){
            CurieTimerOne.stop(); 
          afilename[11]=char( (48+(k%10)));
          afilename[10]=char( ( 48+( int(k/10)) ));
          writefile(afilename);
          break; 
          }
      }
  }
  delay(1000);  // 10 seconds of delay, regularly 'interrupted' by the timer interrupt
  Serial.println("Vibdata Sampling OK.");
    //Serial.println(CurieTimerOne.rdRstTickCount());  // Reads and Resets tick count
}






void setup() {
  pinMode(LED_BUILTIN, OUTPUT);  
  if (!SerialFlash.begin(ONBOARD_FLASH_SPI_PORT, ONBOARD_FLASH_CS_PIN)) {
    //Serial.println("Unable to access SPI Flash chip");
    error();
    }
  else {    
     //SerialFlash.opendir();
    if (SerialFlash.readdir(filename, sizeof(filename), filesize)) {
         //Serial.print("There is file ");Serial.print(filename);
      BOOL_CHIPFULL=1;
      BOOL_SAMPLING =!BOOL_CHIPFULL;
    }
    else {
        //Serial.print("Empty Flash.");
      BOOL_CHIPFULL=0;
      BOOL_SAMPLING =!BOOL_CHIPFULL; 
      SerialFlash.eraseAll();
      vibdata_sampling();
      //Serial.println(BOOL_SAMPLING);SerialFlash.eraseAll();
    }
  }


  // Init Serial if chip is full,
  if (BOOL_CHIPFULL){
    Serial.begin(115200);
    while (!Serial){
      //Wait for the serial ;
      }
      delay(100);
      Serial.println("Ready for Serial Connection and Data Flushing collection."); 
      Serial.println("Selection: (0)-Quit; (1)-lists; (2)- EraseALL; (3)-DataFlush;(4)-BatchSampling."); 
      //Serial.println   (BOOL_SAMPLING);
  }
//Serial.println("End of Setup");
}




void loop() {
  delay(1000);
  if (BOOL_SAMPLING){
    vibdata_sampling();
  }
  else {
    //Serial.println("Selection: (0)-Quit; (1)-lists; (2)- EraseALL; (3)-DataFlush; (4)-BatchSampling."); 
    if (Serial.available() > 0) {
      selectionByte = Serial.read();
      //Serial.println(selectionByte, DEC); // '/n' show with value 10 after number pressed.
    }
    switch (selectionByte) {
      case '0':
        //Serial.println(selectionByte, DEC);
        Serial.println("0 Quit and Re-entry.");
        Serial.println("Selection: (0)-Quit; (1)-lists; (2)- EraseALL; (3)-DataFlush;(4)-BatchSampling.");         
        break;
      case '1':
        //Serial.println(selectionByte, DEC);
        Serial.println("1 List ALL.");
        listfile();
        break;
      case '2':
        //Serial.println(selectionByte, DEC);
        Serial.println("2 Erase ALL.");
        SerialFlash.eraseAll();
        Serial.println("Full chip erase completed.");
        break;
      case '3':
        //Serial.println(selectionByte, DEC);
        Serial.println("3 DataFlush.");
        readfile();
        break;
      case '4':
        //Serial.println(selectionByte, DEC);
        Serial.println("4 Sensor Batch Sampling."); 
        SerialFlash.eraseAll();
        vibdata_sampling();
        break;
      default:
        break;      
    }
    //End of Console Selection.    
  }
  delay(1000);
  //End of Loop
}

5.3 Code for desktop control in python

# Read serail into file


import serial
import time
from datetime import datetime
import os
import pandas as pd
import numpy as np
from sqlalchemy import create_engine
import matplotlib as plt


db_name_merge='kemetvibration'
engine  = create_engine('sqlite:///kemetvib.db')


#
#vbdata=pd.DataFrame(data=np.full([1,len(['vibsample'])],np.nan),columns=['vibsample'])


        
   
BATCHCOUNT=8




def batchreadserial(ser):
    brs_count=0
    while (True):
        #ser.write(b"0\n")
        ser.write(b"3\n")
        #selectionzero=str.encode("0\n");ser.write(selectionzero)
        #rddata=int(ser.readline());brs_count =brs_count +1;
        rd=ser.readline()
        print((rd[0]))
            print (rd)
            readdaba()


def readdb():
    vibdb='kemetvibdata'
    vibdata=pd.read_sql("vibdb", con=engine)




def readdaba():
    rdcount=0;
    ser.write(b"3\n")
    while (rdcount<256):
        rddata=ser.readline()
        rdcount=rdcount+1
        print(rddata)
        if (rddata==4096):
            rdcount=0
                  
    
    
    
if __name__=="__main__" :
    ser=serial.Serial('COM4',115200) #Open port for serial
    ser.close()
    ser.open()
    batchreadserial(ser)
    ser.close()
    print("End of dataread.")

image

5.4 Refer to the flash tiff show,

image

5.5 Data logging in Car Engine

Thanks to the 3m length wire, the vibration sensor can be sticked on top cover of engine and put the arduino 101 inside the car, available for driving state data logging.

image

Look closer,

image

With 9V battery plugged, the arduino 101 can be powered by battery.

image

image

Start the car, wait for the data to be collected.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Connected the arduino board again with Arduino IDE 1.8.5, the reading is different,

image

Fetch the data from the board, the data can be used to train the model.

I have set 64 segment of file.But for data training, that is still not enough.

This car runs in good mode, just routine maintenance out of workshop. The running mode is different after about 5000km running. The data can be collect and tagged with different millage as annotation.

For example, the vibration data of 500km, 1000km, 2000km, 3000km, 5000km, 8000km or 10000km. I have tried 10000km without maintenance , the roaring of engine is quite diffent. But not recommend such a try, damage to car for sure.

Interesting if logging vibration data since 0km. I would make a try if I change new one.

Sample Data collected is attached for reference. The head, tail, and segment text shall be removed for use.

 

 

6 Data training

6.1 Make the data annotation and feed into training mode, then model output for next step.

Even there is no final product. I would like to enlight some idea on how to train data. Basicly,

NNoM is best for ARM-M4 core MCU with 1M flash. Refer to https://majianjia.github.io/nnom/  for more. The example uci-inception with UCI HAR dataset can be used as start point, from gyro-sensor combination to model training. https://github.com/majianjia/nnom/tree/master/examples/uci-inception

6.2  The codeing flow shall be

  Input
  |
  |
  Conv
  / | \
  / | \
Conv Conv Maxpool
  \ | /
  \ | /
  Concat
  |
  Conv
  |  
  Dense
  |
  Dense
  |

  Softmax

The abbrievation means as follows,

image

 

 

Based on The structure of NNoM to deploy on MCU

image

 

6.3 Training shall be made on Keras, simple to use and to understand.

Simple training net can be ,

model = Sequential() 
model.add(Dense(32, input_dim=784)) 
model.add(Activation('relu')) 
model.add(Dense(10))

Then generated Keras model shall be changed to MCU applicable data in commond in NNoM as

generate_model(model, x_test, name='weights.h')

The weights.h is generated and to be used in program as of,

#include "nnom.h" 
#include "weights.h"  
int main(void) 
{ 
nnom_model_t *model; 
model = nnom_model_create(); 
model_run(model); 
}

But this can not compatible with arduino 101. Which I have just realized, CMSIS pack shall be included beforehead. STM32Fxxx can be good.

I have placed order for one new STM32Fxx-nucleo, but can not be here right away.

 

6.4 The routine is quite simple,

  • Collected annotated data with arduino 101, tagging millage of 500km~10000km
  • Train the data with classification model like Keras.Sequential, the data shall be split into training dataset and test dataset randomly with ratio about 8:2. With some luck, the model can be trained with accuracy above 75%,
  • Generate th weight.h by transform the keras model weight,
  • Finally, deploy the model into MCU.

Luck is neccesary element, no doult.

 

7 Data Deploing with AI capabilities

Deploy the model in MCU.

With two arduino 101, one is for datalogging , the other for Prediction.

image

Best part shall be independant lightweight integer type DL engine. I may try build one if I have free time later.

 

8 Summary and Conclusion

The kemet vibration sensor is sensitive and easy to deploy. Best application shall be predictive maintenance with quite a lot space to envision.

 

9  Reference and contributions

Refer to relevent website and git retros.

Some datasheep and source code is attached here.

Attachments:
imageVS-BV203-B.pdf
ReadFileDataFlushing.zip
DataLogger.zip
  • Sign in to reply

Top Comments

  • fyaocn
    fyaocn over 4 years ago in reply to 14rhb +3
    This car runs in good mode, just after routine maintenance out of workshop. The data can be collect and tagged with different millage as annotation. For example, the vibration data of 500km, 1000km, 2000km…
  • 14rhb
    14rhb over 4 years ago +1
    An interesting read, thank you. Something I too have pondered is how to make a system to predict failure on a mechanical system but to train it when there is no failure available ! I guess you can only…
  • 14rhb
    14rhb over 4 years ago in reply to fyaocn +1
    Thank you. Have you seen the ARDUINO NANO 33 BLE SENSE that is running currently, it might be really useful to what you are doing as you can embed the AI model on that Arduino board; there are some great…
Parents
  • 14rhb
    14rhb over 4 years ago

    An interesting read, thank you. Something I too have pondered is how to make a system to predict failure on a mechanical system but to train it when there is no failure available ! I guess you can only train it to determine things are good...anything else is a sign of failure to be investigated? For instance you mention your car - I cannot imagine any hobbyist wanting to damage their car's engine just to collect some 'fault state' data image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yosoufe
    yosoufe over 4 years ago in reply to 14rhb

    14rhb I think this is called `Anomaly Detection` which is kind of unsupervised learning. You do not need a broken engine.

     

    Maybe this helps??


    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    I guess for this case you would need more than just vibrations of engine. You would need the gas pedal location, and maybe intake temperature and all kind of measurements of stuff that have effect on the performance of engine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 4 years ago in reply to yosoufe

    That it is.

    Unsupervised machine learning in cars is best ever idea for AI in industrial. For most middle-class car brand like BMW, Audi, Car-Net like CAN can provide signals like gas pedal location, temperature in heat dissipation, EPS, tyre pressure etc. There are specilized instrument for on-line analyse on fault.

    I think Tesla Model Y would be my next choice. With many intelligence settings.

    And I have received my new STM32H7A3, I only apply for the Kemet Vibration Sensor without board. Now, I think it time to use the same board as other experimenter have done.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fyaocn
    fyaocn over 4 years ago in reply to yosoufe

    That it is.

    Unsupervised machine learning in cars is best ever idea for AI in industrial. For most middle-class car brand like BMW, Audi, Car-Net like CAN can provide signals like gas pedal location, temperature in heat dissipation, EPS, tyre pressure etc. There are specilized instrument for on-line analyse on fault.

    I think Tesla Model Y would be my next choice. With many intelligence settings.

    And I have received my new STM32H7A3, I only apply for the Kemet Vibration Sensor without board. Now, I think it time to use the same board as other experimenter have done.