Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Blog Taming The Wild Stirling Engine
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
  • Author Author: dougw
  • Date Created: 24 Nov 2020 3:55 AM Date Created
  • Views 2965 views
  • Likes 13 likes
  • Comments 10 comments
  • doug wong
  • saga of tokin
  • winners
  • nanotron
  • stirling engine and vibration sensor
  • kemet vibration sensor
  • kemet
  • stirling engine
  • experimenting with vibration sensors
  • vibration
Related
Recommended

Taming The Wild Stirling Engine

dougw
dougw
24 Nov 2020

Introduction

Sensor technologies of all descriptions have intrigued me throughout my career. I have blogged about approximately 36 different sensor types on element14, but I have never used an industrial vibration sensor. I am really looking forward to trying out this Kemet vibration sensor and seeing what it can do.

To illustrate my interest in sensors, like vibration sensors, here is an example vibration sensing device I built for fun when I had a job working for a seismometer company. It looks like a miniature seismometer, but uses entirely different technology:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I was trying to make it very sensitive to ultra small but relatively quick motions of a desktop. This one is “de-tuned” a bit so it doesn't (usually) trigger when people walk by. It uses a simple brass disk with lead zirconate titanate (PZT) coated on one side. And a bit of a fancy circuit to stably boost sensitivity.

 

Kemet Vibration Sensor Experiments

For this experimentation challenge I will be performing some experiments to characterize the Kemet sensor so I can get a feel for its performance, but I also want to use it in a cool application. I will try to use interesting methods to keep the basic characterization tests entertaining and hopefully the main application I will explore is also interesting.

image

Sensor Frequency Response

I will be trying to characterize frequency response in a several ways:

  1. a variable tuning fork type of vibration (the output can be compared to what a microphone picks up at the same time)
  2. a sweep of vibration frequency - comparing excitation signal to sensor output at all frequencies in the time domain - and create a Bode plot
  3. I will also try to inject both white noise and pink noise to see what the results look like in the time domain as well as the frequency domain (using an FFT)
  4. I will also try injecting music into my drivers to see what the response will be to audio frequency vibrations, including trying to convert the samples from the sensor back into audio.

I have 2 different drivers I want to try, one is electromagnetic and the other is piezoelectric.

Some of these tests may highlight resonant frequencies in my test apparatus - we will see. (for sure the tuning fork experiment will showcase a resonant apparatus)

 

Resonant Frequency Exploration

I will try to excite the sensor's resonant frequency although the specs indicate this could be tough since it is way up in the ultrasonic range..

  1. I will try with the piezoelectric driver even though I doubt it can stimulate that high a frequency, even with square wave harmonics
  2. I will also try to stimulate resonance with an impulse impact

I don't expect too much from these experiments, since this is a strong suit of this sensor, but maybe I can confirm performance to some degree.

 

Sensor Sensitivity

I should easily be able to create small vibrations to subjectively explore sensitivity, however I am not sure yet how to quantify results. We will see what can be done.

 

The Wild Stirling Engine Problem

The application I want the vibration sensor to help with is a Stirling engine. Normally vibration isn't something you see, it is more like something you feel. The engine I have is highly unbalanced and it vibrates so violently that its whole chassis moves around on the table, even with rubber feet. This is a good visual and should make the videos less boring. I want to try different techniques to minimize vibration and stop it from wandering around. I will use the Kemet vibration sensor to quantify vibration with each mounting method and each balancing method to see which ones are practical and which ones do the best job of reducing unwanted motion. I don't just want to minimize vibration of the engine, I also want to minimize vibration of the table, so I will be using the vibration sensor on both the engine and the table.

Here is a quick video of my Stirling engine on the loose:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This machine is so wild, it cannot be left unattended.

 

This has been a quick introduction to me, my interest in this challenge and what I hope to tackle.

Check out the sequel episode where we get into some real tests, surprising results and the Taming of the Wild Stirling Engine in "The Saga of Tokin".

 

Relevant links:

The Saga of Tokin -  the sequel to this blog

Experimenting with Vibration Sensors: About the Competitionhttps://api.kemet.com/component-edge/download/specsheet/VS-BV203-B.pdf

VS-BV203-B_datasheet.pdf

Kemet website

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 5 years ago +7
    Hi Doug, One simple experiment would be to see if balancing the flywheel might help. You can do this by adding a small piece of solder at one spoke. Run the engine and see if it is better or worse. Move…
  • Andrew J
    Andrew J over 5 years ago +6
    That Stirling engine is a beautiful bit of kit - I could watch it for hours. Looking forward to the results of your experiments.
  • ajcc
    ajcc over 5 years ago +4
    Exciting stuff! Really curious to see your experiments and results with the vibration sensor. The Stirling engine is a nice visual demonstration indeed!
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Doug,

    One simple experiment would be to see if balancing the flywheel might help. You can do this by adding a small piece of solder at one spoke. Run the engine and see if it is better or worse. Move the solder piece to the next spoke and try again. When you find the spoke with the lowest vibration try adding a little more solder. If the vibration is worse try using a bit less solder. I have used this technique to trial balance machines that were used in the dental clinics that had too much vibration. Since the flywheel has the greatest mass it is most likely the major source of the vibration.

    John

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 5 years ago in reply to jw0752

    Reminds me of the technique of adding weights to car wheels to balance them, after having new tyres fitted. Of course, they put the wheel onto a machine which spins and identifies both the size of the weight and it's position on the wheel rim.

     

    Neil

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 5 years ago in reply to jw0752

    Reminds me of the technique of adding weights to car wheels to balance them, after having new tyres fitted. Of course, they put the wheel onto a machine which spins and identifies both the size of the weight and it's position on the wheel rim.

     

    Neil

    • Cancel
    • Vote Up +4 Vote Down