Experimenting with Vibration Sensors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Vibration Sensors
  • More
  • Cancel
Experimenting with Vibration Sensors
Forum How are you going to connect the sensor?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 7 subscribers
  • Views 2524 views
  • Users 0 members are here
Related

How are you going to connect the sensor?

neuromodulator
neuromodulator over 5 years ago

The only requirement for the "experimental design challenge" is to use the vibration sensor. How are you going to use it? I suppose most (if not everyone) will sample the analog signal, but what are you going to use to sample it? Are you going to use the provided STM32 MCU, a different MCU. a DAQ, or something else?

 

As of me I still haven't decided yet. I got a NI DAQ, a DMM with sampling capabilities and of course a bunch of MCUs and FPGAs. the NI DAQ is probably the easiest to use, its 200 ksps @ 16 bits. Then my DMM could sample up to 1msps @ 16 bits, but not continuously, or at much higher resolution but also a much slower speed. Then the provided STM32 can sample at up to 3.6 Msps @ 16 bits, (and eventually at higher speed through interleaving) but requires much more effort as it needs to be programmed.

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 5 years ago in reply to dougw +3
    Hi Doug, If you look on page 4 of the manual - the suggested connectors are SM03B-SRSS-TB or BM03B-SRSS-TB, these are surface mount PCB connectors. I think even if you found the cable connectors they would…
  • ralphjy
    ralphjy over 5 years ago +2
    The sensor spec indicates the frequency range is 15KHz and the measuring range is about 1V, so your NI DAQ has more than enough capability. I wish the spec had a frequency response curve but I guess that…
  • dougw
    dougw over 5 years ago +2
    I will hook it up this weekend and see what I can do with it. The first issue for me will be connecting to the tiny connector - I don't think I have a mating connector yet. It looks to be a 1mm pitch.…
Parents
  • ralphjy
    ralphjy over 5 years ago

    The sensor spec indicates the frequency range is 15KHz and the measuring range is about 1V, so your NI DAQ has more than enough capability.  I wish the spec had a frequency response curve but I guess that's something to be determined.  There's also no power supply sensitivity curve although the operating range is specified as 3-5.5V (I plan to use it at 3.3V).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 5 years ago

    The sensor spec indicates the frequency range is 15KHz and the measuring range is about 1V, so your NI DAQ has more than enough capability.  I wish the spec had a frequency response curve but I guess that's something to be determined.  There's also no power supply sensitivity curve although the operating range is specified as 3-5.5V (I plan to use it at 3.3V).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • neuromodulator
    neuromodulator over 5 years ago in reply to ralphjy

    Yes, but through oversampling you can reduce noise, so its not a bad idea to go for high sampling speed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to ralphjy

    I'm one of the judges so I have to be careful what I say but I think it's OK to point out that you can find a spec with frequency response here:

     

    https://www.kemet.com/en/us/sensors.html?t=931

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to michaelkellett

    Thanks.  I'm afraid I'm guilty of a case of not RTFM sufficiently.  I had downloaded that document and used parts of it already.  Appreciate that you pointed out that it had the frequency curve included.  I also missed the part about the resonant frequency being >30kHz.  I think I need new glasses image.

     

    Ralph