Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Waterproofing the RJ45 Connection
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 36 subscribers
  • Views 4387 views
  • Users 0 members are here
  • experimenting with Waterproof Connectors
  • waterproof rj45 backshell
Related

Waterproofing the RJ45 Connection

ralphjy
ralphjy over 3 years ago

I've been looking for a solution that would allow me to operate the RJ45 connection in a waterproof condition.  I had posted a question on the Amphenol Product Forum with hope that an Amphenol rep might be monitoring it.  shabaz  was nice enough to give me a quick reply.  I realized that I should have posted on this forum.

I think that I found the solution that that I was looking for, but I'd still like to verify that with a Product Specialist.  I asked charlieo21  for his contact.

I found an Amphenol IP67 connector backshell (basically a rubber boot) that is IP67 rated - IP67 Boot for our Harsh Environment products.

The one specifically for the RJ45 is this one - MUSBRAHD2241SK Connector Backshell, Hood, Amphenol Standard USB and RJ Plug Connectors, 180°, Rubber Body.

I wonder if rscasny  would be willing to supply these?

image

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 3 years ago +5
    I ordered 7 of these today that the MUSBRAHD2241SK from Newark. Thanks ralphjy for researching it. Randall
  • rscasny
    rscasny over 3 years ago +4
    We have started receiving the RJ45 connector hoods. So, we are sending them out as they come in.
  • shabaz
    shabaz over 3 years ago in reply to ralphjy +2
    Hi Ralph, The holes should not match with the socket holes if this part is fitted, because the two holes on the socket are for screwing to the enclosure. The holes on the cover also screw into the enclosure…
Parents
  • ralphjy
    ralphjy over 3 years ago

    Actually, I was sitting here looking at the panel connector and now I'm a bit concerned.  The picture in the post was from Digi-Key.

    Here is the view looking into the panel connector:

    image

    It seems like the screw holes in the backshell are in the wrong corners.

    Even more confusing is that here is the picture from Newark which has the interface piece flipped around - but the backshell holes also flipped?  There must be a removable piece on the end of the rubber backshell:

    image

    So, maybe a conversation with a Product Specialist is required.  I think this could be made to work.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to ralphjy

    Hi Ralph,

    The holes should not match with the socket holes if this part is fitted, because the two holes on the socket are for screwing to the enclosure. The holes on the cover also screw into the enclosure, but in two different holes, according to the diagram below. The diagram mentions clearance for "receptacle panel screw" which is for the screws for the RJ45 socket. I believe it doesn't interfere with the mounting of the socket, it covers the cable entry side if the enclosure or environment does not provide any other protection. 

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to ralphjy

    Hi Ralph,

    The holes should not match with the socket holes if this part is fitted, because the two holes on the socket are for screwing to the enclosure. The holes on the cover also screw into the enclosure, but in two different holes, according to the diagram below. The diagram mentions clearance for "receptacle panel screw" which is for the screws for the RJ45 socket. I believe it doesn't interfere with the mounting of the socket, it covers the cable entry side if the enclosure or environment does not provide any other protection. 

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ralphjy
    ralphjy over 3 years ago in reply to shabaz

    Yes, that makes sense.  I did not think about extra holes in the enclosure to mount the cable boot.  The picture from the Newark site confused me.

    If I think about this like PC D connectors mount  - I need standoffs on the enclosure side and thumbscrews on the boot.

    Thanks for pointing that out.