Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Tips on Writing the Final Summary Blog and Winning the Big Prizes
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 35 subscribers
  • Views 7070 views
  • Users 0 members are here
  • experimenting with Waterproof Connectors
Related

Tips on Writing the Final Summary Blog and Winning the Big Prizes

rscasny
rscasny over 3 years ago

Hi all participants.

The Experimenting with Waterproof Connectors is winding down with the final extra credit blogs due today.

On June 6th, I'll review the Forum participation and add points earned for each participant.

That leaves the big one task left to do: The Final Summary Blog.

The final summary blog is worth 300 points. I'll hand them over to the judges who will score them. Since I have two judges, I will average their individual scores into a final score and add them to the points earned for the rest of the blogs.

I wanted to offer some tips on writing the final summary blog.

1. The final blog should summarize all the work and experimenting you ghave done with waterproof connectors. Hence, a focus on the waterproof connectors should be prominent in the final blog.

2. The intro blog and the 5 extra credit blogs were added to the program for a specific reason: They can help you write the final blog (while adding points). Rather than simply linking these supplement blogs in the final blog, use the information they have to write a self-contained final blog. Now, if you want to add links to your intro/extracredit blogs in your discussion, that's fine. But our intention is to give the judges your final blog to grade your efforts.

3. The final blog should demonstrate the technical merit and your creativity around employing waterproof connectors in an electronics design. So, providing images, screenshots, and other media to lend to your tech finesse and creativity should be utilized.

4. Beyond the waterproof connectors, we provided the latte panda SBC in the kit. Show the reader how you used it, how you prepared it, and how you connected it to the waterproof connectors.

5. Articulate what your experiments were and how they turned out.

6. Draw some conclusions about participating in this program. They can range from what you may have learned about waterproofing an electronics design to what the successes and challenges were.

7. Make sure your final blog flows with some logical structure. The judges are going to read it for the first time. They want so see not only what you did but how your experiments evolved. Of course, this depends on what you did.

Like I said, the final summary blog is worth 300 points. We want the final blog to be an authoritative document. The more comprehensive it is, the closer it will get to the 300 points.

Good luck.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago in reply to shabaz +4
    I use MS Word too - but I don't strip the formatting. I find that you can easily use styles (e.g. Heading 2, 3), bullet-points, bold/italics and they will transfer right over with no hassle. Just don…
  • michaelkellett
    michaelkellett over 3 years ago in reply to Gough Lui +3
    My method is very similar to this except that I don't do quite so much formatting in the Word document. I would much rather use a non Microsoft tool but when I tried Libre Office it was fine except for…
  • rscasny
    rscasny over 3 years ago +3
    I see that there have been some great suggestions regarding approaches to writing the final blog. Just to recap: The final blog should not simply be a table of contents to linked blogs you have produced…
Parents
  • misaz
    misaz over 3 years ago

    What is the recommended length?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to misaz

    I have the same dilemma - if I wanted to put all/most of  the information from blog posts into final post (to make it very detailed, standalone work) it will be long and heavy, possibly difficult to read (with all the screenshots and photos) - but from the above guidance I suspect that if I post only most important points from already published work (with references to the more detailed texts), supplemented with experiment results and conclusions  it could be unfavorably scored...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to JWx
    rscasny said:
    The more comprehensive it is, the closer it will get
    JWx said:
    it will be long and heavy, possibly difficult to read

    Being comprehensive and 'long and heavy' are often one and the same.

    I've never known anyone entering competitions on the Community be penalised for providing too much valuable information about what they've done, it's very easy to instead penalise for not providing enough.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to JWx

    JwX--In the past, some participants sometimes wrote separate blogs and linked all of these blogs (in some cases it was 12 or 15 blogs) to the final blog, which acted like a table of contents. My suggestion is to include those blogs in a references section. But the main discussion should be in the final blog. Well, you are concerned with it being long and heavy. But short and light isn't probably a winning strategy either. If you have a lot of screenshots and photos then you need to probably make some compromise of what to include or exclude. With regard to your "unfavorably scored" comment. The judges are getting your final blog. Just so long as it has a logical flow, makes sense and demonstrates technical merit and creativity, I don't see you being penalized. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 3 years ago in reply to JWx

    JwX--In the past, some participants sometimes wrote separate blogs and linked all of these blogs (in some cases it was 12 or 15 blogs) to the final blog, which acted like a table of contents. My suggestion is to include those blogs in a references section. But the main discussion should be in the final blog. Well, you are concerned with it being long and heavy. But short and light isn't probably a winning strategy either. If you have a lot of screenshots and photos then you need to probably make some compromise of what to include or exclude. With regard to your "unfavorably scored" comment. The judges are getting your final blog. Just so long as it has a logical flow, makes sense and demonstrates technical merit and creativity, I don't see you being penalized. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • JWx
    JWx over 3 years ago in reply to rscasny

    thank you (and cstanton) for clarification - I will go with aggregating most of the information into final blog route (maybe without most of the console output - it takes more space that is providing information)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to JWx
    JWx said:
    (maybe without most of the console output - it takes more space that is providing information)

    You can always upload files as either attachments or into the 'files' media gallery and link to them if you don't want to miss anything out.