EZ-EV Challenge
  • Challenges & Projects
  • Design Challenges
  • EZ-EV Challenge
  • More
  • Cancel
EZ-EV Challenge
Forum Vape Cell EV - part II - RS485 comms
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join EZ-EV Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 58 subscribers
  • Views 131 views
  • Users 0 members are here
  • ADM3068E
  • EVAL–ADM3068EEBZ
  • rs-485
  • uno q
Related

Vape Cell EV - part II - RS485 comms

saramic
saramic 2 months ago

I have been out on a few unplanned mid-winter trips (Southern Hemisphere here ) away from home which has put a huge deficit in my ability to deliver. Secondly I have been scratching my head watching a bunch of online videos mentioning how people have burnt their house down charging lithium batteries, let alone unlabelled ones from vapes. Also a bunch of contradictory advice on when to use a BMS (Battery Management System) and how to build one. For today I want to focus on the Design Challenge kit I was lucky to receive, and getting RS-485 up and running between 2 Arduino UNO Q’s using the EVAL-ADM3068EEBZ Evaluation Board.

Recap

Vape Cell EV is the idea of a smart cell charging system that can handle cells with unknown histories, charging, power distribution, any safety issues and ultimately if a cell should be removed from a battery of many cells.

  • Vape Cell EV - part I - What’s in a Vape

The Design Challenge Kit

The design challenge kit is made up of 2 UNO Q’s, Arduino module with a docker capable MPU attached, an evaluation board for the ADM3068E RS-485 Transceiver capable of 50 Mbps, some Molex connectors, access to LabView, some cool stickers and a metal Element 14 pin.
image

I must say I am not much of a fan of the stickers but a pin is exactly the kind of identification you need in a crowd.

image

Analog Devices EVAL-ADM3068EEBZ RS485 transceiver

The Analog Devices EVAL-ADM3068EEBZ is a small breakout board for the ADM3068E RS485 transceiver. It has screw terminals for power, data and bus signals and is rated 50 Mbps. Worth mentioning that this figure seems to be based on a measurement at the transceiver’s own pins, essentially zero cable — a bench loopback number, not a claim about what survives a real cable run.

RS485 is differential — data is the voltage difference between two wires, not one wire against ground — and that’s why the cable has to be a twisted pair specifically. The twist is what gives common-mode noise rejection and keeps the pair’s impedance consistent enough to match the 120 Ω termination resistors on the board. The classic rate-vs-distance rule of thumb (10 Mbps at ~12 m, 1 Mbps at ~120 m, 100 kbps at up to ~1200 m) is worth keeping in mind, even though I’m not yet sure exactly where RS485 will end up being used on my cell monitor — I’m fairly confident none of these distances or speeds will actually be needed.

Which jumpers, though

The eval board has seven jumpers (LK1–LK7) controlling driver/receiver enable, half- vs full-duplex wiring, and termination. Table 1 in the datasheet lays it all out, but in fairly technical terms — it took me a while to fully understand what each jumper actually did, and a few of them got plugged in by gut feel.

The board ships configured for its own bench self-test: LK1=B (receiver always on), LK2=A (driver always on). That turned out to be genuinely useful: with LK4/LK6 inserted (folding the chip’s full-duplex A/B/Y/Z pins into one half-duplex pair), the factory jumpers already give you a single-board loopback test for free — the same idea as a CAN controller’s internal loopback mode which I explored in my previous project Green Brain - Part I - CAN bus introduction. Whatever goes out DI comes straight back on RO, no second board or cable required. Good for smoke testing the sketch’s framing and checksum logic before anything else is wired up.

I attempted to get half-duplex control working, which needs LK1=D, LK2=C — tying the driver enable (DE) and receiver enable (RE̅, active-low) together onto one control line, so a single GPIO can flip the whole board between transmit and receive. I got led astray for a while by some MCU (Micro Controller Unit) / MPU (Micro Processor Unit) interop quirks in Zephyr, which had me convinced this wasn’t working as expected.

An echo test that barely touched the board

The single-board loopback test worked nicely once the sketch’s UART code was right (more on that below) — but in hindsight it barely exercised anything RS485-specific. Driver and receiver were both hard-wired permanently on; there was no direction switching, no real bus, no second board’s independent clock. Moving to the actual two-node config (LK1=D, LK2=C, a twisted pair between two separate boards) immediately surfaced problems the echo test had no way of catching — which led me down the goose chase of the direction-control wire mentioned above, and a forgotten ground wire between the two boards’ RS485 sides. Neither would have mattered for a board looping back to itself.

When two boards refuse to talk

First symptom: total silence, on both boards, at every baud. Turned out my naive idea of sweeping baud rates on a timer was the culprit:

int idx = (int)((millis() / STEP_MS) % NUM_BAUDS);

millis() counts from each board’s own power-on, so two independently started boards drift out of phase almost immediately — over a 28-second full sweep they can end up spending the whole test on different baud rates from each other. Fix: pin both boards to a single fixed baud rate before attempting to sweep across multiple speeds.

Still silence after that — after a bunch of wire changes, including the direction-control wire, the symptom finally changed from silence to garbage: real activity on the bus, but corrupted frames and a fast-climbing error count. To rule the transceiver out entirely, the next step was a direct crossover — UNO Q D1 straight to the other UNO Q’s D0 and back, no eval board in the loop at all:

  • Node A D1 (TX) → Node B D0 (RX)
  • Node A D0 (RX) ← Node B D1 (TX)
  • shared GND between the two boards

This should have been plain old UART between two boards — I’d even written up a simple example in a comment on my recent Smart Security and Surveillance Sentinel Box forum post. Instead, I got the same corruption. That single test ruled out the transceiver, the jumpers, and the bus wiring all at once — whatever was wrong was in the MCU/software layer, not the RS485 hardware.

Back to the UART — the Serial trap

The sketch had been writing to Serial, same as any Arduino sketch would. On real hardware, that hit a build error deep into an unrelated change:

error: 'class BridgeMonitor<>' has no member named 'end'

Serial on the UNO Q, it turns out, isn’t the physical UART at all once Arduino_RouterBridge.h is included. This is one of the recurring confusions of working across an MPU and an MCU — which one actually owns the pins, and which “serial” you’re really talking to. In this case it turned out to be the internal Bridge/Monitor channel used for debug printing:

// Arduino_RouterBridge/src/monitor.h
extern BridgeMonitor<> Serial;   // aliased to the same object as Monitor

Zephyr bit me again here — I’d run into similar MCU/MPU quirks before in Green Brain - Part II - Dev setup and had mostly learned to live with them. The fix was to skip the Arduino Serial/Stream wrapper and talk to the STM32’s usart1 peripheral directly through Zephyr’s own UART driver API:

#include <zephyr/drivers/uart.h>
static const struct device* rs485_dev = DEVICE_DT_GET(DT_NODELABEL(usart1));
// uart_configure(rs485_dev, &cfg)   — set baud at runtime
// uart_poll_out(rs485_dev, byte)    — blocking single-byte write
// uart_poll_in(rs485_dev, &byte)    — non-blocking single-byte read

The buffer that wasn’t there

With real hardware access sorted, a byte counter told the next story: the same-board loopback test was receiving exactly 2 bytes back for every 23-byte frame sent, every single time, regardless of baud. That precision ruled out noise and pointed at something structural — this UART has almost no receive buffering in polling mode, just a ~2-byte pipeline (shift register plus holding register). The original code wrote a whole frame in one blocking loop before ever checking for incoming bytes; on a looped-back wire the echo starts arriving while still transmitting, and without draining it concurrently, everything past the first couple of bytes was lost to overrun. Interleaving the write with polling reads fixed the same-board test cleanly.

Cross-board traffic, though, stayed badly corrupted even at a generous 9600 baud — a rate that should have made timing-related errors rare. The clue came from an old, unrelated UART proof-of-concept in Smart Security and Surveillance Sentinel Box forum post, on completely different hardware, whose own comment explained why it just worked:

// TMR_Delay is blocking for TICK_MS but the hardware RX FIFO
// (32 bytes) holds incoming bytes while we wait.

That MCU has a real 32-byte hardware FIFO. Ours has essentially none, and Zephyr — unlike that PoC’s bare-metal loop — is a genuine preemptive RTOS. Our loop() can be paused by other threads (the Bridge/RPC channel, USB, kernel housekeeping) for however long the scheduler decides, and with only a 2-byte cushion behind it, any such pause silently drops data no matter how carefully the polling loop is written. That’s a fundamentally different problem from “the baud rate is too high.”

The real fix was getting reception off the polling loop entirely — a proper interrupt handler draining the peripheral into a ring buffer the instant a byte arrives, independent of whatever the main loop happens to be doing:

static void rs485Isr(const struct device* dev, void* user_data) {
    while (uart_irq_update(dev) && uart_irq_rx_ready(dev)) {
        uint8_t b;
        while (uart_fifo_read(dev, &b, 1) == 1) {
            // push b into a ring buffer
        }
    }
}
// in setup():
uart_irq_callback_user_data_set(rs485_dev, rs485Isr, NULL);
uart_irq_rx_enable(rs485_dev);

The difference was immediate: the receiving board’s error count went from climbing continuously to 8 total (a brief startup transient) then flat zero across the next ~490 clean frames.

Timing budgets that don’t scale with baud

A smaller, satisfying bug fell out right behind the buffer fix: the fixed 50 ms reply timeout didn’t scale with baud. At 9600 baud a bare 23-byte round trip already takes ~48 ms on its own, leaving almost no slack for the other board’s own turnaround — late replies were routinely missing the deadline and landing during the next round instead, silently miscounted rather than just timed out. Scaled the timeout to 5× the theoretical round trip at the current baud, and it cleared up at 9600.

It came back once bauds got extreme, just from the opposite direction. At 3,000,000 baud, a chunk of replies kept landing as mismatched rather than timed out — same symptom, different cause this time. The 5×-round-trip formula assumes overhead shrinks along with wire time, but the other board’s own turnaround (sync detection, checksum, flipping the transceiver direction, ordinary scheduler jitter) costs roughly the same wall-clock time no matter the baud — trivial next to 48 ms at 9600 baud, the dominant cost once wire time itself drops to ~150 µs at 3 Mbaud. Added a flat 5 ms floor on top of the scaled portion and that gap closed too. Two different bugs, same underlying lesson: a timing budget derived purely from bit-time doesn’t account for the parts of the round trip that don’t shrink with it.

A wiring mix-up, and a way to test a driver with just a multimeter

Wiring the real two-board bus (as opposed to the single-board loopback above) turned up one more of the “forgotten/misremembered wire” family: the UNO Q’s D0 and D2 pins got swapped on one board — RO (the transceiver’s data output) ended up wired to D2, the direction-control pin, instead of D0, the real hardware UART’s receive pin. Software has no way to notice this: D2 is just a GPIO the sketch actively drives, so it was fighting the transceiver’s own output on that pin the whole time, while the STM32’s real UART receiver sat on a disconnected, floating D0.

With no oscilloscope on hand, the multimeter still settled a real question: was a driver’s signal weak or was it not there at all? A rapidly-toggling half-duplex signal only pulses “on” for a fraction of each round, so a plain DC meter, which effectively averages what it sees, reads a small fraction of the true swing even on a perfectly healthy line — 0.07–0.1 V measured this way is not the same claim as “the driver only makes 0.1 V.” Trick: force the driver into a steady state instead of a fast pulse, so the meter has something constant to read. Jumper the direction-control pin straight to 3V3 (driver permanently enabled, bypassing the MCU), disconnect the data input so nothing’s toggling it, then read across A/B. A healthy driver holds a steady 2–5 V that way; this one read 2.2–2.4 V, confirming the transceiver and its enable wiring were both fine — the fault really was the D0/D2 swap, not the chip.

The vanishing frame

With the wiring fixed, most frames arrived clean — but a fraction still failed, and only ever the same way: a complete, checksum-_invalid_ frame, every field correct except the very last byte. Random noise doesn’t behave like that; noise-corrupted bytes should be unpredictable, not the same wrong value every time. A raw hex dump (every byte of the frame, not just the derived pass/fail) confirmed it precisely:

raw: A5 00 00 00 00 10 00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F A5

sync, the 4-byte sequence number, len, all 16 payload bytes — every one matched (seq+i) mod 256 exactly. Only the final byte was wrong, and it was wrong in a very specific way: it always read back as 0xA5 — the sync byte, not a checksum. Dumping the transmit side too (bytes about to go out, not what came back) showed why: the sender was transmitting every sequence number in order, but the receiver only ever logged the even ones. Odd frames vanished completely — not corrupted, just gone. The receiver’s checksum slot for frame N was silently being filled by frame N+1’s real sync byte, and the rest of frame N+1 got scanned through as noise looking for the next sync match.

Root cause: the delay before dropping the transceiver’s drive-enable line assumed 10 bit-times of margin was enough — one byte period — for the last byte to finish shifting out. It isn’t. The UART call used to write that byte only guarantees it moved into the transmit register once the previous byte vacated it — not that the previous byte finished transmitting. Worst case, the byte before the checksum can still have a full bit-time left to go, and the checksum byte itself hasn’t started: two byte periods needed, not one. That mismatch was exactly big enough to reliably clip the last byte’s transmission every single time — not occasionally, which is what made the “always exactly 0xA5” signature so recognisable once dumped raw. Doubling the margin fixed it outright: 100% clean, zero errors, hundreds of frames straight.

Teaching the boards to run the sweep themselves

With a fully clean 9600-baud link finally confirmed, it was worth rebuilding the automatic baud sweep — properly this time. The first attempt (mentioned above) swept bauds on a free-running timer and fell apart because two independently-booted boards’ clocks drift apart with nothing to re-anchor them. The fix: make 9600 a permanent “home” baud that’s proven reliable enough to carry its own handshake.

  • One side sends a control frame — the same 23-byte frame format, told apart only by a different leading byte (0x5A instead of 0xA5), reusing every bit of the already-debugged build/checksum/echo code.
  • The other side echoes it back as an acknowledgement — again, the exact same mechanism already used for ordinary data frames — and only then switches its own baud rate.

First attempt at the control frame was just a bare pulse meaning “advance to your next rate,” relying on both boards independently counting their own position through the same compiled-in list. That worked fine until a board got restarted on its own (once autostart-on-boot was wired up) — its counter reset to zero while the other board’s didn’t, so the pulse still succeeded every time, each side just quietly advanced to a different rate. Fix: send the actual target baud — the real number, e.g. 115200, packed as a 4-byte value straight into the control frame’s payload — instead of an index/offset into the shared list. One side is now the sole authority and the other just applies whatever number it’s handed, with no shared table position to keep in sync at all.

  • Reverting back to 9600 needs no handshake at all — each side just counts down a short local timer (a few seconds) from the moment it entered the test baud, then reverts on its own. That only requires the two sides to enter the test baud within about one handshake round trip of each other, not to stay in sync for an entire run — so drift can never accumulate past a single short cycle, which is what actually broke the original design.

Where things stand

RS485 itself never turned out to be the problem — every wrong turn along the way was a jumper misunderstanding, a forgotten wire, or a software assumption two or three layers removed from the bus itself. The pattern that got through each one was the same: isolate ruthlessly (a bare wire loop instead of the transceiver, a direct crossover instead of the bus, a forced steady-state instead of a fast pulse for the multimeter), don’t trust an API name at face value (Serial wasn’t Serial), and let a raw byte dump settle an argument that theorising alone kept getting wrong.

With the auto-sweep running end to end, here’s the actual reliability curve across a real two-node bus — twisted pair, real transceivers, real half-duplex turnaround — not a self-loop bench test and not a datasheet figure:

Baud Success rate Round trip
9600 ~96–100% ~48 ms
19200 – 460800 ~98–100% scales with bit-time
921600 ~91% ~1.3 ms
1,000,000 ~95% ~1.4 ms
2,000,000 ~83.5% ~1.2 ms
3,000,000 ~60% ~1.1 ms

Clean and reliable from 9600 all the way through 460800 baud. Real, gradual degradation starts around 921,600–1,000,000, and gets substantial by 2–3 Mbaud. Round trip time tracks bit-time almost exactly at every rate, with no artificial timeout ceiling distorting it anymore — this is the genuine electrical/timing ceiling, not a software one, and it’s a believable curve: nowhere near the 50 Mbps bench figure, but comfortably enough for a cell-monitor poll bus running well under 1 Mbaud.

image

The video below shows 2 UNO Q’s connected to the ADM3068E eval board. The RS-485 boards are connected with a twisted pair. The screen displays an overkill display hosted on one of the UNO Q’s. At the top is the NODE, and anothr node connected. In the middle is the radar like view of the topology of the network, in this case a primary and a secondary. At the bottom are the logs of the various baud speeds being tested and a graph on the bottom right shows the link quality.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Next

  • onto the batteries and charging them, I think I have the necessary knowledge and courage to proceed safely.

Source

https://github.com/saramic/vape-cell-EV