Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Electricaly controled mechanical device needed
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 10 subscribers
  • Views 3510 views
  • Users 0 members are here
  • Design
Related

Electricaly controled mechanical device needed

inception007
inception007 over 10 years ago

Any available device that can control water flow in pipe ( by allowing or blocking pipe ) when triggered  with electrical signal.?@

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    100% Brand new and high quality

    Model:2W-025-08

    Working Medium: Air, Water, Oil

    Operating Method: Direct action

    Type: Normal Closed

    Flow bore: 2mm

    Pipe Size: 1/4"

    Working Pressure:  0.15~0.8Mpa

    Max Pressure:1.0Mpa

    Working Temperature: -5~60℃

    Voltage: DC 12V

    Material: Brass

    What other operating methods are there?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    100% Brand new and high quality

    Model:2W-025-08

    Working Medium: Air, Water, Oil

    Operating Method: Direct action

    Type: Normal Closed

    Flow bore: 2mm

    Pipe Size: 1/4"

    Working Pressure:  0.15~0.8Mpa

    Max Pressure:1.0Mpa

    Working Temperature: -5~60℃

    Voltage: DC 12V

    Material: Brass

    What other operating methods are there?

    Clem