Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum active weigh ing of cable drum
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 2382 views
  • Users 0 members are here
Related

active weigh ing of cable drum

malcolm51
malcolm51 over 6 years ago

this ought to be easy but my brain doesn't seem to be working.......

 

problem.... a drum of wire or filament etc is mounted on a shaft (axle) supported at both ends........... what is the best way to continuously weigh and display its weight, in grams, as te contents are used?

 

weighing one end is simple but for an accurate reading both ends must be weighed at the same time for a single indication of weight.

 

solution could be electronics or arduino or raspberry pi

 

please help prevent me going nuts.....

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    0 Workshopshed over 6 years ago

    You should find that the force on one end is half the total force, assuming that the spool is in the middle of the bar. So take a measurement and double it.

     

    https://www.engineeringtoolbox.com/levers-d_1304.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 6 years ago

    You should find that the force on one end is half the total force, assuming that the spool is in the middle of the bar. So take a measurement and double it.

     

    https://www.engineeringtoolbox.com/levers-d_1304.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Workshopshed

    That would only work if there were no motion constraint other than vertical at the non-load cell end, and everything in balance - difficult to achieve in practice.

     

    With a 1kg (or 5kg) load cell costing about £2 complete with amplifier it's not expensive to use 2.

     

    https://www.aliexpress.com/item/32945697076.html?spm=a2g0o.productlist.0.0.45534de7ogUpBl&algo_pvid=5e51702b-1a78-41ae-a267-e2b8ad40df8d&algo_expid=5e51702b-1a78-41ae-a267-e2b8ad40df8d-12&btsid=1a95fd43-d715-4d97-b15f-ac411b7c89d3&ws_ab_test=searchweb0_0,searchweb201602_7,searchweb201603_53

     

    MK