Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum active weigh ing of cable drum
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 2381 views
  • Users 0 members are here
Related

active weigh ing of cable drum

malcolm51
malcolm51 over 6 years ago

this ought to be easy but my brain doesn't seem to be working.......

 

problem.... a drum of wire or filament etc is mounted on a shaft (axle) supported at both ends........... what is the best way to continuously weigh and display its weight, in grams, as te contents are used?

 

weighing one end is simple but for an accurate reading both ends must be weighed at the same time for a single indication of weight.

 

solution could be electronics or arduino or raspberry pi

 

please help prevent me going nuts.....

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Workshopshed

    That would only work if there were no motion constraint other than vertical at the non-load cell end, and everything in balance - difficult to achieve in practice.

     

    With a 1kg (or 5kg) load cell costing about £2 complete with amplifier it's not expensive to use 2.

     

    https://www.aliexpress.com/item/32945697076.html?spm=a2g0o.productlist.0.0.45534de7ogUpBl&algo_pvid=5e51702b-1a78-41ae-a267-e2b8ad40df8d&algo_expid=5e51702b-1a78-41ae-a267-e2b8ad40df8d-12&btsid=1a95fd43-d715-4d97-b15f-ac411b7c89d3&ws_ab_test=searchweb0_0,searchweb201602_7,searchweb201603_53

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • malcolm51
    0 malcolm51 over 6 years ago

    Thanks for the help

     

    Now to get on with it

     

    malcolm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 6 years ago

    You should find that the force on one end is half the total force, assuming that the spool is in the middle of the bar. So take a measurement and double it.

     

    https://www.engineeringtoolbox.com/levers-d_1304.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to malcolm51

    Connecting 2 load sensors in series is not possible, connecting load cells in parallel is sometimes done but not a good idea.

    The best way is to give each load cell its own amplifier and use multiple ADC inputs.

     

    Here's an article on E14 that should give you some ideas:

     

    3d printer filament roll holder and monitor for Arduino

     

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • malcolm51
    0 malcolm51 over 6 years ago in reply to michaelkellett

    sorry for lack of detail

     

    load axle/ spindle rests on 2 supports, one each end, and a yoke is not practical

     

    weight range 50g to 2kg

     

    as an example this could be a roll of 3d print filament.

     

    tension is zero.... weighed at rest point and/or continuous reading (varying with tension/ rest) displayed on 7seg display or (more likely) a TFT display attached to arduino or pi.

     

    low budget... reasonable accuracy e.g +- 5g at rest zero tension.... environment closed acrylic case with steady temperature and airflow (no outside forces...

     

    hope this helps......

     

    can 2 load sensors be connected in series to give single reading of entire load (both ends added together)

     

    unfortunately was in R&D but brain fried with excessive age (and little experience of arduino/ pi)...

     

    malcolm

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago

    You don't give enough context to give a good answer - it would be good to know how big and heavy the drum is, what's the tension in the wire, how is it all controlled and a load more stuff (environment, accuracy required, budget etc.)

     

    The very simplest way to do it is to hang the drum from a yoke attached to a single load cell - you can buy these easily enough but your talk of Arduino or RPi suggests you may not be in the classic load cell price range. If you are not too fussy you could buy cheap load cells from China.

     

    If the drum is heavy and rotates fast or the wire tension is significant it might get harder, maybe use load cells to support each end of the drum and if necessary sample the weight (or more correctly down-force)  multiple times per revolution.

     

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer