Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RDM3600 RFID COMPONENT
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 8 subscribers
  • Views 4841 views
  • Users 0 members are here
Related

RDM3600 RFID COMPONENT

e14 Contributor
e14 Contributor over 11 years ago

I have been using the Arduino platform for a while now(about 6 months) and I tried to hook up the RDM3600 RFID reader to my Arduino Uno and it seems like the reader does not communicate with the board. I present a card, but the serial interface does not display a serial number or anything. I am following this tutorial:

 

http://tronixstuff.com/2013/11/19/arduino-tutorials-chapter-15-rfid/

 

I modified the code to get an indication that the setup was complete:

 

#include <SoftwareSerial.h>

 

SoftwareSerial RFID(2, 3);

 

int i;

 

void setup()

{

  RFID.begin(9600);

  Serial.begin(9600);

  Serial.println("ready");

}

 

void loop()

{

  if (RFID.available() > 0)

  {

    i=RFID.read();

    Serial.print(i, DEC);

    Serial.println(" next");

  }

}

 

 

 

Does anyone have any idea why I don't get any communication from the RDM3600 when I present a RFID tag.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    #include <SoftwareSerial.h>

     

     

     

    SoftwareSerial RFID(3, 4);

     

     

     

    int i;

     

     

     

    void setup()

     

    {

     

      RFID.begin(9600);

     

      Serial.begin(9600);

     

      Serial.println("ready");

     

    }

     

     

     

    void loop()

     

    {

     

      if (RFID.available() > 0)

     

      {

     

        i=RFID.read();

     

        Serial.print(i, DEC);

     

        Serial.println(" next");

     

         }

     

      }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    can you post your current code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    I jumpered pin 3 and pin one together and I sent a value via the serial monitor, but it was not received/displayed on the serial monitor. Does this mean there is a problem with the Arduino Uno?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Try linking Pin 1 to Pin 3. Sending a value from the serial monitor should send a value into Pin 3 to be displayed on the serial monitor output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    I have tried this configuration with the same results. It seems like I'm not getting any communication from the RDM3600 board. Is there a way I can test the Rx pin on the Arduino Uno?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Looking at your wiring it seems you are putting your power pins in a different place to that shown on the guide you linked to.

    Arduino_RFID_reader_setup.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I have switched the Rx and Tx pins, in addition to adding the LED function changing digital input pins on the Arduino Uno. I have also bought another RDM6300 board and tried a different Arduino board. Nothing seems to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gadget.iom

    Here is a picture. Just power, ground, and a jumper to pin 3 on the Arduino Uno and the antenna that came with the RDM3600. I modified the code to change the RX and TX pins to 3 and 4:

     

    #include <SoftwareSerial.h>

     

    SoftwareSerial RFID(3, 4);

     

    int i;

     

    void setup()

    {

      RFID.begin(9600);

      Serial.begin(9600);

      Serial.println("ready");

    }

     

    void loop()

    {

      if (RFID.available() > 0)

      {

        i=RFID.read();

        Serial.print(i, DEC);

        Serial.println(" next");

         }

      }

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago

    These issues are often causes by the simple things. image

    Have you tried swapping the TX/RX pins around?

     

    Can you take a photo or sketch out your connections between the RFID reader and the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<