Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking Feedback on ADDITIONAL Parts -- Experimenting with Waterproof Connectors
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 9 subscribers
  • Views 2096 views
  • Users 0 members are here
  • Seeking Feedback on ADDITIONAL Parts -- Experimenting with Waterproof Connectors
Related

Seeking Feedback on ADDITIONAL Parts -- Experimenting with Waterproof Connectors

rscasny
rscasny over 4 years ago

Since I last wrote about the Experimenting with Waterproof Connectors program I will be launching soon, we have been discussing what to include in the kit for this program. My original post described the program. My updated post spelled out what I wanted to include in the kit.

This post is seeking feedback on additional parts to include in the kit. They are:

132245
RF / Coaxial Connector, SMA Coaxial, Right Angle Bulkhead Jack, Crimp, 50 ohm, RG174, RG188A, RG316
image
242125-10
RF / Coaxial Adapter, N, Jack, SMA, Jack, Straight Adapter, 50 ohm
image
AD-SMAJMCXJ-1 AD-SMAJMCXJ-1
RF / Coaxial Adapter, SMA, Jack, MCX, Jack, Straight Bulkhead Adapter, 50 ohm
image
122192-15
RF / Coaxial Connector, TNC Coaxial, Straight Bulkhead Jack, Crimp, 50 ohm, RG174, RG316U
image
336209-13-0250
RF / Coaxial Cable Assembly, 90° AMC Plug to TNC Bulkhead Jack, 1.32mm, 50 ohm, 9.84 ", 250 mm
image

  • Sign in to reply
  • Cancel
  • Gough Lui
    0 Gough Lui over 4 years ago

    I'm more of an N-connector person myself - those are pretty chunky and robust connectors, great to use for long-life, high-cycle applications e.g. on spectrum analysers.

    SMA may be my next preference but the top one seems to be a crimp type which will need special tooling. BNC is pretty useful too, but again, seems to be a crimp type.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 4 years ago in reply to shabaz

    I do have some N connectors and maybe even a cable, just no instruments that use them. I doubt I will use them for my LoRa system. Relaxed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to neuromodulator

    Also N is really common for outdoor antenna cabling, although it all tends to be $$$.

    The N is also great for interfacing to really fat coax : ) 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neuromodulator
    0 neuromodulator over 4 years ago in reply to dougw

    A spectrum analyzer. Type N appear to be more or less standard for RF test equipment that's on the low GHz. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 4 years ago in reply to neuromodulator

    N connectors definitely work great, although I have nothing that uses them - What do you have that uses them?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neuromodulator
    0 neuromodulator over 4 years ago

    I like Type N, which are kind of like TNC but larger and very robust. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 4 years ago

    Gee, I had this cute project all worked out to utilize the updated list. It didn't need an RF connector. Relaxed

    I dunno, I think as shabaz points out it would be easier to cablize the TNC and it translates naturally to a BNC on the other end, which connects to a lot of instruments.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago

    Hi Randall,

    I reckon the second and last ones (242125-10 and 336209-13-0250) are the most preferred from this choice, because they do not require the user to crimp their own cables (it requires kit that often users will not have access to). The 336209-13-0250 product has an AMC connector which is apparently similar to u.FL connectors, and they are fairly common too, as are SMA (which 242125-10 can connect to).
    Probably 242125-10 is slightly more convenient, because there are many cables with SMA connector at one end, and whatever required connector for the development board at the other end.

    MCX is not that popular from what I have seen, but although this is a not an insurmountable problem (since there will be adapter cables out there to go from MCX to say SMA) the choices may be fewer, so it is less flexible.

    TNC is a nice choice because there are lots of adaptors out there. SMA would be a very good choice for the external interface for indoor equipment, but TNC is a bit more rugged, and probably more common for outdoor use.

    Unfortunately, no matter what part is chosen for the kit, to use the part, some adaptation cable could be needed which will be specific to the dev-board or whatever that it will be connected to, and to external coax or antennas. The user may need to specify what adapter cable they need : (