Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your opinion about an Experimenting with Flat Flexible Cables
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3219 views
  • Users 0 members are here
  • molex
  • community survey
  • experimenting challenge
Related

Seeking your opinion about an Experimenting with Flat Flexible Cables

rscasny
rscasny over 3 years ago

imageLaunching an Experimenting Challenge can be a lengthy process. In general, we have a lot of meetings with the sponsor and a lot of brainstorming within the element14 team. Even choosing the prizes takes some time, with back and forth between us. Perhaps the thing that takes the most time is choosing the products. Sometimes I suggest products that I think will will work. Other times it's a collaboration between element14 and the sponsor. And sometimes we choose a product because it's something new; a good example of that is gesture sensors.

Recently, we were approached by a sponsor who makes flat flexible cables (FFCs) and would like to see element14 members experiment with them. There is a growing use of them, especially for space-constrained electronic sub-assemblies. And some of these FFCs have special characteristics such as EMI protection, hi temp environments, low voltage differential for signal integrity, impedance matching, and so on.

But designing an Experimenting Challenge means building the activity, the kit, and the experiments. That's where I like to ask community members. At face value, offering an Experimenting Challenge with FFCs seems like a hill to climb. Do we just send a kit of FFC's to the participants and see what they do? Or do we add in some other products to fill out the kit. (I did this with the Experimenting with Waterproof Connectors Challenge by adding a imageDFRobot SBC.) Of course, the more specific we get, the more specific (circuit count, length, & pitch, for instance) the FFCs would need to be.

But right now, I would like to toss around some ideas of how we could frame an Experimenting Challenge with FFCs. What should be in the kit? Types of experiments? Even, the kinds of prizes you would like to see for this activity. For myself, I see FFCs as a product we haven't talked about that much, but complements a lot of different kinds of electronics. I suspect that a lot of creative content and blogs could be created for this kind of activity.

Here are some relevant links:

Webpage

Essentials

If you have any thoughts about an Experimenting with FFCs challenge, I invite you to write a comment below.

Some polls

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    This is probably going to be quite challenging to pull off. For one, the best use of FFCs are for board-to-board connections which necessitates the design of PCBs and soldering of surface mount connections which clamp onto the FFC (at least most of the time). There are some broad-pitch FFCs which can be used with crimp connections, but these are probably not being demonstrated. Note that hot-air soldering of FFC connections from the top is likely to be an exercise in futility - you are very likely to melt the plastic due to temperature issues ... but from the underside may be possible.

    If the key is to demonstrate high-speed connectivity, the test of a good connection requires not only a VNA but suitable test fixtures (i.e. open/through) designs to be able to cancel out the influence of the board and connector and determine the transmission characteristic of the FFC itself. Similarly, if we're talking about shielding, a full EMI/EMC set-up with a chamber or cell and a spectrum analyser will often be required. This is not really within the realm of most hobbyists - even myself, as an academic, may not find it easy to run such experiments even if I had the gear (which, sadly, I mostly do not).

    The FFCs on polyimide (Kapton) may take to being gently soldered to, but at such fine pitches, that's probably not the aim either.

    An LCD may well be a good way to demonstrate the stuff ... or a mezzanine board for a microcontroller, extension for a microSD UHS-I bus or something like that ...

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago

    This is probably going to be quite challenging to pull off. For one, the best use of FFCs are for board-to-board connections which necessitates the design of PCBs and soldering of surface mount connections which clamp onto the FFC (at least most of the time). There are some broad-pitch FFCs which can be used with crimp connections, but these are probably not being demonstrated. Note that hot-air soldering of FFC connections from the top is likely to be an exercise in futility - you are very likely to melt the plastic due to temperature issues ... but from the underside may be possible.

    If the key is to demonstrate high-speed connectivity, the test of a good connection requires not only a VNA but suitable test fixtures (i.e. open/through) designs to be able to cancel out the influence of the board and connector and determine the transmission characteristic of the FFC itself. Similarly, if we're talking about shielding, a full EMI/EMC set-up with a chamber or cell and a spectrum analyser will often be required. This is not really within the realm of most hobbyists - even myself, as an academic, may not find it easy to run such experiments even if I had the gear (which, sadly, I mostly do not).

    The FFCs on polyimide (Kapton) may take to being gently soldered to, but at such fine pitches, that's probably not the aim either.

    An LCD may well be a good way to demonstrate the stuff ... or a mezzanine board for a microcontroller, extension for a microSD UHS-I bus or something like that ...

    - Gough