Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your opinion about an Experimenting with Flat Flexible Cables
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3219 views
  • Users 0 members are here
  • molex
  • community survey
  • experimenting challenge
Related

Seeking your opinion about an Experimenting with Flat Flexible Cables

rscasny
rscasny over 3 years ago

imageLaunching an Experimenting Challenge can be a lengthy process. In general, we have a lot of meetings with the sponsor and a lot of brainstorming within the element14 team. Even choosing the prizes takes some time, with back and forth between us. Perhaps the thing that takes the most time is choosing the products. Sometimes I suggest products that I think will will work. Other times it's a collaboration between element14 and the sponsor. And sometimes we choose a product because it's something new; a good example of that is gesture sensors.

Recently, we were approached by a sponsor who makes flat flexible cables (FFCs) and would like to see element14 members experiment with them. There is a growing use of them, especially for space-constrained electronic sub-assemblies. And some of these FFCs have special characteristics such as EMI protection, hi temp environments, low voltage differential for signal integrity, impedance matching, and so on.

But designing an Experimenting Challenge means building the activity, the kit, and the experiments. That's where I like to ask community members. At face value, offering an Experimenting Challenge with FFCs seems like a hill to climb. Do we just send a kit of FFC's to the participants and see what they do? Or do we add in some other products to fill out the kit. (I did this with the Experimenting with Waterproof Connectors Challenge by adding a imageDFRobot SBC.) Of course, the more specific we get, the more specific (circuit count, length, & pitch, for instance) the FFCs would need to be.

But right now, I would like to toss around some ideas of how we could frame an Experimenting Challenge with FFCs. What should be in the kit? Types of experiments? Even, the kinds of prizes you would like to see for this activity. For myself, I see FFCs as a product we haven't talked about that much, but complements a lot of different kinds of electronics. I suspect that a lot of creative content and blogs could be created for this kind of activity.

Here are some relevant links:

Webpage

Essentials

If you have any thoughts about an Experimenting with FFCs challenge, I invite you to write a comment below.

Some polls

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    I always find I need one conductor more than the flat flex I choose!

    Anything 0.5 mm or higher pitch will be easily hand-solderable (especially with vertical connectors since they often had odd and even pins splayed on each side, so the pitch becomes 1mm, which then anyone can do with any iron, but even if it is on one side it is doable but that needs a bit more care). 0.4mm and smaller are intolerable to do by hand! Amazing what a difference that 0.1mm delta makes.

    1mm pitch is a pleasure to use, as easy and quicker than soldering pin headers.

    Unless space is super-constrained (which it usually is not, for non-consumer stuff) then it's good to just use (say) 10-way even if just a few conductors are needed, because there's not much board space saved between (say) a 4-way connector and a 10-way connector, and the extra conductors could be used for future expansion or doubling up, and less different inventory items.

    Example use-case where flat flex works out nicely:

    image

    There's a bit of an art folding flat flex for (say) 90 degree turns and positioning things just right to not have any slack on boards! I think flat flex is one of the best cabling inventions ever. Curious to know its history!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    I always find I need one conductor more than the flat flex I choose!

    Anything 0.5 mm or higher pitch will be easily hand-solderable (especially with vertical connectors since they often had odd and even pins splayed on each side, so the pitch becomes 1mm, which then anyone can do with any iron, but even if it is on one side it is doable but that needs a bit more care). 0.4mm and smaller are intolerable to do by hand! Amazing what a difference that 0.1mm delta makes.

    1mm pitch is a pleasure to use, as easy and quicker than soldering pin headers.

    Unless space is super-constrained (which it usually is not, for non-consumer stuff) then it's good to just use (say) 10-way even if just a few conductors are needed, because there's not much board space saved between (say) a 4-way connector and a 10-way connector, and the extra conductors could be used for future expansion or doubling up, and less different inventory items.

    Example use-case where flat flex works out nicely:

    image

    There's a bit of an art folding flat flex for (say) 90 degree turns and positioning things just right to not have any slack on boards! I think flat flex is one of the best cabling inventions ever. Curious to know its history!

    • Cancel
    • Vote Up +4 Vote Down