Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your opinion about an Experimenting with Flat Flexible Cables
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3219 views
  • Users 0 members are here
  • molex
  • community survey
  • experimenting challenge
Related

Seeking your opinion about an Experimenting with Flat Flexible Cables

rscasny
rscasny over 3 years ago

imageLaunching an Experimenting Challenge can be a lengthy process. In general, we have a lot of meetings with the sponsor and a lot of brainstorming within the element14 team. Even choosing the prizes takes some time, with back and forth between us. Perhaps the thing that takes the most time is choosing the products. Sometimes I suggest products that I think will will work. Other times it's a collaboration between element14 and the sponsor. And sometimes we choose a product because it's something new; a good example of that is gesture sensors.

Recently, we were approached by a sponsor who makes flat flexible cables (FFCs) and would like to see element14 members experiment with them. There is a growing use of them, especially for space-constrained electronic sub-assemblies. And some of these FFCs have special characteristics such as EMI protection, hi temp environments, low voltage differential for signal integrity, impedance matching, and so on.

But designing an Experimenting Challenge means building the activity, the kit, and the experiments. That's where I like to ask community members. At face value, offering an Experimenting Challenge with FFCs seems like a hill to climb. Do we just send a kit of FFC's to the participants and see what they do? Or do we add in some other products to fill out the kit. (I did this with the Experimenting with Waterproof Connectors Challenge by adding a imageDFRobot SBC.) Of course, the more specific we get, the more specific (circuit count, length, & pitch, for instance) the FFCs would need to be.

But right now, I would like to toss around some ideas of how we could frame an Experimenting Challenge with FFCs. What should be in the kit? Types of experiments? Even, the kinds of prizes you would like to see for this activity. For myself, I see FFCs as a product we haven't talked about that much, but complements a lot of different kinds of electronics. I suspect that a lot of creative content and blogs could be created for this kind of activity.

Here are some relevant links:

Webpage

Essentials

If you have any thoughts about an Experimenting with FFCs challenge, I invite you to write a comment below.

Some polls

  • Sign in to reply
  • Cancel
Parents
  • misaz
    misaz over 3 years ago

    In last question I chosen Other. In this question missed option "I do not know".

    I currently have one personal project need in near future when I want to use flex cables but selecting products to flex cables kit is very hard task becase there are tons of variants. Flex cables in selected molex family have between 4 to 60 circuits and they also differ in length. How would you select cables to the kit? FOr example if you select 4pin cables and provide 10 length options that it would be fine for connecting i2c temperature sensors, but unluckily challengers will not be able to connect RGB TFT LCD display which requires about 30-50 wires. In other way if you provide 50 wire option it will be overkill for temperature sensor projects because even the connector will be larger than the whole sensor board. You can think about it form other side. Provide multiple pin count options but with fixed length. It will handle most needs but it will be less flexible in mechanical terms.

    In all case i recommend select one pitch option and provide all cables (and connector) with one selcted pitch. Otherwise it became complex even in this direction.

    The other related question is in provided quantity. For example for temperature sensor application challenger will mos tprobably utilize more than one cable (for connecting more sensors) but for display application one cable is sufficient.

    My idea is to enable challenger to describe his/her needs in application by providing filled excel template which you will provide to download. It can look for example as follow:

    image

    The lengts which I selected in column are standard lengths in which molex offers their cables but note that not all combinations are possible and table requires furhter checking (for example shortest 60pin is 51 and 30 mm variant with this pin cout does not exists), so table require furhter checking before publishing.

    I am not sure that my idea is the best one because there may be some organisational troubles like stock unavalaiblity of some variants which user may select. So take it like an idea but most probably it would be better to go different way and just provide kit of preselected cables and let challenger to adapt their projects and expriments to parts from provided kit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to misaz

    I think the table could just have values in increments of 10, since there's hardly any board size difference if there are spare conductors, nor any significant cost difference. For length, just (say) 100 and 200 would be OK because people could fold them if the length is too long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to misaz

    I think the table could just have values in increments of 10, since there's hardly any board size difference if there are spare conductors, nor any significant cost difference. For length, just (say) 100 and 200 would be OK because people could fold them if the length is too long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • misaz
    misaz over 3 years ago in reply to shabaz

    Lengths come from Molex website. Only offered lengths arenhere.