Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking your opinion about an Experimenting with Flat Flexible Cables
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3223 views
  • Users 0 members are here
  • molex
  • community survey
  • experimenting challenge
Related

Seeking your opinion about an Experimenting with Flat Flexible Cables

rscasny
rscasny over 3 years ago

imageLaunching an Experimenting Challenge can be a lengthy process. In general, we have a lot of meetings with the sponsor and a lot of brainstorming within the element14 team. Even choosing the prizes takes some time, with back and forth between us. Perhaps the thing that takes the most time is choosing the products. Sometimes I suggest products that I think will will work. Other times it's a collaboration between element14 and the sponsor. And sometimes we choose a product because it's something new; a good example of that is gesture sensors.

Recently, we were approached by a sponsor who makes flat flexible cables (FFCs) and would like to see element14 members experiment with them. There is a growing use of them, especially for space-constrained electronic sub-assemblies. And some of these FFCs have special characteristics such as EMI protection, hi temp environments, low voltage differential for signal integrity, impedance matching, and so on.

But designing an Experimenting Challenge means building the activity, the kit, and the experiments. That's where I like to ask community members. At face value, offering an Experimenting Challenge with FFCs seems like a hill to climb. Do we just send a kit of FFC's to the participants and see what they do? Or do we add in some other products to fill out the kit. (I did this with the Experimenting with Waterproof Connectors Challenge by adding a imageDFRobot SBC.) Of course, the more specific we get, the more specific (circuit count, length, & pitch, for instance) the FFCs would need to be.

But right now, I would like to toss around some ideas of how we could frame an Experimenting Challenge with FFCs. What should be in the kit? Types of experiments? Even, the kinds of prizes you would like to see for this activity. For myself, I see FFCs as a product we haven't talked about that much, but complements a lot of different kinds of electronics. I suspect that a lot of creative content and blogs could be created for this kind of activity.

Here are some relevant links:

Webpage

Essentials

If you have any thoughts about an Experimenting with FFCs challenge, I invite you to write a comment below.

Some polls

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    I have a potential application. I want to connect little data acquisition modules to a mother board but the twist is that the modules must have at least 500V isolation. So each module will have its own isolating DC-DC converter and 4 isolated high speed signals (2 transmit and 2 receive). The idea is that each module connects to the motherboard by a multi way cable which must use LVDS drivers/receivers on each module to talk to LVDS ports on the FPGA on the motherboard. The flexi cable drivers and receivers are at earth referred potential.

    A classical motherboard with // connections is no help -  I need 10 modules to be star connected and I don't want the mechanical constraints of a Eurocard (or rack) system.

    So the first part of my plan was to do some signal integrity experiments with flexible cables. The minimum required signal speed is 20Mbits/s but 50 would be nicer.

    So to do this experiment I will need a scope and some custom built ends, one with FPGA and one with ADUM14x isolators LVDS transceivers. The cable will need at least 20 ways.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago

    I have a potential application. I want to connect little data acquisition modules to a mother board but the twist is that the modules must have at least 500V isolation. So each module will have its own isolating DC-DC converter and 4 isolated high speed signals (2 transmit and 2 receive). The idea is that each module connects to the motherboard by a multi way cable which must use LVDS drivers/receivers on each module to talk to LVDS ports on the FPGA on the motherboard. The flexi cable drivers and receivers are at earth referred potential.

    A classical motherboard with // connections is no help -  I need 10 modules to be star connected and I don't want the mechanical constraints of a Eurocard (or rack) system.

    So the first part of my plan was to do some signal integrity experiments with flexible cables. The minimum required signal speed is 20Mbits/s but 50 would be nicer.

    So to do this experiment I will need a scope and some custom built ends, one with FPGA and one with ADUM14x isolators LVDS transceivers. The cable will need at least 20 ways.

    MK