Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum UPCOMING - Have You Experimented with Flyback Transformers? If Not, Step Up and Participate to Win Big Prizes - Seeking Your Feedback
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 12 subscribers
  • Views 3482 views
  • Users 0 members are here
  • EXPERIMENTING WITH FLYBACK TRANSFORMERS
Related

UPCOMING - Have You Experimented with Flyback Transformers? If Not, Step Up and Participate to Win Big Prizes - Seeking Your Feedback

rscasny
rscasny over 3 years ago

Greetings to All!

I am preparing to launch a new Experimenting Challenge activity focusing on  flyback transformer experiments.

I wanted to tell you about it before I launch it.

I'd like to give you some facts and let you see what I am thinking about during my planning stage with the sponsor.

I'd also like to hear your thoughts about what you might like included in the kit.

The kit will contain twelve different flyback transformers (Scroll down to see). I would consider adding things to the kit. I'd like to hear your suggestions. You can post in the comment sections below.

Of course, there will be some great prizes as well. Here are the prizes I am considering:

Grand Prize

image

Handheld Oscilloscope

image

NEW! Beagle V-Ahead

image

DC Electronic Load

For More Info For More Info For More Info

Runner Up Prize

image

Hot Air Station

image

DC Power Supply

image

NEW! Beagle V Ahead

For More Info For More Info For More Info

Finisher Prize

image

Heat Shrink Kit

For More Info

Before I get into the details, I thought it might be good to pose the question:

Here's something to chew on:

A flyback transformer is a coupled inductor with a gapped core. During each cycle, when the input voltage is applied to the primary winding, energy is stored in the gap of the core. It is then transferred to the secondary winding to provide energy to the load. Flyback transformers are used to provide voltage transformation and circuit isolation in flyback converters.
Here's the parts the sponsor selected for the kit:

(A couple of images)

image image

Here are the product pages. (Note: some of these are new products so all the info may still need to be loaded on the page.)

Product Description See Entire Kit
PFBR45-ST13150S Gate Drive Transformer, 1MH, 2KV  See Here
PFBR45-ST13150S Gate Drive Transformer, 1.15MH, 4.5KV See Here
BA60951CS XFMR, SMPS, FLYBACK, 2.5KV See Here
SM13117EL Ethernet & LAN Transformer, PoE, 1 Port, 1:0.5:0.5:0.5, 350 µH, 1.5 kV, Surface Mount See Here
063929 SMPS Transformer, Flyback, 250 mA, 44kHz to 132kHz, 4 W, 85V to 265V See Here
063932 SMPS Transformer, Flyback, 250 mA, 44kHz to 132kHz, 6 W, 85V to 265V See Here
093830 SMPS Transformer, Flyback, 650 mA, 132kHz, 8 W, 85V to 265V See Here
063934 SMPS Transformer, Flyback, 370 mA, 44kHz to 132kHz, 9 W, 85V to 265V See Here
094931 SMPS Transformer, Flyback, 1.8 A, 66kHz to 132kHz, 22 W, 85V to 265V See Here
094932 SMPS Transformer, Flyback, 1.2 A, 132kHz, 22 W, 85V to 265V See Here
071923 Choke, Common Mode, 0.28 A, 22 mH, Through Hole See Here
093267 Choke, Common Mode, 0.5 A, 27 mH, Through Hole See Here
D00413 Compartment Box, Clear, Plastic, General Purpose Storage, 35x125x230mm See Here

Datasheets on some of the parts:

a. https://www.farnell.com/datasheets/3742805.pdf

b. https://www.farnell.com/datasheets/3774338.pdf

c. https://www.farnell.com/datasheets/2868806.pdf

d. https://www.farnell.com/datasheets/3967078.pdf

e. https://www.farnell.com/datasheets/3967079.pdf

f. https://www.farnell.com/datasheets/3967080.pdf

g. https://www.farnell.com/datasheets/3967081.pdf

  • Sign in to reply
  • Cancel
Parents
  • rsc
    rsc over 3 years ago

    Probably too small for tesla coil action..........

    image

    Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsc
    rsc over 3 years ago

    Probably too small for tesla coil action..........

    image

    Scott