Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking Feedback on Kit for Upcoming Experimenting with Extreme Environments
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 17 subscribers
  • Views 4130 views
  • Users 0 members are here
  • experimenting challenge survey
Related

Seeking Feedback on Kit for Upcoming Experimenting with Extreme Environments

rscasny
rscasny over 2 years ago

At least once a year, I try to do some activity along the lines of protecting electronics. In 2023, I launched Experimenting with Waterproof Connectors. In late 2021, we launched the Just Encase Design Challenge. As more electronics are employed outdoors and more IOT solutions are installed in remote locations in the open environment, the need to protect electronics is increasing.

In the challenge I am now planning, I hope to take the idea of "electronics environmental protection" to the extremes.

In brief, the challengers will be given a kit to build something -- anything. They will house their electronic-builds in a durable, IP65-67 enclosure. After doing those the things, the real fun begins.

We would like the participants to experiment with extreme environments such as hot & cold temperatures, light & strong water sprays, vibrations, dust "storms," etc. You get the idea. They will need to design a testing environment to simulate the extreme condition being tested and then put their protected-build in it. And write about it.

Feedback on Proposed Kit

For the remainder of this discussion, I will overview selections for the kit. I have three options each for:

  • Electronics
  • Enclosure
  • Display
  • Sensor Connector

Please vote for your preference of each kit component. Now, if you have an alternate suggestion, feel free to post a comment.

I would like the electronic-builds to be battery-powered since a lot of remote monitoring is battery powered. Take a look at the viability of that. If that doesn't work, I may then give special extra credit to those participants that have a battery-powered experiment. At this point, I am in the planning stage. Not everything is cast in stone, so to speak.

Of course, there other parts such as cables, other types of connectors, power supplies, sensors, etc. that I have not included in this preliminary kit. Go ahead and post a comment on the accessories you would like.

Thanks for participating in this discussion.

Here are the polls:

ELECTRONICS under consideration

MICROCHIP EV36W50A WFI32-IOT Board, 32bit, PIC

image

Datasheet

Raspberry Pi Compute Module 4 Lite and I/O Board

image

image

Datasheet

ARDUINO AKX00034 EDGE CONTROL BOARD

image

Datasheet

Display under consideration

ADAFRUIT 2260 TFT Display

image

Datasheet

MIDAS MC42005A6W-SPTLYI-V2 DISPLAY, ALPHANUMERIC, 20X4

image

Datasheet

MIKROE-55 Display, Character LCD 2x16

image

Datasheet

ENCLOSURES under consideration

HAMMOND 1554VA2GYCL, Plastic Enclosure, IP68

image

Datasheet

HAMMOND 1590Z231GY Metal Enclosure, Small, Diecast Aluminum, IP68

image

Datasheet

HAMMOND 1555HF17GY Plastic Enclosure, Watertight, Industrial, IP67

image

Datasheet

SENSOR CONNECTOR under consideration

AMPHENOL MRDBG02L13000, Circular Connector, 2 Contacts

image

Datasheet


AMPHENOL MRDBG03L13000, Circular Connector, 3 Contacts

image

Datasheet

AMPHENOL MRD-BG04-L13-000, Circular Connector, 4 Contacts

image

Datasheet

  • Sign in to reply
  • Cancel
Parents
  • JWx
    JWx over 2 years ago

    another observation - after quick check, WFI32-IoT (nor probably Ardunio) doesn't seem to have external antenna connector, so radio cannot be used when placed in  metal case, leaving Raspberry that has "Either the onboard antenna or an external antenna kit [...]" according to the datasheet...

    Will need to check if base board provides some antenna connector

    As an alternative, 1554 with pressure compensation plug could also be interesting - like this (IP66)

     https://www.hammfg.com/part/BDN4XN1?referer=448

    or third party when better IP rating is to be obtained.

    This way, some comparison can be done if someone who participated with the previous challenge would be selected in this one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 2 years ago

    another observation - after quick check, WFI32-IoT (nor probably Ardunio) doesn't seem to have external antenna connector, so radio cannot be used when placed in  metal case, leaving Raspberry that has "Either the onboard antenna or an external antenna kit [...]" according to the datasheet...

    Will need to check if base board provides some antenna connector

    As an alternative, 1554 with pressure compensation plug could also be interesting - like this (IP66)

     https://www.hammfg.com/part/BDN4XN1?referer=448

    or third party when better IP rating is to be obtained.

    This way, some comparison can be done if someone who participated with the previous challenge would be selected in this one.