Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum Seeking Feedback #2 - Expanding Design Challenge Kit - USB Camera, AC Adapter & PMOD Sensor
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 10 subscribers
  • Views 1626 views
  • Users 0 members are here
  • member survey
Related

Seeking Feedback #2 - Expanding Design Challenge Kit - USB Camera, AC Adapter & PMOD Sensor

rscasny
rscasny over 2 years ago

image

This is a follow up to my previous poll/discussion on Seeking Feedback on Kit and Prizes for Design Challenge.

I didn't add the camera initially because I saw this challenge could be done in different ways. But I'm open to adding to the kit.

So, the challenge is using the Digilent Arty Z7 Dev board.

image

Here are three things that could be added to the kit:

USB camera

  • Logitech C270 HD Webcam, 720p
  • Webcam HD 1080p ,Live Streaming Web Camera

Poll


AC Adapter

  • TRIAD MAGNETICS WSU120-2000 AC/DC Power Supply, 12 V, 2 A
  • XP POWER VEL24US120-US-JA AC/DC Power Supply, 12 V, 2 A

Poll

Sensors

  • Pmod ALS: Ambient Light Sensor SKU: 410-286
  • Pmod LS1: Infrared Light Detector

Poll

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 2 years ago

    A nice triple boost to the kit - should improve popularity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago

    Hi all. 

    Thanks for the feedback. I'll be adding some things to the kit. Perhaps I rushed this challenge out the gate a bit too soon. Life is a lesson learned. 

    Randall

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago

    I opted for the 720p camera because more isn't always better.  Is processing twice the amount of data for the same image going to net any better recognition?  I'm skeptical.  720p is a lot of resolution.

    Triad Magnetics for the lower ripple.

    Ambient light sensor because most of my USB cameras seem to change the light setting automatically for no reason what-so-ever.  Maybe this will help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago

    I think the best option for performance for this board is to use the HDMI input. Regarding the power supply, Digilent's reference page mentions 12 VDC 3A, supporting from 7 VDC to 15 VDC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Nice set of functionality on that board! I voted C270 camera, only because there's a higher chance that it could be easy to use with Linux (since it's a major brand, it is more likely there will be online information about how to get it going with Linux).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to DAB

    Thanks for mentioning the ac adapter links. They are working now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    The links to the power supplies gave me an error message.

    To be of use to the camera modules, you will need both IR and visible light sensors so you can measure the available light 24/7.