Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog Forget Me Not: Episode 14 - Nearing the End
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelwylie
  • Date Created: 20 Oct 2014 4:10 AM Date Created
  • Views 1628 views
  • Likes 1 like
  • Comments 9 comments
  • forget_me_not
  • iot_auto_monitor
Related
Recommended

Forget Me Not: Episode 14 - Nearing the End

michaelwylie
michaelwylie
20 Oct 2014

Previous Posts:

 

Epidode 1: Forget Me Not: Application

Episode 2: Forget Me Not: The Best Laid Plans ...

Episode 3: Forget Me Not: Setup EnOcean with openHAB

Episode 4: Forget Me Not: Medication System

Episode 5A: Forget Me Not: Using Notify My Android with OpenHab

Episode 6: Forget Me Not: Plant Watering System Design

Episode 7: Forget Me Not: Medication System Demo

Episode 8: Forget Me Not: Using Twitter

Episode 9: Forget Me Not: Sunshine, Lollipops, and Rainbows

Episode 10: Forget Me Not: It's so hot!

Forget Me Not: Episode 11A: Watering System Construction

Forget Me Not: Episode 11B - Soil Sensor Design

Forget Me Not: Episode 12: An Update

Forget Me Not: Episode 13: Watering System Finalization

 

Update


There hasn't been much progress this week. I'm still waiting for parts.

 

Plant Watering Update

 

The watering system is on my patio watering my plant. Figure 1 shows a picture of it installed.

image

Figure 1: Watering System Installation.

 

I installed it yesterday, and it over watered the first day. I made some adjustments to the thresholds and we'll see how that pans out. Figure 2 shows my overwatered plant.

 

image

Figure 2: Overwatered plant.

 

Air Conditioning Update

 

I've set to work on the Air Conditioning Switch. Figure 3 shows a collage of items showing some details from the air conditioning switch design. In the upper left a diagram is shown that details the measurements and physical layout of the air conditioning unit switch mechanism. Note, I live in an apartment, and therefore cannot alter the unit itself. It would be easiest to use an electrical signal to turn on and off the AC, but, it is what it is. The requirement was to turn the AC on and off remotely. Below on the left is my two solenoid arrangement that has a travel of 5 mm, Driving the left solenoid pulls the two plungers to the left and driving the right solenoid pulls the two plungers to the right. The plungers are coupled together, ideally by a bracket, but currently by a dab of super glue. The picture on the right shows the AC interface. You can see the switch in the lower right of the picture.

image

Figure 3: Air Conditioning Switching

 

Figure 4 shows my design for the solenoid driver circuits. On the left is the header for the Raspberry Pi B+ and on the right are the two solenoid driver circuits. R1 and R2 are pull down resistors that ensure the solenoids are not energized while the Pi is booting. Setting GPIO17 high turns on transistor T1 and energizes SOILENOID1. D1 provides a path for current when the solenoid is de-energized, and is appropriately called a free-wheeling diode (also known by snubber, clamp, and flyback diode). The circuit for SOLENOID2 is the same as the circuit for SOLENOID1.

image

Figure 4: Solenoid Driver Circuits.

 

I do not have the components yet to build this circuit, but I've tested my solenoids with a 5V power supply. Only one solenoid is driven at-a-time.

 

My intention at the beginning of this challenge was to learn because it would stretch my skill set. I've definitely been stretched, not only as an engineer, but also as a procurement agent and project planner. So, thank you to Element14 and Newark for giving me the opportunity to compete.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +1
    At least you didn't flood the house, just some plants got wet.... Pity you didn't have a 3D printer, otherwise you knock up a cam arrangement, and drive a stepper. I see that there are Airconditioning…
  • michaelwylie
    michaelwylie over 11 years ago in reply to shabaz +1
    Ohhh yeaaaaah ... I remember those. Now everything is touch, you kids ...
  • DAB
    DAB over 11 years ago in reply to michaelwylie

    Depends on the plant.

     

    I think all of her orchids need just a cube or two a week.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to shabaz

    Ohhh yeaaaaah ... I remember those. Now everything is touch, you kids ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelwylie

    Hehe small solenoids were really popular in the pre-iPod era, when they were in every cassette player with "soft-touch" buttons (as tactile switches were branded at the time). You kids..

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to shabaz

    Thanks!

     

    Originally I knew NOTHING practical about solenoids; all my knowledge was theoretical. So I ordered this one and when it showed up I thought it looked odd. It took me a while to figure out how it worked because it didn't come with a spring! I only realized this after looking at every other solenoid and comparing it to mine. That's what I get for buying the cheapest one, right? This is how the double solenoid rig was born ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Love the double-solenoid : )

    Very cool : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>