Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog "Remember Me Always!" - Part 015
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 22 Sep 2014 10:22 AM Date Created
  • Views 1638 views
  • Likes 1 like
  • Comments 11 comments
  • forget_me_not
  • remember_always
Related
Recommended

"Remember Me Always!" - Part 015

COMPACT
COMPACT
22 Sep 2014

Postcards not from the Edge

imageimage

 

I'd like to thank Cypress SemiConductor for sending me out two new CY8CKIT-049 PSoC4200 Prototyping kits. They arrived in quite novel packaging.

I was privileged enough to receive an engineering prototype earlier and was going to use it for this challenge but was provided the released versions to showcase them.

The engineering prototype contained just a PSoC 4200 on a 600mil DIP breakout board so I performed programming and debugging with a MiniProg 3.

The released kit include a detachable USB-Serial adapter to remove the need for a MiniProg 3 or equivalent. Unlike a MiniProg 3, this adapter does not provide any interactive debugging capabilities and requires the connected PSoC4 to have bootloader firmware loaded.

The adapter communicates to the PSoC4 using its P4.0 and P4.1 configured as a serial port.

 

There are many hazards getting the USB-Serial adapter working and I must have stumbled on most of them. I was not alone because a search on the Internet found many others with the same or similar difficulties. I persevered sorted out each issue to produce a reliable repeatable procedure.

Here are some of my stumbles and I won't bore you with the error messages encountered.

Stumble 1. - The rapid blinking LED when the bootloader is enabled is not that much faster than the default test program. This can give you the false impression that you are not in bootloader mode.

Stumble 2. - After connection of the second CY8CKIT-049 kit (which probably would be assigned as COM32:), all my USB-Serial adapters were no longer being enumerated by Windows. I had to use Device Manager and clear out all Virtual Serial Port Enumerations to get it working again.

Stumble 3. - The communication to the PSoC4 is 115000 baud. The documentation if not read carefully may give you the impression to set it to 9600 baud.

Stumble 4. - When using the bootloader programing function from PSoC Creator 3 SP1 the path to the .cycad file does not automatically point to the correct path for your project.

 

So with a bit of tuning to the Prototyping Kit Guide text most of the stumbles could have been avoided.

 

Here is a helpful hint for creating blank PSoC 4 bootloadable projects for use with the CY8CKIT-049 4200.  Use it in conjunction with Section 5.3 of the CY8CKIT-049 4xxx Prototyping Kit Guide.

After creating a new PSoC Creator project copy the Dependencies folder from the CY8CKIT-049 4200 example to your new project folder. (for .HEX and .ELF files). This keeps all of your source files together easier management.

 

Although working and working well I really do prefer using the MiniProg3. I think the added expense is well worth the cost and makes debugging considerably simpler and development faster.

If you don't do as much PSoC development work as myself then you could use a PSoC 4 Pioneer Kit to get the equivalent functionality.

The Prototype Kit's USB-Serial adapter is a great way to get a PSoC 4 communicating with a PC without any serial ports.

 

Now why would I have a PSoC 4 for this challenge?

Can anyone guess? Could it be for a RPiSoC alternative? Maybe something else?

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Yea, I won't bore you with the size of my first work computer that was much less capable than the little Psoc board.

     

    It is just totally amazing what you can do with something you can barely see.

     

    Or am I just getting blind, naw can't be.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Yea, I won't bore you with the size of my first work computer that was much less capable than the little Psoc board.

     

    It is just totally amazing what you can do with something you can barely see.

     

    Or am I just getting blind, naw can't be.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • COMPACT
    COMPACT over 12 years ago in reply to DAB

    Hi Don,

    I built my first computer which is now 36 years old and still works. It's filter caps are huge and its power transformer weighs a tonne.

    I've added Hard Disk, TCP/IP and Ethernet capabilities to it proving that the only major technological breakthroughs since then have been with miniaturisation and technology tuning and control with its subsequent performance, reliability and power efficiency improvements.

    In the 1970's it took me 6 months to save up enough money to add a 4KB memory card to it. Now we can get 8GB memory sticks for free as advertising trinkets.

     

    I've also built three replicas of this machine - two physical ones - a single FPGA version (with extended colour graphics support), a version that consists of more highly integrated Zilog components (with TCP/IP and Ethernet support) and a virtual one with just an mbed and AVR32 (with TCP/IP, Ethernet and USB support) for which I received a Circuit Cellar Distinctive Excellence award

    http://circuitcellar.com/contests/nxpmbeddesignchallenge/winners/DE3784.htm

     

    Very Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 12 years ago in reply to COMPACT

    Its funny that you meet the same people in other contests again image My entry to that mbed challenge was the starting point for the current one: NXP mbed Design Challenge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 12 years ago in reply to hlipka

    Congratulations for that and it's nice to know that you read my posts.

    The writing is on "The Wall"!

    There's no REST for the wicked!image