Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog The Forget Me Not Challenge - Now With Added RPiSoC!
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: doctorcdf
  • Date Created: 22 Aug 2014 7:29 AM Date Created
  • Views 4461 views
  • Likes 4 likes
  • Comments 62 comments
  • forget_me_not
  • rpisoc
  • internet_of_things
  • cypress_semiconductor
  • cypress
Related
Recommended

The Forget Me Not Challenge - Now With Added RPiSoC!

doctorcdf
doctorcdf
22 Aug 2014
Earlier this week, the element14 community was introduced to an exciting new Raspberry Pi Accessory, the RPiSoC, which is currently seeking funding through Kickstarter:
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
I'm pleased to say that Embedit Electronics, in collaboration with Cypress Semiconductor, have allocated 17 prototype units for the challengers involved in the Forget Me Not Challenge.  They are currently winging their way to our warehouse.
image
In order to obtain one of these highly exclusive boards, only the most compelling use cases will do.  The competitors are invited to submit their proposals as comments in reply to this blog.  Thank you.
  • Sign in to reply

Top Comments

  • crosseyejack
    crosseyejack over 12 years ago +2
    I've spent all day thinking about this and this is my response. Thank you very very much for giving me the chance of getting this SOC add-on board to the Raspberry Pi. It is a very nice board indeed. BUT…
  • doctorcdf
    doctorcdf over 12 years ago +2
    Thanks to everyone for their use cases. We are going to ship RPiSoCs to the following competitors: Mark Beckett Abhijit Bose Ravi Butani Ambrogio Galbusera Jeremy Kuek Hendrik Lipka Pascal Martin Vishnu…
  • ipv1
    ipv1 over 12 years ago in reply to michaelwylie +1
    Please excuse me as I faint out of happiness... and..
  • ipv1
    ipv1 over 12 years ago in reply to doctorcdf

    Sir when will the finalists be err... finalized? I have to send a PCB for manufacturing BUT I wont have to if I get one of these.

    Thanks,

    IP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 12 years ago

    I was planning to use an Arduino connected via FTDI to the RPi to enable accessing ADCs for measuring Temperature and currents. Additionally the PWM were supposed to be connected to RGB leds which translate notifications in OpenHAB to various colors. Combination of RGB we can generate almost any shade of color. Additionally I was dependent of the Arduino to convert all the serial messages into corresponding actions as well as a little bit of filtering. I though of using the PSOC 5 (from the Cypress MBBR3 Kit but It cannot be programmed as is and making a board or buying one was not an option. The power of the PSOC is that things happen in hardware which means that I can have some digital logic doing one thing and another logic something else. The RPiSOC goes beyond it by providing tested python scripts that will enable it to be interfaced with OpenHAB directly. I will use the RPi SOC for...

     

    1. Controlling RGB LEDs to produce color indications. the RPiSOC can generate better PWM.

    2. Add a small display for notifications and messages. My current HDMI display is a bit TOO power hungry.

    3. Expose additional UART for connecting with the secondary sensor network.(XBEE because I plan to demonstrate how OpenHAB can also connect with non-standard networks using bindings)

    4. Measuring battery status and OFFLOAD the entire measure and compare and notify burden from the RPi to the RPiSOC Programmable Gain amplifier eliminates the need for me to build extra circuitry. I head there were Digital Filters available as well.

    5. I have a motor control planned in the future which will need the PWM outputs. Think wheels+motors+RPi+RPi Camera+WiFi+battery=  OpenHAB Controlled RPi Rover image  I have already done some work some time back.

     

    I can bypass my board making task and use this board directly. The python examples will make it simpler to interface with OpenHAB with the exec Binding/Serial binding.

     

    Hope I get one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bose
    bose over 12 years ago in reply to bose

    I wish to the Arduino Shield that these guys are using .

    It would be a great addition to the existing FHEM based online interface.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bose
    bose over 12 years ago

    This brings back memories from my DAS project. Since this uses PSoC5(kitchen sink! type image) there is lots more LUT unlike the PSoC4.

    I wish all the GPIO headers can be male pins to connect other modules.

    The stock image of the RpiSoc has lots API so many things can already be done even without the PSoC creator.

    Actually the USB bootloader means no need for MiniProg3.

    Lots of possibilities for additional analog sensors and real world controls.

     

    As simple to say RPi B+ & RPiSoC is great combo for real time processing with IoT. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • doctorcdf
    doctorcdf over 12 years ago

    Our intention is to get moving on shipping these units by mid to late next week - so if you could have your ideas put forward here by the end of play Wednesday, that would be ideal.  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>