Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog The Forget Me Not Challenge - Now With Added RPiSoC!
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: doctorcdf
  • Date Created: 22 Aug 2014 7:29 AM Date Created
  • Views 4459 views
  • Likes 4 likes
  • Comments 62 comments
  • forget_me_not
  • rpisoc
  • internet_of_things
  • cypress_semiconductor
  • cypress
Related
Recommended

The Forget Me Not Challenge - Now With Added RPiSoC!

doctorcdf
doctorcdf
22 Aug 2014
Earlier this week, the element14 community was introduced to an exciting new Raspberry Pi Accessory, the RPiSoC, which is currently seeking funding through Kickstarter:
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
I'm pleased to say that Embedit Electronics, in collaboration with Cypress Semiconductor, have allocated 17 prototype units for the challengers involved in the Forget Me Not Challenge.  They are currently winging their way to our warehouse.
image
In order to obtain one of these highly exclusive boards, only the most compelling use cases will do.  The competitors are invited to submit their proposals as comments in reply to this blog.  Thank you.
  • Sign in to reply

Top Comments

  • crosseyejack
    crosseyejack over 12 years ago +2
    I've spent all day thinking about this and this is my response. Thank you very very much for giving me the chance of getting this SOC add-on board to the Raspberry Pi. It is a very nice board indeed. BUT…
  • doctorcdf
    doctorcdf over 12 years ago +2
    Thanks to everyone for their use cases. We are going to ship RPiSoCs to the following competitors: Mark Beckett Abhijit Bose Ravi Butani Ambrogio Galbusera Jeremy Kuek Hendrik Lipka Pascal Martin Vishnu…
  • ipv1
    ipv1 over 12 years ago in reply to michaelwylie +1
    Please excuse me as I faint out of happiness... and..
  • electronichamsters
    electronichamsters over 12 years ago

    Hi Christian,

    Nice addition.  Makes it so we can have less dependence on auxiliary Arduinos when the RPi could be used.  I have two mini projects that could use a single RPiSoc for my home automation project.

     

    1)  Dog Location Indicator, or "Dog Vane"

     

    As part of my project, I'm building a GPS dog collar that communicates with OpenHAB and alarms when the dog goes beyond the yard.  I want a large indicator in the living room that points to the direction of the dog, so you always have awareness of where the dog is.  I can use the Living Room Raspberry Pi and the RPISoC to control the direction of a an arrow mounted on a servo motor.  As the dog wonders around the yard, the large arrow on a stick points towards where the dog is.  When the dog wonders off the yard and the OpenHAB sounds an alarm, you can look up to see which direction the arrow is pointing.

     

    image

     

    2)  I already have a Garage Door monitor as part of my project.  I have a couple of relays connected to the Raspberry Pi , this would provide additional output for the garage door remote.

     

    So that would be the short term use of the RPiSoC.  My next project requires a bigger budget and more time, which won't fit within this Element 14 competition.  But I'd like to build a doll-house size replica of my house, complete with servo controlled garage door and windows.  Using OpenHAB rules and the Raspberry Pi, when the real garage door or window is opened, I would make the replica house open the corresponding door/windows.  And I would also have simple light sensors monitoring which rooms have the lights on, and turn on tiny LED's in the corresponding rooms in the replica house.  And when the washer or dryer is running, I'll turn on a red LED on the replica basement washer to show it's in the on state.  The replica house would also play the same audio alarms and cues.

     

    The doll house would be a physical dashboard that's powered by Openhab, instead of a virtual dashboard being displayed on a tablet.  The neat thing is I could put the replica in some other house or at work, and open up a secure MQTT connection to my home server...an interesting twist on remote home monitoring.  A Raspberry Pi and the RPiSoC would do the servo control, LED's, and audio alarms on the doll house.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to fvan

    Too slow bro.  image

     

    I managed to get in and there were 15 available ...  image

     

    We need to go back and add Cypress and Embedit to the advertising logos in our posts. ...

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to mcb1

    That's the $44 reward with the miniprog ? Unfortunately all gone at that level image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to doctorcdf

    The kickstarter has some additional benefits ... get in early and get the programmer.

     

    I signed for one as it's a worthwhile addition.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • doctorcdf
    doctorcdf over 12 years ago

    Sorry, this offer is only for those who are in the Forget Me Not design challenge.  You can obtain one via Kickstarter. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>