Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Forum programmer for EnOcean?
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 7 subscribers
  • Views 2102 views
  • Users 0 members are here
  • forget_me_not
  • enocean
Related

programmer for EnOcean?

electronichamsters
electronichamsters over 12 years ago

Hello,

This is my first time playing with EnOcean products.  If I want to utilize the GPIO on the STM330 temperature sensor, the manual gives a method of doing so, but it requires either the USB300 USB-SPI adapter or the development board.  I was hoping that would come with the sensor kits, but I didn't get one.  Did anyone receive one with their kit?

 

Does anyone know of some alternate method of programming the STM330?  Being able to program it opens up a world of possibilities...most of what I was hoping to do with it.

  • Sign in to reply
  • Cancel

Top Replies

  • electronichamsters
    electronichamsters over 12 years ago in reply to michaelwylie +1
    Yes, I think you're right, that's the dev kit that's referenced. Thanks.
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Eric,

     

    Temperature sensor STM 330 can be configured and programmed.

    Configuration will set new parameters e.g. for manufaturer ID, wake-up and measurements cycles etc.

    Writting new firmware for STM 330 is also possible with the libraries from EnOcean, however you

    need ARM Keil uVision to program the 8051 core. The PC Software DolphinStudio supports both.

    In order to connect STM 330 with the PC you need a programmer which is part of EDK 350 or 

    EPK 350,

     

    Markus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Eric,

     

    Temperature sensor STM 330 can be configured and programmed.

    Configuration will set new parameters e.g. for manufaturer ID, wake-up and measurements cycles etc.

    Writting new firmware for STM 330 is also possible with the libraries from EnOcean, however you

    need ARM Keil uVision to program the 8051 core. The PC Software DolphinStudio supports both.

    In order to connect STM 330 with the PC you need a programmer which is part of EDK 350 or 

    EPK 350,

     

    Markus