• Products and Partners
    Products and Partners
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
Get Closer Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Get Closer Wearables Design Challenge
  • More
  • Cancel
Get Closer Wearables Design Challenge
Blog Testing the GPS module for the Get Closer Challenge
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: funwithbots
  • Date Created: 20 Aug 2013 7:52 PM Date Created
  • Views 695 views
  • Likes 2 likes
  • Comments 1 comment
  • get_closer
Related
Recommended

Testing the GPS module for the Get Closer Challenge

funwithbots
funwithbots
20 Aug 2013

Working on the basics to ensure the parts are all in good order. I clipped the leads to the FLORA and the GPS and ran a simple echo sketch to verify the GPS is talking.

 

The next step is to code the math calculate distances to the Geocache. I knew I was going to need math but I'm now realizing I'm going to be doing vector arithmetic to calculate headings and distances! Fortunately, I found a nice site to check my math. http://www.movable-type.co.uk/scripts/latlong.html It gets me to about +/- 10 meters with the resolution of the GPS signal.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here's the code for the sketch I used to test output streaming to the Serial Monitor:

 

#include <Adafruit_GPS.h> //GPS Library available from https://github.com/adafruit/Adafruit-GPS-Library/

#include <SoftwareSerial.h>

Adafruit_GPS GPS(&Serial1); 


// Set GPSECHO to 'false' to turn off echoing the GPS data to the Serial console

// Set to 'true' if you want to debug and listen to the raw GPS sentences

#define GPSECHO false


// this keeps track of whether we're using the interrupt

// off by default!

boolean usingInterrupt = false;


void setup()

{

// connect at 115200 so we can read the GPS fast enough and echo without dropping chars

// also spit it out

Serial.begin(115200);

Serial.println("Adafruit GPS library basic test!");


// 9600 NMEA is the default baud rate for Adafruit MTK GPS's- some use 4800

GPS.begin(9600);

// uncomment this line to turn on RMC (recommended minimum) and GGA (fix data) including altitude

GPS.sendCommand(PMTK_SET_NMEA_OUTPUT_RMCGGA);

// Set the update rate

GPS.sendCommand(PMTK_SET_NMEA_UPDATE_1HZ); // 1 Hz update rate

// For the parsing code to work nicely and have time to sort thru the data, and

// print it out we don't suggest using anything higher than 1 Hz


delay(1000);

// Ask for firmware version

Serial1.println(PMTK_Q_RELEASE);

}


uint32_t timer = millis();

void loop() // run over and over again

{

  // read data from the GPS in the 'main loop'

  char c = GPS.read();

  // if you want to debug, this is a good time to do it!

  if (GPSECHO)

    if (c) Serial.print(c);

    // if a sentence is received, we can check the checksum, parse it...

    if (GPS.newNMEAreceived()) {

      Serial.println(GPS.lastNMEA()); // this also sets the newNMEAreceived() flag to false

      if (!GPS.parse(GPS.lastNMEA())) // this also sets the newNMEAreceived() flag to false

      return; // we can fail to parse a sentence in which case we should just wait for another

    }

    // if millis() or timer wraps around, we'll just reset it

    if (timer > millis()) timer = millis();


    // approximately every 2 seconds or so, print out the current stats

    if (millis() - timer > 2000) {

    timer = millis(); // reset the timer

    Serial.print("\nTime: ");

    Serial.print(GPS.hour, DEC); Serial.print(':');

    Serial.print(GPS.minute, DEC); Serial.print(':');

    Serial.print(GPS.seconds, DEC); Serial.print('.');

    Serial.println(GPS.milliseconds);

    Serial.print("Date: ");

    Serial.print(GPS.day, DEC); Serial.print('/');

    Serial.print(GPS.month, DEC); Serial.print("/20");

    Serial.println(GPS.year, DEC);

    Serial.print("Fix: "); Serial.print((int)GPS.fix);

    Serial.print(" quality: "); Serial.println((int)GPS.fixquality);

    if (GPS.fix) {

      Serial.print("Location: ");

      Serial.print(GPS.latitude, 4); Serial.print(GPS.lat);

      Serial.print(", ");

      Serial.print(GPS.longitude, 4); Serial.println(GPS.lon);

      Serial.print("Speed (knots): "); Serial.println(GPS.speed);

      Serial.print("Angle: "); Serial.println(GPS.angle);

      Serial.print("Altitude: "); Serial.println(GPS.altitude);

      Serial.print("Satellites: "); Serial.println((int)GPS.satellites);

    }

  }

}

  • Sign in to reply

Top Comments

  • bekathwia
    bekathwia over 13 years ago +1
    Hey Bill! You might want to take a look at our GPS Jacket project-- it has some code that can help get you started with distance calculation: http://learn.adafruit.com/flora-gps-jacket/ Nice to see your…
Parents
  • bekathwia
    bekathwia over 13 years ago

    Hey Bill!

     

    You might want to take a look at our GPS Jacket project-- it has some code that can help get you started with distance calculation: http://learn.adafruit.com/flora-gps-jacket/

     

    Nice to see your update!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bekathwia
    bekathwia over 13 years ago

    Hey Bill!

     

    You might want to take a look at our GPS Jacket project-- it has some code that can help get you started with distance calculation: http://learn.adafruit.com/flora-gps-jacket/

     

    Nice to see your update!