In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - 17 - Data map
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
  • Author Author: amgalbu
  • Date Created: 7 Jan 2015 10:43 AM Date Created
  • Views 742 views
  • Likes 2 likes
  • Comments 2 comments
  • iot_distributed
  • airvantage
  • google_maps
  • in_the_air
  • in-the-air
Related
Recommended

AirMobile - 17 - Data map

amgalbu
amgalbu
7 Jan 2015

Representing data on the map

In this post I will talk about the representation of data collected by AirMobile on a map. Representing data o the map is the easiest way to understand the locations to avoid when doing outdoor activities. The solution I was thinking of is to draw a vertical line on the map at the position where the sample was taken. The height of the line is proportional to the sample value.

To implement this feature, some technical background about Google Maps is required

 

Overlay

In order to determine the screen coordinate of a given location (expressed in terms of latitude and longitude), an overlay is required. To create an overlay,

 

overlay = new google.maps.OverlayView();
 overlay.draw = function () { };
              overlay.setMap(map);

Map projection

After the overlay is created, a projection object is required in order to perform the conversion. The projection can be obtained by calling the projection.getProjection() method. However, the getProjection() method returns undefined when the map is not ready on the screen. For this reason, a event listener is installed waiting for the map entering the 'idle' state. When the map is in the 'idle' state, we are sure that the getProjection() method returns a valid projection.

After the projection is available, values can be drawn

 

// Wait for idle map
 google.maps.event.addListener(map, 'idle', function () {
 // Get projection
 projection = overlay.getProjection();
 setTimeout(loadData, 100);
 });

Getting data values

To get data values from the AirVantage cloud, I leveraged the jQuery's ajax object

 

loadData = function () {
 var dataIds = "airmobile_" + measure + ".value," + 
                            "airmobile_" + measure + ".latitude," + 
                            "airmobile_" + measure + ".longitude";
 $.ajax({
 url: "https://na.airvantage.net/api/v1/systems/data/raw" +
 "?access_token=" + accessToken + 
 "&dataIds=" + dataIds + 
 "&targetIds=" + systemUid,
 success: function (data, status, jqXhr) {
                    // data returned successfully
 }
 });

Scaling sample values

Raw values should be scaled to get the height (in pixels) of the polygon to draw. I found out 50 pixels in height to give good readability to the graph. In order to make evident changes in the values, I first find the minimum and maximum values in the array of samples returned by the AirVantage cloud, and I show these limits in the upper left corner of the page in order for the user to understand the graph scale. Minimum and maximum values are then used to calculated the height of the polygon by means of the following function

 

mapPixels= function(value, min, max) {
      var delta = max - min;
      var deltaPixels = 50;

      var pixels = deltaPixels / delta * value;
      return pixels;
};

 

 

Converting latitude and longitude to screen coordinates

The projection object has a convenient method to convert the latitude and longitude into screen coordinates. So it's easy to implement an helper function


convertCoords = function (lat, lon) {
      return projection.fromLatLngToContainerPixel(new google.maps.LatLng(lat, lon));
};

 

Drawing the polygon

To draw the polygon, some geometry is required. The polygon I want to draw has four vertexes: two are included in the AirVantage's response. The other two points are on the perpendicular line passing through each of these two points, as shown in picture

 

image

Line between two points equation

The equation for the line between two points (in explicit form) is

 


image


Being p1 and p2 two points, we can determine m and q using the code below


var value1 = values[i];
var value2 = values[i + 1];
var p1 = convertCoords(value1.latitude, value1.longitude);
var p2 = convertCoords(value2.latitude, value2.longitude);

var m = (p1.y - p2.y) / (p1.x - p2.x);
var q = p1.y - (m * p1.x);

 

Perpendicular

The equation of the perpendicular line is

 

  image

 

(where m is the value calculated in previous section)

So, the parameters of the two perpendicular lines can be calculated using the following code

 

var pm = -1 / m;
var pq1 = p1.y - (pm * p1.x);
var pq2 = p2.y - (pm * p2.x);

 

To compute the other point, I need to use the formula of the distance between a line and a point

 

image

 

The coordinates of the point (YP, Xp) lays on the perpendicular line, so YP can also be written as

 


image


The distance from the line is given by


var d1 = mapPixels(value1.value, min, max);

 

Because I already have the distance, I can calculate the point coordinate using the previous formulas. The code is as follow


var x1 = (d1 * Math.sqrt(1 + (m * m)) - pq1 + q) / (pm - m);
var y1 = (pm * x1) + pq1;

 

Here is comes a small problem: hot to draw the polygon on the same side? The equation of the distance between a line and a point has an absolute value, which leads to two possible solutions. Which one do I have to choose? I experimented with the normal of the polygon...

Surface normal

The normal vector to a surface is a vector which is perpendicular to the tangent plane to the surface. A surface normal for a polygon can be calculated by taking the vector cross product of all edges of that polygon. The order of the vertices used in the calculation will affect the direction of the normal (in or out of the face). This latter property of the surface normal is the one I want to use to try to draw all the polygons on the same side of the path determined by the samples positions

Because the polygon lies on the X-Y plane, I can just compute the Z component of the normal vector


computeNormal = function(p1, p2, p3, p4) {
      var nz = 0;

      var vertexes = [p1, p2, p3, p4];
      for (var i=0; i<vertexes.length-1; i++) {
            var curr = vertexes[i];
            var next = vertexes[i + 1];

            nz += (curr.x * next.x) * (curr.y * next.y);
      }

      return nz;
};

 

If the Z component is positive, I will select the other solution of the equation and re-calculate the polygon points using the new formula


var x1 = (d1 * Math.sqrt(1 + (m * m)) - (-pq1 + q)) / (- (pm - m));
var y1 = (pm * x1) + pq1;

 

Screenshot

This is the first version of the AirMobile data visualization page.  To be improved, but the foundations are there...

 

image

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Nice way to couple your data to digital map displays.

     

    We used to do this process using a GIS with a CAD section so that we could setup the overlay.

     

    The technology has come a long way since then.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to DAB

    Hi DAB

    What actually amaze me is how is easy today to implement features that a few year ago were considered "leading edge of technology"

     

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • amgalbu
    amgalbu over 11 years ago in reply to DAB

    Hi DAB

    What actually amaze me is how is easy today to implement features that a few year ago were considered "leading edge of technology"

     

    Ambrogio