In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - 30 - Bluetooth issues
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
  • Author Author: amgalbu
  • Date Created: 24 Feb 2015 10:23 AM Date Created
  • Views 1013 views
  • Likes 2 likes
  • Comments 2 comments
  • bluetooth
  • iot_distributed
  • interference
  • in_the_air
Related
Recommended

AirMobile - 30 - Bluetooth issues

amgalbu
amgalbu
24 Feb 2015

After recording this video, I closed down the bonnet with the intent to go around and collect some data. But as soon as I closed the bonnet, AirMobile sensor disconnected from the smartphone. I reopened the bonnet, and connection was back

The problem was clear, the reason less. I didn't expect the steel of the bodyshell to shield Bluetooth 2.4 GHz frequencies to that extent

In my opinion, the possible causes could be

 

Antenna / module position: the Bluetooth module was placed between the LaunchPad board and the AirMobile board. While the LaunchPad has a ground plane, the AirMobile hasn't. But the LaunchPad in on the "line of sight" between the Bluetooth module and the smartphone, so the ground plane could actually act as a shield

Bodyshell grounded: the steel the bodyshell is made of shields Bluetooth frequencies more than I expected because the bodyshell connected to the ground. I assumed that the simple equation "tyre = rubber = insulation" is not completely true. I found out that tyre's compound contains a certain amount f graphene (to reduce internal friction and hence fuel consumption) and graphene is a conductor...

High-frequency noise due to sparks: the last hypothesis is that high frequency noise are produced by the electrical system of the engine, in particular by the high voltages involved in generating sparks

 

Because I was not able to determine the root cause, I moved the Bluetooth module outside the case and placed it directly on the bonnet in a protective bag

 

image

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +1
    Ah, last minute problems, always a pain in the rear Trying to get some resolved myself ...
Parents
  • fvan
    fvan over 11 years ago

    Ah, last minute problems, always a pain in the rear image Trying to get some resolved myself ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fvan
    fvan over 11 years ago

    Ah, last minute problems, always a pain in the rear image Trying to get some resolved myself ...