In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [Firecracker Analyzer]Brief update
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
  • Author Author: ipv1
  • Date Created: 29 Nov 2014 11:09 AM Date Created
  • Views 2233 views
  • Likes 5 likes
  • Comments 14 comments
  • iot_firecracker
  • eagle
  • iot_ip
  • in_the_air
Related
Recommended

[Firecracker Analyzer]Brief update

ipv1
ipv1
29 Nov 2014

Its been a hectic couple of weeks and progress has been slow. I will be posting a series of smaller posts to cover work done and my "evil plans". One of the factors that contributed to my slow progress was sensor selection and I am still a bit stuck on that- the reasons I will explain. I also received the basic kits from E14 so thanks for the support. Lets jump in to the progress part direcly.

 

 

The Sensor Problem

I had planned on building a sensor system for open air and in order to do so I started contacting vendors like I usually do. I asked about the sensors they provide as well as their suitability for my application. Turns out that sensors such as the ones provided by SGX Sensortech (IS) Ltd like the MICS series is really not suitable for outdoor use. At least that what their sales manager says. Most of these sensors are made for indoor use and not sensitive enough for ambient air measurements. So what next?

 

 

Moving On

The objective here is to monitor air quality and that is why I had divided the system into two segments. There is an indoor as well as outdoor unit but there are many ready made solutions in the market so what can I do different? Well most of these work on measuring air quality and alerting when a level is exceeded so we can add a display as well as connecting it to the Internet. I already experimented with connecting the CC3200 with OpenHAB using MQTT for the Forget Me Not Challenge. That works! One change will be that we will be posting to the Sierrra Wireless Cloud instead of OpenHAB.

 

 

Since we have a 50USD budget for the PCBs I started work on the circuits. Not having selected the sensors still meant that I can work with power circuit. For the charger, I am using the BQ25504 so I used eagle to make the schematic.

 

image

 

 

Had to jump through a few hoops to make the footprint and that thing is smaller than small. Next was the boost converter for the 5V. This is getting to be very similar to the Fuel Booster Pack but it has its differences. The boost converter selected is  the TPS61200. Again a few hoops and I made the footprints to match the devices.

 

image

 

 

Next is the buck converter which is the tps62740. The footprint of this one is still a bit fuzzy and if anyone has it please send it across.

 

image

As of this writing, that part is under construction and I will blog about it in the next post.

 

 

I was thinking about doing a post on using eagle but there seems to be too many already and to be honest everyone has a systemm of doing things. I typically make the schematic in parts and keep committing to git. Once I am done with a part of the circuit, I jump into layout and just place the parts in a suitable arrangement. This makes sure that the part groups don't get mixed up and there is less confusion while doing the final placement and routing.

Anyway I will do a video when I route the board which I think I will have to dedicate some time for since there are layout considerations for the used devices and fitting them all on the PCB will be a challenge on its own.

 

Thanks to Micheal W for inputs on the post on inductors. It was useful.

 

Baby Steps:

I am going to finish the schematic this weekend and move onto the software part. More progress will be updated in separate posts.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Good update. DAB
  • ipv1
    ipv1 over 11 years ago in reply to michaelwylie +1
    That's is a good suggestion, however here is the deal... We do not have PCB making facilities at the university because it has never been a requirement. I am currently working to slowly get equipment for…
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1 +1
    Sounds like the best plan.
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Inderpreet,

     

    Great post! It's good to see this work on low-voltage regulator/ power mgmt devices, these are interesting parts - especially the first one which implements MPPT as you know (I see you have the solar capability on the diagram!).

    Looking forward to seeing how you get on!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 11 years ago in reply to shabaz

    Many thanks sir!

    Schematic is done and I will post a post soon image

    The schematic was painful and the layout is even more so. The no of devices on one booster is a bit much. Solar, buck, boost, lpm91000 and hdc1000 plus a cc110l. I think I am going to kick out the anaren module and use the booster pack as is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1

    How many ICs? If you need to move to four layers, the price at Seeed goes from 9.99 to 39.99 USD I think.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 11 years ago in reply to michaelwylie

    I am sticking to 2 layers  and that's why it might tàke a bit longer to layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ipv1
    ipv1 over 11 years ago in reply to michaelwylie

    I am sticking to 2 layers  and that's why it might tàke a bit longer to layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1

    Get a good stock of 0 ohm resistors image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 11 years ago in reply to michaelwylie

    Oh I am getting them in bulk from the higher quality maker. image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1

    I got an e-mail today from Seeed with a coupon code for $9.99 USD because I ordered my board during the Thanksgiving time. Would you like to use it for your purchase?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 11 years ago in reply to michaelwylie

    I got a 25USD coupon but I can only use it on the 10th image

     

    So in short, I will need the coupon IF i can get things done.

     

    Thanks for the support. I really appreciate it!

     

    Sincerely,

    IP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1

    ok, just let me know image