In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [FireCracker Analyzer]: Index
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
  • Author Author: ipv1
  • Date Created: 26 Oct 2014 8:21 AM Date Created
  • Views 1048 views
  • Likes 0 likes
  • Comments 2 comments
  • iot_firecracker
  • internet_of_things
  • in_the_air
  • index
Related
Recommended

[FireCracker Analyzer]: Index

ipv1
ipv1
26 Oct 2014

  • Project Proposal: The Firecracker Aftermath Analyzer
  • Blog Posts
  • Refrences

Project Proposal: The Firecracker Aftermath Analyzer

 

In order to measure the effect of Diwali firecrackers in India, a air pollution analyzer will be designed. It will have sensors for the following:

    1. Air Temperature

    2. NO2 Levels

    3. Single Sensor for carbon monixide, alcohol, acetone, thinner, formaldehyde

    4. particulate levels in the air

    5. Humidy

    6. Carbon Monoxide (CO)

    7.O2

    8. Sulphur based gases and

    9. Nitrus Gasous

The device will be based on the CC3200 which will be powered from the Fuel Booster Pack just like from my design in the Forget Me Not Challenge. It will charge using a solar panel and will also have a secondary battery pack which will be used only to power the sensors. The sensors can be selectively enabled or disabled remotely. It will connect to the Air Vantage Cloud for logging the data in real time. The system will demonstrate the pollution levels before Diwali and the days after. The data will also be collected by a in-building system made up of the BeagleBoneBlack which will also have similar sensors to the outside unit and will also talk to the Air Vantage Cloud.

 

image

 

Blog Posts

  • [Firecracker Analyser] [week 0] Project Description

 

Refrences

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    You might want to add a radiation detector.

    Some of the powders use radioactive materials.

     

    Just a thought.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    You might want to add a radiation detector.

    Some of the powders use radioactive materials.

     

    Just a thought.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ipv1
    ipv1 over 11 years ago in reply to DAB

    Why not... A gieger counter it is then.

    Thanks for the input DAB sir