In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog HAB monitoring Post#6 ( Sensor node enclosure design )
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
  • Author Author: rmlab
  • Date Created: 11 Dec 2014 1:09 AM Date Created
  • Views 2648 views
  • Likes 3 likes
  • Comments 14 comments
  • buoy
  • carbon_dioxide
  • pvc
  • iot_algal
  • airvantage
  • boosterpack
  • msp430fr5969
  • sierra
  • box
  • launcpad
  • water
  • beagleboneblack
  • in_the_air
  • enclosure
  • texas_instruments
  • iot
  • msp430
  • wireless
  • cc3200
  • solar
  • iot_water
Related
Recommended

HAB monitoring Post#6 ( Sensor node enclosure design )

rmlab
rmlab
11 Dec 2014


The image below shows my sensor node enclosure. The enclosure is an air-tight box where all electronics ( MSP430FR5969, batteries, C110L tranceiver) will be fixed inside. A total of four PVC elbows with 12 inches pipes are mounted on two longer sides of the air-tight box for sensor probes that will be submerged in the water. Additionally, upward pipe on one of the shorter side is also mounted for the Air temperature and Carbon dioxide sensors. A 5W soloar panel is placed in an inclined position on top of the box. I am still working on the removable holder for the solar panel that can adjusted 45 degrees on the pivot point. This enclosure will be embedded on a bamboo tray before deploying in sea water.

 

 

image


Additional photos of the sensor node enclosure.

image    imageimage

Click this link Ryan Labutap to view my previous post on this project.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +2
    Ryan If you are having trouble with sealing the upper pipe, you could add a u section so that any water would have to travel upwards before entering. This would ensure that wind blown water is not resting…
  • jw0752
    jw0752 over 11 years ago +2
    Hi Ryan, It looks like you are handling the water challenges of your project very well. Will your raft be tethered in position so that the solar panel remains tilted towards the sun? If so, how will your…
  • mcb1
    mcb1 over 11 years ago in reply to rmlab +2
    Ryan Have a search for mooring hints/suggestions for yachts. They face similar issues where they are tied and subject to wind and current action as well as the tide. You may wish to know how much the tidal…
  • rmlab
    rmlab over 11 years ago in reply to mcb1

    I'm thinking of making bamboo raft where I will embed the enclosure above. The bamboo raft is for buoyancy and at the same time protect my enclosure from direct water wave impacts.

    What do you think about the bamboo raft idea?

    Thanks mcb1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rmlab
    rmlab over 11 years ago in reply to nmctiglao

    The original reason for the upward pipe is actually for the color sensor to sense in upward direction. But yes I agree it might help prevent water from entering the box. Thanks for the idea sir, I might put upward pipe on the other three pipes that was originally designed straight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago

    Ryan

    If you are having trouble with sealing the upper pipe, you could add a u section so that any water would have to travel upwards before entering.

    This would ensure that wind blown water is not resting against your seal.

     

    I'd be inclined to add something tying the colour sensor and disolved oxygen pipes together to stop the wave action working at the seal.

    The last thing you need is water inside and damaging your electronics.

     

    I presume you will be adding some bouyancy inside as the last precaution.image

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nmctiglao
    nmctiglao over 11 years ago

    Is the upward pipe designed to keep water from entering the box?  Good work! It would be interesting to see in action.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<