Inductive Sensing
  • Challenges & Projects
  • Design Challenges
  • Inductive Sensing
  • More
  • Cancel
Inductive Sensing
Blog Inductive Sensing Design Challenge: USB Microphone based on the LDC1000 Inductance to Digital Converter (week 4)
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 21 May 2014 4:47 PM Date Created
  • Views 3073 views
  • Likes 0 likes
  • Comments 12 comments
  • inductive_sensing
  • eagle
  • inductive_sensing_challenge
  • microphone
  • farnell
  • winners
  • usb
  • ldc1000
  • texas_instruments
  • road_test
Related
Recommended

Inductive Sensing Design Challenge: USB Microphone based on the LDC1000 Inductance to Digital Converter (week 4)

e14 Contributor
e14 Contributor
21 May 2014

I can't believe it's already week 4 of the challenge, but here we are. Michael Kellett's comments on my last blog post prompted me to do some calculations on the dimensions of my initial design. As such I have put off Matlab and actually 3D printing the mount until I am sure about the dimensions, material, structure, etc. I am going to use. I definitely welcome all comments and criticism on my blog as this is a learning experience for me too (I obviously don't design microphones for a living).

 

I was initially confused about the typical dimensions of condenser microphones, because I couldn't find a real explanation besides the usual: a larger diaphragm will have a bad high frequency response. But why is this exactly? And what is considered large?

 

If we are talking about vibrations in a membrane, most texts start with a description of the movement and various modes in a stretched rectangular membrane and then move on to variations where the membrane is circular, fixed at a rim and the vibrations are forced. The condenser microphone and the microphone I am designing are special cases of a fixed circular membrane with forced vibrations.

Basically you take a thin piece of material (thin means the thickness is much less than the other dimensions of the membrane, otherwise it's considered a plate) and stretch it to a certain tension which is lower than the maximum allowed tension. Now it is quite obvious that the tension of the material will determine how much the membrane is displaced if a certain force is applied. The tighter the material is stretched, the less the displacement will be. But there is another important factor which is partially determined by the tension: the resonant frequency of the membrane.

Vibrations in a membrane can be described using the 2D wave equation. I will not go into this in detail, but the solutions of the 2D wave equation determine what the response of the membrane will be to an applied wave with a certain frequency and amplitude.

The first resonant frequency appears at image, since this is the first zero of the Bessel function image (you can calculate all zeros at http://keisan.casio.com/exec/system/1180573472) . image is the wave number and image is the diameter of the membrane (a list of symbols is given at the end of this blog post).

 

The fundamental frequency for a circular plate fixed at the rim is:

image

Where image is the surface density of the membrane in kg/m² and image is the tension applied to the membrane in N/m.

As an example we can calculate the resonant frequency of a circular membrane with a diameter of image, made of image aluminum  foil. Aluminum has a density of image.

To start our calculations we first need to determine how much the foil will be stretched. I'm not quite sure how I will measure this in practice, but suppose the maximum allowed tension is image (this will actually depend on the membrane thickness and the maximum allowable stress).

 

The surface density of the membrane is calculated by multiplying the density by the thickness of the membrane:

 

image

As stated earlier, the fundamental frequency appears at image. And for a uniform circular membrane we can calculate the value by:

 

image

Not very good for a general purpose microphone right? However, keep in mind that a practical microphone will have some form of damping, which will decrease the peak at resonance, somewhat extending the usable range. However, it will still be way below the audible range.

 

So how can we increase this? Well the first thing we could do is to try and increase the tension of the membrane, however this will decrease the average displacement as we will see next. The other thing we can try is to decrease the diameter, but this will again decrease the displacement of the membrane (which is more effective?) Finally, we could try using another material, preferably one with a lower density as you can clearly see from the formula. Copper and Steel both have a much higher density than aluminum as do most metals (which is intuitive because aluminum is pretty light). The only other candidate I can think of that has a decent permeability (if we are thinking ahead, for the LDC1000's requirements) is Magnesium, which has a density of only 1700kg/m^3.

 

The following figure shows the influence of various design parameters on the basic fundamental frequency of the vibrating membrane.

 

image

 
Clearly, the best high frequency response is obtained with a small membrane. We can also see that the thickness of the membrane will have a considerable impact on the fundamental frequency. However, this assumes that the tension on the membranes is identical. Typically you will be able to put more stress on a thicker membrane. The use of Magnesium increases the resonance frequency with a factor of about 1.26.
There are several acoustical structures that can have a positive effect on the usable range of the microphone. These will be discussed in a later blog.
 

The next important parameter is the sensitivity of the microphone. This will be determined by the resolution of the LDC1000 and coil, but also by the displacement of the membrane.

To determine the displacement we have to make certain assumptions. First of all the displacement will, over a large frequency range, depend on the frequency and the amplitude of the applied pressure wave. Second, we can determine either the displacement in the center, or probably more important in our case, the average displacement over the entire membrane.

Displacement of the membrane at distance image from the center is:
 
image
The average displacement amplitude over the entire surface area of the membrane is found by averaging the first expression over the surface area:
 
 
image

Using the same values as before, we have:

 

image

The Bessel functions are:

image

image

The average displacement then becomes:

image

The next figure shows the influence of the membrane diameter, thickness and material on the average displacement.

 

image

 
The average displacement increases significantly with the diameter and thickness of the membrane, however increasing these parameters will decrease the fundamental frequency. The type of material also has an effect on the displacement: a lighter membrane decreases the average displacement. EDIT: the first figure shows membrane displacement at a frequency of 1000Hz, which is close to the resonance frequency. The following figure shows the effect of resonance (remember: ka=2.405) on the
imageThe next figure shows the displacement at 100Hz, much lower than the resonance frequency:
This figure shows that the displacement is nearly independent of membrane thickness. I will have to verify if this is actually correct, because it seem counter intuitive at first sight (try putting a piece of paper in front of a speaker and then try the same with a sheet of plastic). It might be because the stifness of the membrane is so small compared to the applied tension that it does not have a significant effect (as compared to vibrating bars or plates), but as I said I will need to double check this.image
 
Not shown here is the effect of the tension, but it is obvious from the expressions that a tighter membrane will have a higher resonance frequency and a lower average displacement.
 
I have not done any full calculations on the LDC1000, but there are some parameters that can be derived from the basic calculations in this blog.
First of all, the coil will have to be mounted very close to the diaphragm in order to detect submicron vibrations. I am not quite sure how this will affect the signal to noise ratio or what the actual limits of the LDC1000 are. Also, the thickness of the material needs to be quite thin as shown in these calculations. However, the LDC1000 has a maximum sensor frequency of 5MHz. This is important, because the sensitivity will be significantly reduced if the thickness of the metal is less than three times the skin depth.
 
The skin depth can be calculated by:
image
Where image is the resistivity of the metal, about image for Aluminum.imageand image are the relative and absolute permeability which is approximately image for Aluminum. At the maximum frequency of 5MHz we get:
 
image
The sensitivity at three times the skin depth is about 95%. We can calculate how much the sensitivity will be using the following approximation:
 
 
image
The sensitivity at various thicknesses, for a skin depth of 37µm is shown on the next figure.
 
image
 
In conclusion the size, construction and materials of the microphone will have a significant impact on the frequency response and sensitivity. Further calculations and experiments will be required to determine the actual feasible frequency range and sensitivity.
 
Symbols used:
image
image
image
image
image
image
image
image
image
image
image
image
image
image
image
image
image
References:
Fundamentals of acoustics 4th edition (L. Kinsler)
 
  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Part of the challenge is to try many different designs.

    You never know when an unlikely combination of materials can give you a neat affect.  Ie. the Thomas Edison approach to science. image

    After all, its not a good experiment unless something loses the magic smoke.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Part of the challenge is to try many different designs.

    You never know when an unlikely combination of materials can give you a neat affect.  Ie. the Thomas Edison approach to science. image

    After all, its not a good experiment unless something loses the magic smoke.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to DAB

    You are right about that image It's hard to predict what type of design will have the best performance. I plan to print a ton of 3D mounts of various diameters which I will try with all sorts of foils.