Inductive Sensing
  • Challenges & Projects
  • Design Challenges
  • Inductive Sensing
  • More
  • Cancel
Inductive Sensing
Blog SteelQuad: Steel Quality Sensing Device (week 4)
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lexbryan
  • Date Created: 31 May 2014 4:05 PM Date Created
  • Views 1583 views
  • Likes 0 likes
  • Comments 4 comments
  • inductive_sensing
  • inductive_sensing_challenge
Related
Recommended

SteelQuad: Steel Quality Sensing Device (week 4)

lexbryan
lexbryan
31 May 2014

This week I got to check with construction material suppliers and ask for a quotation. I've also negotiated a place where I can do my concrete mix, water curing, and conduct inductance test.


Here’s the list of materials needed:


  • Rebars
    • 10 mm dia.
      • Grade 33
      • Grade 40
      • Grade 60
    • 12 mm dia
      • Grade 33
      • Grade 40
      • Grade 60
  • Cement
  • Sand and gravel
  • PVC Pipe
    • 2" dia
    • 4" dia
  • Cover
  • hacksaw and blades
  • Tarpaulin
  • Shovel
  • Hollow Blocks
  • Tier Wire


The tarpaulin and hollow blocks will be used for concrete curing. There’s also a helpful video I saw on youtube regarding interfacing with other coils: https://www.youtube.com/watch?v=5-Vg-ppdRGs


More exciting update in the coming weeks when I purchase the materials.


  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    It sounds like you are organized to begin testing.

     

    Can't wait to see what you come up with.

     

    DAB

     

    PS, have you thought of running some measurements while the cement cures?

    You could get some valuable data by seeing if the values change over the 30 day curing cycle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lexbryan
    lexbryan over 12 years ago in reply to DAB

    yeah. I've consider that. yet I'm also considering that it will affect the strength of the concrete. However, I can always do a separate group on same batch of concrete mix that won't be touch until done curing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to lexbryan

    The idea of doing several tests during the cure sounds very interesting. In fact one of the more unusual experiments I've seen on E14!

    On thing I was wondering when you said doing a separate batch is how consistent is any given batch from one to the next and is this in fact more than the differences in the cure strength or would add a large un known to the measurements?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Problemchild
    Problemchild over 12 years ago in reply to lexbryan

    The idea of doing several tests during the cure sounds very interesting. In fact one of the more unusual experiments I've seen on E14!

    On thing I was wondering when you said doing a separate batch is how consistent is any given batch from one to the next and is this in fact more than the differences in the cure strength or would add a large un known to the measurements?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • lexbryan
    lexbryan over 12 years ago in reply to Problemchild

    I mean, same batch of concrete but won't be touched until it's done curing. This phase will only be a prototype of my idea coz there are a lot of things to consider (e.g. strength of aggregate, temp., water quality, etc.) to make this scanning device 100% accurate. But I will surely continue this project even after the judging.