Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Blog CC3200 IoT Backyard Challenge Tomato Greenhouse Summary
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: janisalnis
  • Date Created: 7 Nov 2014 2:33 AM Date Created
  • Views 4971 views
  • Likes 6 likes
  • Comments 22 comments
  • iot_backyard
  • iot_tomato
  • backyard
  • winners
  • cc3200_launchpad
  • internet-of-things
  • iot
Related
Recommended

CC3200 IoT Backyard Challenge Tomato Greenhouse Summary

janisalnis
janisalnis
7 Nov 2014

Previous post: Energia is out there for CC3200

 

 

A summary for Internet of Things roadtest

 

Thanks to Texas Instruments Element 14 for possibility to be a roadtester for Simplelink Wi-Fi CC3200 launchpad.

It is a single chip containing  both Wi-Fi connectivity processor and Cortex M4 core ARM processor communicating over internal SPI connection.

I have tried to learn programming CC3200 in CCstudio and bloged about every step: Internet connectivity,  analog inputs, I2C, hibernation, power consumption, motor driving.

 

Data were stored and visualized by Plotly and Xively, and on a Linux webserver.

 

One of CC3200 boards worked autonomously for a month in a tomato greenhouse powered from solar panel and AA cells. Greenhouse was filmed by Android phone providing internet hotspot and later a time lapse was made: IoT in tomato greenhouse on Vimeo

From Sept 24 in video one can see a box containg CC3200.

 

The autumn came and was not enough time to implement automatic watering system in the greenhouse. I have set up automatic watering system using CC3200 on a flower pot indoors and it is continuously uploading data to IoT. From photodiode sensor one can see that days are getting shorter now in autumn:

http://85.254.232.222/webcammob3/sunlight/

 

Another successful application of CC320 is wireless measuring of hot water pipe temperature at home for over 1 month:

https://xively.com/feeds/242759090

 

I was first to write a blog on Element 14 website (1800 views) about CC3200 programming using Texas Instruments Energia when it was released in September 2014 and at Instructables.com (1500 views).  I was very happy that this blog was highligted by Hackaday.com reviewing coolest things done within hobby electronics.

 

Thanks to Element 14 for generously donating 7 launchpads and I could share boards with my colleagues and students. One of applications they are making is e-paper display for doors telling when will be back from lunch or meeting. Another will be about air quality monitoring in classrooms: CO2, dust, etc...

 

More ideas:

  • wireless bathroom scale that will allow me to follow my weight dynamics online.
  • mailbox notifying about post arrival
  • bicycle alarm employing onboard accelerometer
  • camera application for photos and household water/electricity meter readout.

 

 

 

Solar IoT garden lamp - weather station - intrusion detector

 

In my first blog entry I envisioned solar powered garden lamp with IoT connectivity and have recently started building it.

Solar driven garden lamps often can not supply light through all the night. PIR motion detector allows to switch on LEDs only when someone is nearby. Such lights are very practical at the house entrance door when trying to find keys.

 

12 superbright white LEDs are drawing 400 mA from 2xAA 2500 mAh rechargeable batteries. Actually, 2.4V is not enough to drive a white LED. I used step-up board from Wurth Electronics that was supplied in another roadtest (wireless challenge). Each 3 LEDs are connected in series and there are four such series. If necessary, it might be possible to program PIR alarm mode going to a mobile phone. Everything including the solar panel is hidden inside the white glass ball. Solar cell is placed on the upper part inside the ball.

 

image

 

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

image

  • Sign in to reply

Top Comments

  • doctorcdf
    doctorcdf over 11 years ago +3
    Hello - As the decision was made by Texas Instruments' panel of engineers, I am going to ask them to put together a blog post detailing their reasons for this decision. I hope that this resolves the matter…
  • doctorcdf
    doctorcdf over 11 years ago +3
    Here is the official response from Texas Instruments and element14 - In July, 10 participants were selected to receive the SimpleLink Wi-Fi CC3200 LaunchPad based on the quality of their submitted Internet…
  • mcb1
    mcb1 over 11 years ago in reply to .lukasz. +2
    The application that element14 posted (which may have been reduced) Internet of the Backyard Challenge Competitors Project: Tomato Plant Monitoring System Synopsis: We grow tomatoes in a small home…
Parents
  • .lukasz.
    .lukasz. over 11 years ago

    tomato grenhouse == solar garden lamp

    great competiton

     

    Project: Tomato Plant Monitoring System
    Synopsis:

    We grow tomatoes in a small home garden greenhouse. And they are so tasty! Greenhouse must be watered every 2nd day. And it is quite hard job. Water is brought from a small pond into a 200 l barrel to let it warm up and then manually distributed with a can to each plant.

     

    I would like to automate this process. I have bought a 20 W solar panel and a pool fountain pump able to lift water ca 2 m. Water consumption depends if day is sunny or cloudy and so also the available solar pump power. On a cloudy day the solar panel current is too weak to start the pump. I have deviced a circuit storing solar energy into a 1 Farad super-capacitor. When capacitor is charged full it starts to drive the pump for ca 20s. This eliminates battery that would need replacement after a few years.

     

    could somebody explain it for me ?

    this is joke or what ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • janisalnis
    janisalnis over 11 years ago in reply to .lukasz.

    Solar powered Wi-Fi garden lamp with sensors is some outcome from the Challenge that could be brought to Maker's Fair for show and possibly become a new product if there is a demand. By measuring soil moisture it is a part of plant watering system. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • janisalnis
    janisalnis over 11 years ago in reply to .lukasz.

    Solar powered Wi-Fi garden lamp with sensors is some outcome from the Challenge that could be brought to Maker's Fair for show and possibly become a new product if there is a demand. By measuring soil moisture it is a part of plant watering system.