Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Forum Have a question for TI re: The Internet of the Backyard Challenge? Ask here!
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 8 subscribers
  • Views 5871 views
  • Users 0 members are here
  • iot_backyard
Related

Have a question for TI re: The Internet of the Backyard Challenge? Ask here!

doctorcdf
doctorcdf over 12 years ago

This thread is dedicated to questions for the Internet of the Backyard challenge; Texas Instruments' staff will be monitoring it regularly.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to BigG +1
    It looks like the is a FET switch configured to protect against reverse voltage and should also protect the batteries from harm if the USB or other supply is also connected (Q2 bottom right)
  • bwelsby
    bwelsby over 12 years ago in reply to DAB +1
    DAB wrote: What is the APP needed to open the CCS 6 download? I got the same message on Windows 8.1 and 7. The TI message indicated that they were .exe files, but when I tried to change the name…
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor +1
    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots. Is there an simple HTTP POST example for CC3200? There is a GET function used…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Just so I do not recreate what may be already available, are there libraries already available for CC3200 to Plot.ly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Just so I do not recreate what may be already available, are there libraries already available for CC3200 to Plot.ly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Bill,

    I don't think there is a plot.ly port for CC3200 yet. Here are the list to the current TI official Cloud ecosystem partners for CC3200:

    CC31xx & CC32xx Cloud Ecosystem - Texas Instruments Wiki

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I was under the impression we were to use Plotly as our platform, is that no longer the case?

     

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    QUOTE:

     

    After being selected, you'll also be given access to Plotly, the web's premier data streaming and visualization software. Plotly has written code specifically designed to make it easy to get your backyard data to the Internet. Just imagine what you could do: the possibilities are endless.

    Once every two weeks, you'll post a blog entry showing us how you're getting on. The final build needs to be finished by October 3. Winners will be selected on October 13... and the prize?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    even without a library, every contestant should be able to write code to do this

     

    it is a challenge after all and with an amazing prize for the winner, that should take effort to win and im talking about a significant effort both in software, hardware and artistry/creativity, not just pulling a few libraries together

     

    the community will help of course, you only have to ask, but each one of you must be prepared to research, learn and document

     

    Good luck

     

    This is not aimed at you in particular but all too often road testers / contestants seem to take the easier road and replicate other peoples work, in some cases verbatim and that is not what this is about, sure borrow and modify other peoples code, ideas etc but make them your own

     

    if something does not exist, create it (Plotly Library for example) , the reward is worth the effort

     

    Peter

     

    a quick update

     

    Just discovered a member has got plotly to work, in linux using curl but the info is there and it should be fairly straight forward to convert to your use

    IoT live data upload to Plotly and Xively

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    My question about Plotly was because there was no mention of login in the congratulation email I got or in the dev kits received, so the 'given access' confused me. I created a login as it appears to be open to public. Just wanted to verify there was not a specific account I was required to use for the contest, or that I missed a step.

     

    thanks,

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    There would be a unique one set up for you, I am not sure of the process but @doctorcdf    may be able to point you in the right direction

     

    regards

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 12 years ago in reply to Robert Peter Oakes

    The closest library I could find which I'm looking at is a plotly library found on the mbed platform but it may be easier for me anyway just to create script that is specific to my app. I believe you can also use json encoding to send payload data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor

    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots.

     

    Is there  an simple HTTP POST example for CC3200? There is a GET function used in OOB example. Is there some example where POST is used? May be in Weather Example?

     

    Would like to HTTP POST following data to Plotly:

     

    http://107.21.214.199/clientresp "HTTP/1.1"

     

    version=2.3&origin=plot&platform=arduino&un=janisalnis&key=p3r69ls929

    &args=[{"x": ["2014-08-26 15:18:01"], "y": [25], "type": "scatter", "stream": {"maxpoints": 20}}]

    &kwargs={"filename": "streaming API", "fileopt": "extend", "world_readable": true}

     

     

    Alternative would be to use Arduino C code example for Plotly to compose a POST message.