Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Forum Have a question for TI re: The Internet of the Backyard Challenge? Ask here!
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 8 subscribers
  • Views 5889 views
  • Users 0 members are here
  • iot_backyard
Related

Have a question for TI re: The Internet of the Backyard Challenge? Ask here!

doctorcdf
doctorcdf over 12 years ago

This thread is dedicated to questions for the Internet of the Backyard challenge; Texas Instruments' staff will be monitoring it regularly.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to BigG +1
    It looks like the is a FET switch configured to protect against reverse voltage and should also protect the batteries from harm if the USB or other supply is also connected (Q2 bottom right)
  • bwelsby
    bwelsby over 12 years ago in reply to DAB +1
    DAB wrote: What is the APP needed to open the CCS 6 download? I got the same message on Windows 8.1 and 7. The TI message indicated that they were .exe files, but when I tried to change the name…
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor +1
    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots. Is there an simple HTTP POST example for CC3200? There is a GET function used…
Parents
  • janisalnis
    janisalnis over 12 years ago

    Hi, TI!

     

    I got stuck with a problem permanently storing programm on LAUNCHXL.

     

    I can build the project, debug it. Wi-Fi connect LED blinks and in serial console I can see text coming.

     

    When I run Uniflash and select oob.bin file to upload, it is uploaded. There are some other files that are present /sys/macadd.bin But after I reset the board and remove SOP2 jumper the board does not seem to run (no LED is blinking)

     

    Janis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • janisalnis
    janisalnis over 12 years ago in reply to janisalnis

    Problem solved.

    Lost half a day  time on Uniflash.

    I tried to add a new file to the project.

    Needed to modify bin file used under sys/mcuimg.bin

    In principle it is logical. That one just does not upload a progrsm file somewhere but to a already defined place.

    Now can flash my programm and it executes from flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • janisalnis
    janisalnis over 12 years ago in reply to janisalnis

    Problem solved.

    Lost half a day  time on Uniflash.

    I tried to add a new file to the project.

    Needed to modify bin file used under sys/mcuimg.bin

    In principle it is logical. That one just does not upload a progrsm file somewhere but to a already defined place.

    Now can flash my programm and it executes from flash.