Internet of the Backyard
  • Challenges & Projects
  • Design Challenges
  • Internet of the Backyard
  • More
  • Cancel
Internet of the Backyard
Forum Have a question for TI re: The Internet of the Backyard Challenge? Ask here!
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 8 subscribers
  • Views 5889 views
  • Users 0 members are here
  • iot_backyard
Related

Have a question for TI re: The Internet of the Backyard Challenge? Ask here!

doctorcdf
doctorcdf over 12 years ago

This thread is dedicated to questions for the Internet of the Backyard challenge; Texas Instruments' staff will be monitoring it regularly.

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to BigG +1
    It looks like the is a FET switch configured to protect against reverse voltage and should also protect the batteries from harm if the USB or other supply is also connected (Q2 bottom right)
  • bwelsby
    bwelsby over 12 years ago in reply to DAB +1
    DAB wrote: What is the APP needed to open the CCS 6 download? I got the same message on Windows 8.1 and 7. The TI message indicated that they were .exe files, but when I tried to change the name…
  • janisalnis
    janisalnis over 12 years ago in reply to e14 Contributor +1
    Registering at Plotly is free of charge for everyone. Limitation, I read somewhere, is that it would allow to store 50 plots. Is there an simple HTTP POST example for CC3200? There is a GET function used…
Parents
  • janisalnis
    janisalnis over 12 years ago

    Hi, TI!

     

    I got stuck with a problem permanently storing programm on LAUNCHXL.

     

    I can build the project, debug it. Wi-Fi connect LED blinks and in serial console I can see text coming.

     

    When I run Uniflash and select oob.bin file to upload, it is uploaded. There are some other files that are present /sys/macadd.bin But after I reset the board and remove SOP2 jumper the board does not seem to run (no LED is blinking)

     

    Janis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • janisalnis
    janisalnis over 12 years ago

    Hi, TI!

     

    I got stuck with a problem permanently storing programm on LAUNCHXL.

     

    I can build the project, debug it. Wi-Fi connect LED blinks and in serial console I can see text coming.

     

    When I run Uniflash and select oob.bin file to upload, it is uploaded. There are some other files that are present /sys/macadd.bin But after I reset the board and remove SOP2 jumper the board does not seem to run (no LED is blinking)

     

    Janis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • janisalnis
    janisalnis over 12 years ago in reply to janisalnis

    Problem solved.

    Lost half a day  time on Uniflash.

    I tried to add a new file to the project.

    Needed to modify bin file used under sys/mcuimg.bin

    In principle it is logical. That one just does not upload a progrsm file somewhere but to a already defined place.

    Now can flash my programm and it executes from flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to janisalnis

    you can upload directly to the launchpad from CCS, does it work this way ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • janisalnis
    janisalnis over 12 years ago in reply to Robert Peter Oakes

    I have not found how to upload programm permanently from the CCS. It remains only untill a reset.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to janisalnis

    Hi Janis,

    it is correct, CCS can only upload the binary to the SRAM. But for real application, you need to flash the binary to the external flash on the Launchpad using the UniFlash. Later during boot, this image will be again copied by the bootloader to the SRAM to be executed.