Products
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
IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog BLOG 14 : The Sensor Subsystem
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
  • Author Author: gsgill112
  • Date Created: 13 Nov 2017 10:58 AM Date Created
  • Views 1268 views
  • Likes 1 like
  • Comments 1 comment
  • sbsr
  • iks01a2
  • x-nucleo-iks01a2
  • sbsr_iotonwheels
  • iotonwheels
  • sensor
Related
Recommended

BLOG 14 : The Sensor Subsystem

gsgill112
gsgill112
13 Nov 2017

Ok, In this Blog I will talk about implementation of the Sensor Subsystem in My project.

 

Firstly the Role of Sensor Subsystem was to identify the weather for ride and to send it to the User. I had Dropped the Idea of pothole detection as it was not a worth Idea, moreover In my Nextion display You could just touch to report the pothole. see the BUMP Button below !!

image

 

As there was a mBed Library available online HERE as well as an Example Program available HERE it was easy to get started with the Library and implement the rest.

 

Now I would like to post my Implementation code snippet

 

Some Important defn

const static float seaLevelPressure = 1013.25;
const static float declinationAngle = 0.003839724;
float alt, LPS22HB_p, LPS22HB_p_previous, LPS22HB_t, HTS221_h, HTS221_t;
float angle;
int32_t LSM303AGR_a[3],LSM303AGR_m[3];
int32_t LSM6DSL_a[3],LSM6DSL_g[3];

 

Message Banks to be displayed on the Nextion display

// Message Bank  
// To 
/*      Var                     Bank            Msg 
 *      greatingMessages        1               0-2
 *      pressureMessages        2               0-1
 *      ridingMessages          3               0-2
 *      weatherMessages         4               0-5
*/ 
  
const char* greatingMessages[3] = {
    "Good Morning",
    "Good Evening",
    "Good Day"
};
const char* pressureMessages[2] = {
    "Up Up Up the hill we go",
    "Down we goooooo.... Yeeaahhh....."
};
const char* ridingMessages[3] = {
    "Com'on its a Pleasent Fine AWESOME day :)",
    "Hey Its a Holiday ! I will pickup dirt :(",
    "I know you are sleeping :| "
};
const char* weatherMessages[6] = {
    "Its pleasent to ride bike :)",
    "Its not to bad :) a bit Humid :)",
    "Its HUMID !! :|",
    "Not Today, Its very Humid :\\",
    "Its Chilling :O",
    "Its Hot :<"
};

 

Obj Creation

/* Instantiate the expansion board */
static XNucleoIKS01A2 *mems_expansion_board = XNucleoIKS01A2::instance(D14, D15, D4, D5);


/* Retrieve the composing elements of the expansion board */
static LSM303AGRMagSensor *magnetometer = mems_expansion_board->magnetometer;
static HTS221Sensor *hum_temp = mems_expansion_board->ht_sensor;
static LPS22HBSensor *press_temp = mems_expansion_board->pt_sensor;
static LSM6DSLSensor *acc_gyro = mems_expansion_board->acc_gyro;
static LSM303AGRAccSensor *accelerometer = mems_expansion_board->accelerometer;

 

Function called to update Messages based on Sensor Values

void updateMessage(void){
    hum_temp->get_temperature(&HTS221_t);
    hum_temp->get_humidity(&HTS221_h);
    // printf("HTS221: [temp] %7s C,   [hum] %s%%\r\n", print_double(buffer1, value1), print_double(buffer2, value2));
   
    // Use this in another function  
    if(HTS221_h < 70){
        messageInUse=0;
    }else if(HTS221_h > 70 && HTS221_h < 80){
        messageInUse=1;
    }else if(HTS221_h > 80 && HTS221_h < 90){
        messageInUse=2;
    }
    else{
        messageInUse=3;
    }
    if(HTS221_t < 20){
        messageInUse=4;
    }else if(HTS221_t > 20 && HTS221_t < 35){
        messageInUse=0;
    }else{
        messageInUse=5;
    }
    
    press_temp->get_temperature(&LPS22HB_t);
    press_temp->get_pressure(&LPS22HB_p);
    //printf("LPS22HB: [temp] %7s C, [press] %s mbar\r\n", print_double(buffer1, value1), print_double(buffer2, value2));
    if(LPS22HB_p_previous > LPS22HB_p){
        messageInUse=0;
    }else{
        messageInUse=1;
    }
    if(LPS22HB_t < 20){
        messageInUse=4;
    }else if(LPS22HB_t > 20 && LPS22HB_t < 35){
        messageInUse=0;
    }else{
        messageInUse=5;
    }
    
    //#ifdef DEBUG
        nextion.printf("%s\n",weatherMessages[messageInUse]);
    //#endif
}

 

inside Perodic Function to gather sensor data periodically

#ifdef DEBUG
        nextion.printf("Speedy Calc Over ---- \n Sensor Data Polling Begin\n");
    #endif    
    
    hum_temp->get_temperature(&HTS221_t);
    hum_temp->get_humidity(&HTS221_h);
    
    #ifdef DEBUG
    printf("HTS221: [temp] %7s C,   [hum] %s%%\r\n", print_double(buffer1, value1), print_double(buffer2, value2));
    #endif
    
    press_temp->get_temperature(&LPS22HB_t);
    press_temp->get_pressure(&LPS22HB_p_previous);
    //wait(5);
    
    #ifdef DEBUG
    printf("LPS22HB: [temp] %7s C, [press] %s mbar\r\n", print_double(buffer1, value1), print_double(buffer2, value2));
    printf("---\r\n");
    #endif
    
    magnetometer->get_m_axes(LSM303AGR_m);
    
    #ifdef DEBUG
    printf("LSM303AGR [mag/mgauss]:  %6ld, %6ld, %6ld\r\n", axes[0], axes[1], axes[2]);
    #endif
    
    accelerometer->get_x_axes(LSM303AGR_a);
    
    #ifdef DEBUG
    printf("LSM303AGR [acc/mg]:  %6ld, %6ld, %6ld\r\n", axes[0], axes[1], axes[2]);
    #endif
    
    acc_gyro->get_x_axes(LSM6DSL_a);
    
    #ifdef DEBUG
    printf("LSM6DSL [acc/mg]:      %6ld, %6ld, %6ld\r\n", axes[0], axes[1], axes[2]);
    #endif
    
    acc_gyro->get_g_axes(LSM6DSL_g);
    
    #ifdef DEBUG
    printf("LSM6DSL [gyro/mdps]:   %6ld, %6ld, %6ld\r\n", axes[0], axes[1], axes[2]);
    #endif
    
    //Altitude computation based on http://keisan.casio.com/exec/system/1224585971 formula 
    alt = pow((double)(seaLevelPressure/LPS22HB_p),(double)(1/5.257)) - 1;
    alt = alt * (LPS22HB_t + 273.15);
    alt = alt / 0.0065;
    
    angle -= declinationAngle;
    // Correct for when signs are reversed.
    if(angle < 0){   
      angle += 2*M_PI;
    }
    // Check for wrap due to addition of declination.
    if(angle > 2*M_PI){
      angle -= 2*M_PI;
    }
    
    angle = angle * 180/M_PI;
    
    updateMessage();

 

Hope you found this SHORT UPDATE useful image

 

If you want more information please comment and I will include it in the blog image 

 

Thanks for Reading

Regards,

GS Gill

  • Sign in to reply
Parents
  • DAB
    DAB over 8 years ago

    Nice update.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Nice update.

     

    DAB