IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog IOT on Wheels Design Challenge - Fatigue Alert System (Blog #6)
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
  • Author Author: dwinhold
  • Date Created: 29 Oct 2017 11:59 PM Date Created
  • Views 521 views
  • Likes 2 likes
  • Comments 1 comment
  • alert
  • fatugue
  • dwinhold
  • iot design
  • internet of things on wheels
Related
Recommended

IOT on Wheels Design Challenge - Fatigue Alert System (Blog #6)

dwinhold
dwinhold
29 Oct 2017

Programming the Nucleo STM32L476

 

I have found it a bit confusing programming the Nucleo in the IDE's suggested from the site. I am use to the Arduino IDE as it is fairly easy to use. So, I found a way to program the Nucleo with the Arduino IDE. This was created by Srihari Koripalli who deserves all the credit for this.

 

Below is how it is done:

 

  • Open the Arduino IDE
  • Go to the "File" menu
  • Go to "Preferences"
  • Under "Additional Boards Manager URLs" enter the link below:

 

https://raw.githubusercontent.com/stm32duino/BoardManagerFiles/master/STM32/package_stm_index.json

 

image

 

 

  • Go to "Tools" menu, Click on "Board" then Click on "Boards Manager"

 

  • Scroll down until you find the "STM32 Core" Package by ST-Microelectronics and install it. This will take a bit of time to install.

 

That is it for this part

 

  • Next download the PinMap for the Nucleo Board to the Arduino IDE

 

https://github.com/sriksh9/Nucleo-PinMapping-for-Arduino

 

The PinMap is technically for the f401 board, but is the same for the L476 and does work

 

  • Put the downloaded folder into the Arduino Library Folder (My directory is "C:\Program Files (X86)\Arduino\libraries")

 

  • Next you will have to change the Board in the IDE to the correct Nucleo board by going to "Tools" - "Board" - Select the correct board type "Nucleo-64"

 

  • Then select "Board Part Number" - Select "Nucleo L476RG" - Finally select the correct "Port" the board is attached to

 

This quick program blinks a light from "Pin D2" on the board (PinMap 1)

 

#include 
int a = pinMap(1); //pinMap(Mapped Pin) - for mapped pin refer the attacted image
void setup()
{
  pinMode(a, OUTPUT);
}
void loop()
{
  digitalWrite(a, 1);
  delay(500);
  digitalWrite(a, 0);
  delay(500);

}

 

I want to thank Srihari Koripalli for coming up with this!!

 

I hope this helps others with the programming of the board. It works great!!

 

Dale W

 

 

 

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +2
    dwinhold Nice find. Well done.
Parents
  • mcb1
    mcb1 over 8 years ago

    dwinhold

    Nice find.

    Well done.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago

    dwinhold

    Nice find.

    Well done.