IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog walkingwheels on Water  #10 Create Mobile APP for X-NUCLEO-IDB05A1 blewrite, control LED on/off
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
  • Author Author: fyaocn
  • Date Created: 18 Oct 2017 3:08 AM Date Created
  • Views 1008 views
  • Likes 2 likes
  • Comments 2 comments
  • walkingwheels
Related
Recommended

walkingwheels on Water  #10 Create Mobile APP for X-NUCLEO-IDB05A1 blewrite, control LED on/off

fyaocn
fyaocn
18 Oct 2017

1. To control the via BLE, the BLE service and BLE characteristics UUID shall be nominated.

In the mbed projects, 0xA000 plus blue UUID default value -0000-1000-8000-00805f9b34fb shall be used.

And set BLE characteristics UUID to 0xA001-0000-1000-8000-00805f9b34fb.

Device name of FLY. With 1 received to LED on and 0 for LED off.as of

    if ((params->handle == ledServicePtr->getValueHandle()) && (params->len == 1)) {
        actuatedLED = *(params->data);

 

Full codes as,

#include "mbed.h"
#include "ble/BLE.h"
#include "LEDService.h"
DigitalOut actuatedLED(LED1, 0);
const static char     DEVICE_NAME[] = "FLY";
static const uint16_t uuid16_list[] = {LEDService::LED_SERVICE_UUID};
LEDService *ledServicePtr;
void disconnectionCallback(const Gap::DisconnectionCallbackParams_t *params)
{
    (void)params;
    BLE::Instance().gap().startAdvertising(); // restart advertising
}
/**
 * This callback allows the LEDService to receive updates to the ledState Characteristic.
 *
 * @param[in] params
 *     Information about the characterisitc being updated.
 */
void onDataWrittenCallback(const GattWriteCallbackParams *params) {
    if ((params->handle == ledServicePtr->getValueHandle()) && (params->len == 1)) {
        actuatedLED = *(params->data);
    }
}
/** 
 * This function is called when the ble initialization process has failled 
 */ 
void onBleInitError(BLE &ble, ble_error_t error) 
{ 
    /* Initialization error handling should go here */ 
} 
/** 
 * Callback triggered when the ble initialization process has finished 
 */ 
void bleInitComplete(BLE::InitializationCompleteCallbackContext *params) 
{
    BLE&        ble   = params->ble;
    ble_error_t error = params->error;
    if (error != BLE_ERROR_NONE) {
        /* In case of error, forward the error handling to onBleInitError */
        onBleInitError(ble, error);
        return;
    }

    /* Ensure that it is the default instance of BLE */
    if(ble.getInstanceID() != BLE::DEFAULT_INSTANCE) {
        return;
    }

    ble.gap().onDisconnection(disconnectionCallback);
    ble.gattServer().onDataWritten(onDataWrittenCallback);
    bool initialValueForLEDCharacteristic = true;
    ledServicePtr = new LEDService(ble, initialValueForLEDCharacteristic);
    /* setup advertising */
    ble.gap().accumulateAdvertisingPayload(GapAdvertisingData::BREDR_NOT_SUPPORTED | GapAdvertisingData::LE_GENERAL_DISCOVERABLE);
    ble.gap().accumulateAdvertisingPayload(GapAdvertisingData::COMPLETE_LIST_16BIT_SERVICE_IDS, (uint8_t *)uuid16_list, sizeof(uuid16_list));
    ble.gap().accumulateAdvertisingPayload(GapAdvertisingData::COMPLETE_LOCAL_NAME, (uint8_t *)DEVICE_NAME, sizeof(DEVICE_NAME));
    ble.gap().setAdvertisingType(GapAdvertisingParams::ADV_CONNECTABLE_UNDIRECTED);
    ble.gap().setAdvertisingInterval(1000); /* 1000ms. */
    ble.gap().startAdvertising();
   while (true) {
        ble.waitForEvent();
    }
}


int main(void)
{
    BLE &ble = BLE::Instance();
    ble.init(bleInitComplete);
}

 

2. Now create empty cordova project with

- cordova create flywheels

- cordova platform add android

in www directory, put index.html as control UI as,

Then,

- cordova build android

- cordova run

I got apk file and here is the screenshot.

image

Upload one web UI for this flywheel introduction,

image

  • Sign in to reply

Top Comments

  • fyaocn
    fyaocn over 8 years ago in reply to carmelito +2
    Thanks, I will try to do it. I am close to complete the project. I will post the whole codes for your reference.
Parents
  • carmelito
    carmelito over 8 years ago

    Nice post,  Please can you elaborate a little on the cordova/mobile app part. I am planning to try out something similar with the BLE module.. Thanks in advance - Carmelito

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • carmelito
    carmelito over 8 years ago

    Nice post,  Please can you elaborate a little on the cordova/mobile app part. I am planning to try out something similar with the BLE module.. Thanks in advance - Carmelito

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fyaocn
    fyaocn over 8 years ago in reply to carmelito

    Thanks, I will try to do it.

     

    I am close to complete the project.  I will post the whole codes for your reference.