Just Encase
  • Challenges & Projects
  • Design Challenges
  • Just Encase
  • More
  • Cancel
Just Encase
Blog Remote Farm Monitoring and Watering System - Blog #2 Arduino MKR 1300 and Farm Update
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Just Encase to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: carmelito
  • Date Created: 10 Jan 2022 4:20 PM Date Created
  • Views 1084 views
  • Likes 5 likes
  • Comments 1 comment
  • grove LCD RGB display
  • Arduino MKR WAN 13000
  • temperature sensor
  • remote_monitoring_farm
  • just_encase
  • just encase
Related
Recommended

Remote Farm Monitoring and Watering System - Blog #2 Arduino MKR 1300 and Farm Update

carmelito
carmelito
10 Jan 2022

As part of second blog, for the Remote Farm Monitoring and Watering System, I am updating both the Arduino MKR 1300 with the latest firmware, that came as part of the kit. To start install the Arduino SAMD Board in the Arduino Board Manager

image

Once the boards are installed in the Arduino IDE, go to the File -> Examples -> MKRWAN2 section, MKRWANFWUpdate_standalone sketch. Now connect the Arduino MKR 1300 board to your computer/laptop using the USB cable and upload the sketch, once done open the serial monitor and ensure that the baudrate is set to 115200 baud.

image

In addition, I used the components in the Grove Starter Kit for Arduino, to quickly test getting the temperature and pot value and display it on the Grove – LCD RGB backlight. Here are the circuit connection

  • Temperature sensor connected to A0 on the MKR 1300
  • Analog sensor connected to A1 
  • And the SDA of the Grove – LCD backlight connected to pin#11 on MKR 1300
  • SCL of the Grove – LCD backlight connected to pin#12 on MKR 1300

imageimage

Also, we started work on the farm just before Christmas, firstly we cleared out the weeds from the area using a weed cutter and some other tools. And, then use a spade, and rake to create beds to put the vegetable seeds in. Here are some picture, we are kind of half done for now with respect to getting the area ready for planting, with a lot more to do in the coming weeks.

imageimage

image

 

  • Sign in to reply
  • DAB
    DAB over 4 years ago

    Nice start.

    It will be interesting to see if you can keep the jungle at bay while your crops grow.