Join us, in congratulating the winners of the Just Encase with challenge using enclosures from Hammond Manufacturing. These project builds are tested for a hazardous environment, such as extreme cold and heat or exposure to water and humidity.
The winners will win the following prizes and anyone who hit the Finisher criteria will get the finisher prize.
Winners will be sent prizes to the address on their application and will be contacted by danzima
The Winners
Grand Prize Winner
milosrasic98 - OrbWeaver Rover
See Blog Post
Judges Notes:
Showing the case working in different environments was good, The cases where well utilized with all the components used in the enclosures, The data collected was shown well, The complexity and design of this project was well thought through. The sensor alone was complexed enough but to add the rover to this project put it over the top.
The report was easy to follow, well laid out, and was a fun read. This guy is a stellar designer. Very impressed he was able to turn our box into a fully functioning rover!
Googly eyes for style points!
Runner Up Winner
christopherskala—Garden Pond Monitor
Judges Notes:
Use of the case in the elements was good. The report was easy to follow and I enjoyed read it. The data collected was display well It also solved a problem that lots of people have. This project was well thought out and showed our cases provided protection against the elements. A complicated project that can measure Water temp at various depths, Total dissolved solids, Water level, pH, Air temp, humidity, light levels, air pressure. I love the testing he did on the enclosures. The one passed 96+ hr submersion test! Very clear results in conclusion. The system works and is very useful!
Finishers:
Finishers will all get the finisher prizes free of charge.
Pratyush_ceteb – Wind Turbine Monitoring
DougW - Just Encase Solar Super Capacitor Weather Station
Feiticeir0 - Pool Water Monitoring
skruglewicz – Case Enclosure Reliability Monitor
vishwasn – Air Quality Monitor Project
milosrasic98 - OrbWeaver Rover
dwinhold – Winter Driving Safety
rsjawale24 - Landslide monitoring for the Himalayan region
RedCharly - Monitoring an irrigation canal using LoRa
gracemcnally - Particulate Matter Monitoring System for Wildfires
christophersky – Garden Pond Monitor
Taifur - Biofloc Monitoring System
guillengap - Monitoring and Protection an Ecological Area
Hammond Manufacturing Technical Judging Team |
![]() |
element14 Community Team Judges |
The Sponsored Kit Buy Now | The Specs |
---|---|
![]() |
Enclosure Case 1554UGY Water Tight ABS 200x120x90 Enclosure |
![]() |
Enclosure Case 1554H2GYCL IP68 60x119x180 PolyCarbonate Enclosure |
![]() ![]() Buy Now |
Electronics Part (x2) The Arduino MKR WAN 1300 has a selection of Arduino compatible sensors |
![]() |
Cable Gland A selection of Hammond Cable Glands |
![]() |
Other Recommended Parts
|