Light Up Your Life
  • Challenges & Projects
  • Design Challenges
  • Light Up Your Life
  • More
  • Cancel
Light Up Your Life
Forum Sponsored Kit Received (#1)
  • News
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Light Up Your Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 49 subscribers
  • Views 492 views
  • Users 0 members are here
  • design challenge
  • würth elektronik
  • Light Up Your Life
Related

Sponsored Kit Received (#1)

ZephyrusBlaze
ZephyrusBlaze 11 months ago

I got the Sponsored Kit

Hey everyone, just letting you know I received the Sponsored Kit. Super excited to start building with it — thanks to the organizers and Würth Elektronik. I’ll be using this kit to make a 10x5 LED matrix and share the process as I go.

What’s inside the box

Here’s everything I found, with quantities:

  • Würth Elektronik 1315050930002
    LED, AlInGaP / InGaN, RGB SMD, 120°, Round, R 13 mA / G 13 mA / B 13 mA — Quantity: 25

  • Würth Elektronik 1313210530000
    LED, AlInGaP / InGaN, RGB SMD, 120°, Dome, R 5.5 mA / G 5.5 mA / B 5.5 mA — Quantity: 25

  • Würth Elektronik 1312020030000
    LED, AlInGaP / InGaN, RGB SMD, 120°, Square, R 5.5 mA / G 5.5 mA / B 5.5 mA — Quantity: 25

  • Würth Elektronik 1312121320437
    LED, AlInGaP / InGaN, RGB SMD, 110°, Square, R 20 mA / G 20 mA / B 20 mA — Quantity: 25

  • Würth Elektronik 1315050930246
    LED, RGB SMD, 120°, Round, R 21 mA / G 21 mA / B 21 mA — Quantity: 25

  • Würth Elektronik 1311610030140
    LED, RGB SMD, 120°, Square, R 6 mA / G 6 mA / B 6 mA — Quantity: 25

  • 5050 LED breakout PCB
    PCB is 0.8 mm / 0.03" thick, ~10 mm / 0.4" spacing between rows — Quantity: 50

  • Multicomp Pro MCBB830K
    Solderless breadboard, ABS, 1 mm, 105 mm x 183 mm — Quantity: 2

  • Texas Instruments TXS0108EPWR
    Level translator, 8 channels, 1.65 V to 5.5 V — Quantity: 1

  • Arduino Zero (ABX00003)
    ATSAMD21G18, ARM Cortex M0+, 32 bit, 32 KB RAM, 256 KB Flash, 20 I/O pins — Quantity: 1

  • Power Supply with Interchangeable Plugs (MP007771)
    AC/DC power supply, 24 W, 9 V DC, 2.5 A — Quantity: 1

imageimageimageimageimage

My plan (short)

I’ll solder the 5050 LEDs to the breakout PCBs, wire them into a 10 columns x 5 rows setup, and control columns as chains from the Arduino Zero. I’ll post step by step: soldering, wiring the chains, code, and troubleshooting notes. Expect pics and short updates as I make progress.

I’ll start with the first solder session later this week and post the results.

  • Sign in to reply
  • Cancel
  • cstanton
    cstanton 11 months ago

    I'm so glad these kits manage to get through Smiley Are you supplementing the kit at all?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ZephyrusBlaze
    ZephyrusBlaze 11 months ago in reply to cstanton

    Yes, I'll be supplementing the kit. I'm planning to add an ESP-01 and connect it to an Arduino Zero so I can control the LED matrix wirelessly.

    By the way, I had mistakenly thought the contest deadline was at the end of November, but I just realized it's actually tomorrow. Since there's no time to publish five forum posts, can I just publish the project article instead?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JoRatcliffe
    JoRatcliffe 11 months ago in reply to ZephyrusBlaze

    Hi ZephyrusBlaze yes I'm sorry the deadline has now passed. But - so everyone can see how your project and your experience shaped up - you are very welcome to share your progress and let everyone know how things have gone Slight smile