Low Power IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Low Power IoT Design Challenge
  • More
  • Cancel
Low Power IoT Design Challenge
Blog Handy BLE drum #2 Get to know PSoC®︎ 62S2 Wi-Fi BT Pioneer Kit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 16 Sep 2021 6:06 AM Date Created
  • Views 772 views
  • Likes 3 likes
  • Comments 0 comments
Related
Recommended

Handy BLE drum #2 Get to know PSoC®︎ 62S2 Wi-Fi BT Pioneer Kit

fyaocn
fyaocn
16 Sep 2021

    • 1 The suprising Pack
    • 2 Compare with PSoCRegistered 6 WiFi-BT Pioneer Kit
    • 3 Hardware and core
    • 4 Hardware Function in The Design.
    • 5 Plug and Play

1 The suprising Pack

Thanks Element14 for surprising pack with PSoCRegistered 62S2 Wi-Fi BT Pioneer Kit. Notebook and sport water bottle in the packs are of very good quality.

Cypress provide classic pattern as always have been, as part of Infineon. The silk print on back of the PCB is very informative, can be one handy quick-reference to pins.

image

image

 

2 Compare with PSoCRegistered 6 WiFi-BT Pioneer Kit

Another part of the story is what new in the dev board, as of PSoCRegistered 62S2 Wi-Fi BT Pioneer Kit. There have been PSoCRegistered 6 WiFi-BT Pioneer Kit (CY8CKIT-062-WiFi-BT) already with part number 43012 and 4343W.

Search for the answer on the web.

  • PSoCRegistered 62 Wi-Fi BT
  • PSoCRegistered 62S2 Wi-Fi BT

In general the In general the difference in secure function, what S2 means.And the increased in Flash and SRAM

  • The PSoC 62S2 Pioneer Kit features the PSoC 62 MCU (CY8C624ABZI-S2D44): 150-MHz ArmRegistered CortexRegistered-M4 and 100-MHz Arm Cortex-M0+ cores, 2MB of Flash, 1MB of SRAM, Secure Digital Host Controller (SDHC) supporting SD/SDIO/eMMC interfaces, programmable analog blocks, programmable digital blocks, Full-Speed USB, a serial memory interface, a PDM-PCM digital microphone interface, and industry-leading capacitive-sensing with CapSenseRegistered.
  • The PSoC 6 WiFi-BT Pioneer Kit features the PSoC 62 MCU: a single- or dual-core MCU, with an ArmRegistered CortexRegistered-M4 and ArmRegistered CortexRegistered-M0+, 1MB of Flash, 288KB of SRAM, programmable analog blocks,  programmable digital blocks, Full-Speed USB, a serial memory interface, a PDM-PCM digital microphone interface, and industry-leading capacitive-sensing with CapSenseTm.

With compatible pins,

image

 

 

3 Hardware and core

Block diagram of PSoCRegistered 62S2 Wi-Fi BT Pioneer Kit PSoCRegistered 62S2 Wi-Fi BT Pioneer Kit

image

Adding CRYPTO Block with AES,SHA,CRC,TRNG,RSA,ECC

The core module is seperate mini-PCB on the base board. This design is good for fast production based on this carrier module.

 

image

 

 

4 Hardware Function in The Design.

PSoCRegistered 62S2 Wi-Fi BT Pioneer Kit is good for this proposed project, the BLE, and capsense are basic function in BLE Handy Drum. Play the handy drum, the beats can send for mobile and share the beat with your friends.

 

5 Plug and Play

Plug the mini-USB into the port, the orange LED blink continuously. The default program runs. Start the putty with 115200-8-N-1 on serial port COMx.

image

This is UART demo project, press <ENTER> the LED shall start/pause blinking.


It works fine. The board is ready to play now.image