Low Power IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Low Power IoT Design Challenge
  • More
  • Cancel
Low Power IoT Design Challenge
Blog Low Power IoT Design Challenge - Microwave Sensor
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 23 Sep 2021 2:39 PM Date Created
  • Views 1903 views
  • Likes 1 like
  • Comments 2 comments
  • node red
  • mqtt
  • low_power_iot
  • rcwl-0516
  • microwave sensor
Related
Recommended

Low Power IoT Design Challenge - Microwave Sensor

ralphjy
ralphjy
23 Sep 2021

I'm going to reuse a remote microwave sensor that I had put together for another project and thought that I should show its implementation.  I am using an inexpensive RCWL-0516 sensor that others in the community have used.  It uses the Doppler frequency shift of a reflected 3 GHz signal to detect motion.  It has a nominal range of about 7 meters and provides a digital output when motion is detected.  You can adjust the range and retrigger time by adding a resistor and capacitor, but you can't get a distance measurement unless you hack into the intermediate analog signals on the detection chip.

 

Here's a front and back view.  Sensitivity is best orthogonal to the component side (front) of the board.

image

image

 

For rapid prototyping of WiFi/BLE enabled sensors, I've developed a preference for using M5StickC modules from M5Stack.  These modules are ESP32-based and are convenient to use because they include a small LCD screen and 95 mAh battery.  Below is the module that I set up.

image

 

I'm publishing the microwave detections and the battery voltage to my local RPi4 MQTT broker.  I also turn on the onboard LED when the detector triggers.

 

Here's a video showing the Node-Red MQTT Dashboard and its response to the microwave detector module.  The Status is either "Secure" or "Motion" if the detector is triggered.  The "Doppler" chart shows a time history of the trigger events - the output signal resets after about a second of inactivity.  You can also see the LED turn on for every detection.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Because the battery on the M5StickC is so small, I use an 18650 rechargeable battery pack shown below when I deploy the unit.

image

 

In use, I can get detections consistently at about 6 meters which is sufficient for the path up to my entry door.  I have the option of directly connecting the sensor to the PSoC 62S2, but for now I'm going to leave it as a remote unit in case I want to reposition the detection zone.

  • Sign in to reply
Parents
  • DAB
    DAB over 5 years ago

    Very interesting approach.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Very interesting approach.

     

    DAB