Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Blog Smart Storage - Blog 6 - things are (still) moving
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: grahamwebberjhb
  • Date Created: 28 Jun 2016 3:52 PM Date Created
  • Views 837 views
  • Likes 2 likes
  • Comments 2 comments
  • design challenge
  • accessibility_projects
  • smartstorage
  • mla
Related
Recommended

Smart Storage - Blog 6 - things are (still) moving

grahamwebberjhb
grahamwebberjhb
28 Jun 2016

I have made some progress and the end is in sight though I am not sure if I will finish in time, but we shall see.

 

I have hacked and chopped and glued an old gearbox together, I found that the output shaft ran at nice speed with the first gear set I used but I was running the motor at 500 RPM, but it just didn't have the power at this speed so I re configured the gears and now I can run the motor at full tilt.

image

 

here is my first attempt at turning it on.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Next I added the rails to keep the buckets orderly, though they do get a bit shaken up as they go over the top roller cutting down the flanges of the roller should minimize this, also adding a swivel to hold the bucket to the chain was necessary. As I expected I had to reinforce the rollers as the CD's came off the bearing when I put a heavier load on the chain.

image

Now that the mechanical side it in an operable state, for now at least, I have to work on the electronics I have bought a couple of RTC chips MCP79410 and DS1307 they both use I2C communication so the implementation should be fairly similar I am planning on attempting to used the MCP79410 first and if I cannot get anywhere with that one I will try the other.

 

Once that is done I would like to use the two proximity sensors as a rough gesture sensing setup move your hand past in one direction the motor turns that way move your hand past the other way the motor moves in that direction hold your hand still it stops moving,  but we shall see if I get there.

 

until next time

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    You might want to add a tensioning device to take the slack out of the chain.

     

    You are getting a lot of movement and oscillation during start up and run time.

     

    Adding some tension will smooth out the chain movement.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    You might want to add a tensioning device to take the slack out of the chain.

     

    You are getting a lot of movement and oscillation during start up and run time.

     

    Adding some tension will smooth out the chain movement.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago in reply to DAB

    Thanks DAB I was originally planning to spring load one of the rollers  to add some tension but it seemed to get tricky, I will try put some foam around the driving roller the compression of the foam may help smooth things.

    I have also changed the gear ratio so I can drive it slower, I will try ramp up the speed, at the beginning and drive it slower during operation.

    If it still wobbles I will have to add a tensioner, maybe a RC car shock absorber or something like that to reduce vibration.