Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Forum Solutions for the visually impaired.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 6 subscribers
  • Views 1359 views
  • Users 0 members are here
  • project
  • iot
  • Accessibility
  • safety
Related

Solutions for the visually impaired.

e14 Contributor
e14 Contributor over 10 years ago

Hi! My name is Eric. I am moderately visually impaired and I have a question. I have a friend who is completely blind and has a child who is just starting to run around and tries to get into trouble (Of course she doesn't see it as trouble, she's just having fun)! image However, sometimes it is difficult to keep track of the child, and know if she's somewhere she shouldn't be. Does anyone have any ideas on what could help her out? I'm thinking of some type of system that would notify her if the child is going somewhere in the house she shouldn't be without supervision. But also will let her find her if she goes somewhere to hide, or just falls asleep on the floor so she doesn't trip over her. Maybe even tell her the child's location in the house. Suggestions on existing products, or parts that could be used to make the product are welcome. This will be an indoor application, so GPS is probably out. Also, would like something relatively inexpensive. Thanks for your time, and for any suggestions. Eric..

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +1
    How about a bell tied to the back of a wearable clothes. Sound can be picked up by mics located at various places around the house connected to a microcontroller with bluetooth. A simple app on a phone…
  • jw0752
    jw0752 over 10 years ago +1
    Hi Eric How about putting a belt on the child with a module that emits a low frequency noise every couple of minutes. Low frequency travels distances well and isn't obnoxious. The unit could have a separate…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to clem57 +1
    Thanks for the reply. Sound is definately one of the solutions I'm considering. My only concerns would be that the child will hear the device and think it's a toy and take it off. Also, I don't know if…
Parents
  • soumitrab
    0 soumitrab over 10 years ago

    You could try Bluetooth beacons. For example, installing a beacon in a place where the child should not be for starters. You can adjust the transmit power to cover a certain radius (as in area of the room/house etc) and every time the child is within the beacon area it triggers an event like a general alarm that the child would recognize as an area which is off limits for her while helping the mother know where in the house she is. Different areas could have different variations of the alarm to enable the mother to know her precise location.

    Of course the child would need to have a beacon like bracelet or something similar on her all the time. But when the wearable does not make any sound or show any sort of display, it is unlikely the child will suspect it, find it to be a nuisance and take it off.

    I can help you create and install this system, feel free to write to me if you want more info.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • soumitrab
    0 soumitrab over 10 years ago

    You could try Bluetooth beacons. For example, installing a beacon in a place where the child should not be for starters. You can adjust the transmit power to cover a certain radius (as in area of the room/house etc) and every time the child is within the beacon area it triggers an event like a general alarm that the child would recognize as an area which is off limits for her while helping the mother know where in the house she is. Different areas could have different variations of the alarm to enable the mother to know her precise location.

    Of course the child would need to have a beacon like bracelet or something similar on her all the time. But when the wearable does not make any sound or show any sort of display, it is unlikely the child will suspect it, find it to be a nuisance and take it off.

    I can help you create and install this system, feel free to write to me if you want more info.