MusicTech
  • Challenges & Projects
  • Design Challenges
  • MusicTech
  • More
  • Cancel
MusicTech
Blog tEChnOLOGICal communion: Introduction to SoftLab and early design sketches
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fraktalize
  • Date Created: 26 Jan 2016 6:10 PM Date Created
  • Views 1644 views
  • Likes 2 likes
  • Comments 8 comments
  • project_communion
Related
Recommended

tEChnOLOGICal communion: Introduction to SoftLab and early design sketches

fraktalize
fraktalize
26 Jan 2016

Hello again!

 

I've been waiting to begin most of my work until my kit arrives, but as I am still waiting for it to arrive I realized I need to get some work done. Since our local SoftLab has opened up about a week ago, I began working at the same time as it opened up. In the video below you will be introduced to the working place and what potential it carries.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

(For all fellow Flash refusers out there: https://goblinrefuge.com/mediagoblin/u/fraktalize/m/intro-to-softlab/  )

 

What I've been working with recently is mainly conceptualizing and trying to put the ideas down on paper. I've been making some early sketches on how the suit might look, and how I can expand on the concept. Since the kit still has not arrived I have decided to focus primarily on the music suit for this challenge, as I have been stumped on quite a bit of time. If the time allows, I will add the plant music into the equation and finish a prototype of the complete vision, but for now I've chosen to put most of my energy on the suit. It feels like it is the part most related to the challenge.

 

image

     First design sketch of the suit

 

Since the beginning of the project I have been thinking a lot about how to manifest what I truly want to. The idea is that the biological life of humans and the biological life of plants are unified through electronic music. Thus, I have considered adding things such as EEGs, heartbeat monitors and other things that could mirror the aspects of biological life. The neopixel setup at the chest would, conceptually, make a light show in conjunction with the heartbeat, and the pace of the music would follow the pace of the heart. I have also been thinking about how the suit should look, and since I love colors I want it to be a very colorful and geometrical suit. This sketch is just a very early sketch, and it is bound to change with time.

 

I have also been looking up different ways to create stretch sensors. There are a bunch of instructables that describe how to create stretch sensors - I believe I will have to try out some different ones and find which ones work best for my needs. I want the suit to smoothly read full body movements, so that the dancer can move fully intuitively without being distracted by trying to trigger the sensors. I want it to be a seamless experience. I'm thinking about where to place the stretch sensors, and below is a sketch of my initial ideas. I will have to experiment further before making a decision.

image

 

I am also considering other ways that movement can be used as a way to manipulate music. Altimeters, accelerometers, tilt sensors... There are a lot of fun tools out there which can be used to track different types of movement, and it is a field I will need to explore further!

 

So that is what I've been up to! More to come in a future update!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +2
    Very interesting post. I like the idea of making cloths that support your data collection for making You can have a person make music by moving and you can train people to walk silently using the same…
  • agerber
    agerber over 10 years ago +2
    Thanks for sharing the suit design sketches, I'm looking forward to seeing how you go with the stretch sensors - will they be a visible part of the design on the outside of the suit? I've played with using…
  • fraktalize
    fraktalize over 10 years ago in reply to DAB +1
    Thank you! Yes, I am sure there might be other ways to utilize the suit other than creating music. It will be fun to explore how to play around with it once it is created!
Parents
  • agerber
    agerber over 10 years ago

    Thanks for sharing the suit design sketches, I'm looking forward to seeing how you go with the stretch sensors - will they be a visible part of the design on the outside of the suit? I've played with using conductive jersey fabric for textile sensors but I've seen instructables for hand knitted and crocheted stretch sensors made from conductive yarn that have a very appealing hand-made aesthetic too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • agerber
    agerber over 10 years ago

    Thanks for sharing the suit design sketches, I'm looking forward to seeing how you go with the stretch sensors - will they be a visible part of the design on the outside of the suit? I've played with using conductive jersey fabric for textile sensors but I've seen instructables for hand knitted and crocheted stretch sensors made from conductive yarn that have a very appealing hand-made aesthetic too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fraktalize
    fraktalize over 10 years ago in reply to agerber

    Thanks for your ideas! Yes, I would like them to somehow be integrated into the visual design of the suit. We have some stretch sensing fabric in the SoftLab which I've been considering using, but I've also been looking around at some other alternatives. A crocheted/knitted stretch sensor would probably work nicely as well! I believe I will have to make different stretch sensors and see how well they function before I can make a final decision. I'm very grateful for your input!