MusicTech
  • Challenges & Projects
  • Design Challenges
  • MusicTech
  • More
  • Cancel
MusicTech
Blog Uploading wav files to Soundcloud.com using the BeagleBone
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: carmelito
  • Date Created: 6 Mar 2016 5:49 AM Date Created
  • Views 1270 views
  • Likes 2 likes
  • Comments 0 comments
  • beagle bone black
  • project_diydrumkit
  • music-tech
Related
Recommended

Uploading wav files to Soundcloud.com using the BeagleBone

carmelito
carmelito
6 Mar 2016

This is a tutorial to record a .wav file, using ALSA -arecord when a button a pressed, and then upload the recorded file to Soundcloud.com , as shown in the video below

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

image

 

Here are the steps you will have to follow -

#1 Setting up USB audio sound card  on the BeagleBone

Connect a  mic and speaker to the USB sound card and SSH into the BeagleBone to run the commands below. And using a LAN cable connect your BeagleBone to your home network router.( the soundcard i am using is called  HDE 7.1 Channel Usb External Sound Card Audio Adapter: Amazon.ca: Electronics )

 

#2 ALSA- utils should be installed by default if you bought your BeagleBone recently,if not run the following command just in case

root@beaglebone:~#apt-get update

root@beaglebone:~#apt-get install alsa-base alsa-utils

 

#3 Check if your sound card is detected using the command

root@beaglebone:~#lsusb

you should see USB sound card in the output ie C-Media Electronics, Inc. CM108 Audio Controller

image

#4 Check the default adapter from which sound will be outputted

root@beaglebone:~# aplay -l

As you see in the output below the sound is defaulted to output from the HDMI port, that is HDMI is maked as card 0

**** List of PLAYBACK Hardware Devices ****

card 0: Black [TI BeagleBone Black], device 0: HDMI nxp-hdmi-hifi-0 []

  Subdevices: 1/1

  Subdevice #0: subdevice #0

card 1: Device [USB PnP Sound Device], device 0: USB Audio [USB Audio]

  Subdevices: 1/1

  Subdevice #0: subdevice #0

 

#5 Modify the uEnv.txt file to disable  HDMI

Navigate to the /boot partition

root@beaglebone:~#cd /boot

and modify the uEnv.txt file and add the line below at the end of the file

root@beaglebone:~#nano uEnv.txt

optargs=capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN

 

image

 

#6 Make the USB sound card as the default by modifying the file below

root@beaglebone:~# nano /etc/modprobe.d/alsa-base.conf

 

In the file modify the value below from -2 to 0

# Keep snd-usb-audio from beeing loaded as first soundcard

options snd-usb-audio index=0

 

Now if  you run the aplay -l command you should see only one card

root@beaglebone:~#aplay -l

image

 

#7 Test recording and playing a file

create a folder called recordtest and then run the following command to test recording a wav file for 10 seconds

root@beaglebone:~#arecord -D plughw:0 --duration=10 -f cd -vv testsound.wav

and to play file with a speaker connected use

root@beaglebone:~#aplay testsound.wav

Note: you have have to adjust the volume of your speaker and mic use the command below

root@beaglebone:~#alsamixer

 

#8 Install the Soundcloud python wrapper

There are a couple of ways you can do this, i prefer to use pip, that is

root@beaglebone:~#pip install soundcloud

 

Here is the github link if you in a mood of manually installing it - https://github.com/soundcloud/soundcloud-python

Note: As of 05 March 2016 , as I am writing this blog there is dependency missing as part of the soundcloud repo use the command below to install it

root@beaglebone:~# pip install six

 

#9 Getting the auth token from Soundcloud

To upload the file to soundclound.com , we will have to get a auth-token which we will use in the final program.

Here start by creating a soundcloud account if you dont have one and go to the Developer console --> Your App --> and Register a new application

Make a client id and client secret, which you will have to modify in the python code below

 

import soundcloud

client = soundcloud.Client(client_id ='XXXXXXXXXXXXXXXXXXXXX',

                           client_secret ='XXXXXXXXXXXXXXXXXXXXXXX',

                           username = 'XXXXXX',

                           password = 'XXXXXXXXX')

print client.access_token

 

to run the program use

root@beaglebone:~#python userAuthToken.py

 

make a note o the access_token , which you will require as part of the next piece of python code. As part of the final deployment/project you will have to refresh the token regularly and if possible store it in database/file.

 

#10 Breadboard the circuit

For the circuit you will need 2 buttons and 2 LED's, in addition to you will also need 2 1kohms and 330 ohms resistors

Connect the LEDS via 330 ohms resistor to pin P9_11 and P9_12

And the button using the 1K ohms pull down resistors to P9_13 and P9_15

 

#Button and LED connections

recordLED = "P9_11"

uploadLED = "P9_12"

recordButton = "P9_13"

uploadButton = "P9_15"

 

image

 

#11 Modify the python program with your token to record and upload to soundcloud

 

Modify the soundcloudToken value as part of the program attached below with the value you received as part of step 9 and run it using

root@beaglebone:~#python soundcloudRecordUpload.py

image

 

#12 Modify the Name and description of the uploaded file on soundclound.com

 

Now once you done you can modify the details on Soundcloud, upload a fancy image and add it to your favorite play-list ..

image

Attachments:
soundcloudRecordUpload.py.zip